Network Developers Kit API  3.61.01.01
Data Fields
_ci_client Struct Reference

#include <netcfg.h>

Collaboration diagram for _ci_client:
Collaboration graph

Data Fields

uint32_t ClientType
 
uint32_t Status
 
uint32_t IPAddr
 
char MacAddr [6]
 
char Hostname [256]
 
uint32_t TimeStatus
 
uint32_t TimeExpire
 

Field Documentation

§ ClientType

uint32_t _ci_client::ClientType

§ Status

uint32_t _ci_client::Status

§ IPAddr

uint32_t _ci_client::IPAddr

§ MacAddr

char _ci_client::MacAddr[6]

§ Hostname

char _ci_client::Hostname[256]

§ TimeStatus

uint32_t _ci_client::TimeStatus

§ TimeExpire

uint32_t _ci_client::TimeExpire

The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale