Network Developers Kit API  3.61.01.01
Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
httpif.h File Reference

Go to the source code of this file.

Data Structures

struct  _ntparam_http
 

Macros

#define HTTPPORT   80
 
#define MAX_RESPONSE_SIZE   200
 
#define http400(Sock)   httpSendErrorResponse((Sock), HTTP_BAD_REQUEST)
 
#define http404(Sock)   httpSendErrorResponse((Sock), HTTP_NOT_FOUND)
 
#define http405(Sock)   httpSendErrorResponse((Sock), HTTP_NOT_ALLOWED)
 
#define http501(Sock)   httpSendErrorResponse((Sock), HTTP_NOT_IMPLEMENTED)
 

Typedefs

typedef struct _ntparam_http NTPARAM_HTTP
 

Enumerations

enum  HTTP_STATUS_CODE {
  HTTP_OK =200,
  HTTP_NO_CONTENT =204,
  HTTP_BAD_REQUEST =400,
  HTTP_AUTH_REQUIRED =401,
  HTTP_NOT_FOUND =404,
  HTTP_NOT_ALLOWED =405,
  HTTP_NOT_IMPLEMENTED =501,
  HTTP_STATUS_CODE_END
}
 

Functions

void * httpOpen (NTARGS *pNTA, NTPARAM_HTTP *pNTP)
 Create an instance of the HTTP Server. More...
 
void httpClose (void *hHTTP)
 Destroy an instance of the HTTP Server. More...
 
int httpVersion (void)
 
void httpSendClientStr (SOCKET Sock, char *Response)
 
void httpSendStatusLine (SOCKET Sock, int StatusCode, char *ContentType)
 
void httpSendFullResponse (SOCKET Sock, int StatusCode, char *RequestedFile)
 
void httpSendEntityLength (SOCKET Sock, int32_t EntityLength)
 
void httpSendErrorResponse (SOCKET Sock, int StatusCode)
 

Variables

char * CONTENT_TYPE_APPLET
 
char * CONTENT_TYPE_AU
 
char * CONTENT_TYPE_CSS
 
char * CONTENT_TYPE_DOC
 
char * CONTENT_TYPE_GIF
 
char * CONTENT_TYPE_HTML
 
char * CONTENT_TYPE_JPG
 
char * CONTENT_TYPE_MPEG
 
char * CONTENT_TYPE_PDF
 
char * CONTENT_TYPE_WAV
 
char * CONTENT_TYPE_ZIP
 
char * CONTENT_TYPE
 
char * CONTENT_LENGTH
 
char * CRLF
 
char * DEFAULT_NAME
 
char * HTTP_VER
 
char * SPACE
 
int(* httpErrorResponseHook )(SOCKET Sock, int StatusCode)
 
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale