The Telnet Server service provides a mechanism for exposing a stream IO connection to any remote telnet client console.
More...
The Telnet Server service provides a mechanism for exposing a stream IO connection to any remote telnet client console.
§ NTPARAM_TELNET
§ CI_SERVICE_TELNET
§ TelnetOpen()
Create an instance of the Telnet Server.
- Parameters
-
| [in] | pNTA | Pointer to common arg structure used for all services |
| [in] | pNTP | Pointer to Telnet parameter structure |
- Returns
- Success: handle to new Telnet Server instance
-
Failure: NULL
- See also
- TelnetClose()
§ TelnetClose()
| void TelnetClose |
( |
void * |
hTelnet | ) |
|
Destroy an instance of the Telnet Server.
- Parameters
-
| [in] | hTelnet | Handle to Telnet Server instance obtained from TelnetOpen() |
- See also
- TelnetOpen()