AWS IoT Plugin Change Log
Table of Contents
3.30
New Features
AWSIOT-78 |
Create macOS installer |
AWSIOT-75 |
Add sysconfig support to examples |
AWSIOT-72 |
Quick Start Guide Updates |
AWSIOT-70 |
Support the SimpleLink 3.30 (Q3 2019) SDKs |
AWSIOT-67 |
Convert large ms timeout values into seconds on iot_tls_read |
AWSIOT-66 |
MSP432E4 - Define certificate arrays in a source file instead of a header file |
AWSIOT-14 |
CC32XX - Use Uniflash tool for flashing certs securely |
Bugs Resolved
AWSIOT-32 |
CC32XX - Support AP WiFi provisioning option |
Compatibility Notes
All examples in this release have been updated to use SysConfig. SysConfig generates .c and .h files with the various configuration data structures and constants. These files were previously written by hand. Check the SimpleLink SDK’s User’s Guide for more information about SysConfig.
2.20
New Features
AWSIOT-62 |
Support the SimpleLink 2.40 (Q4 2018) SDKs |
AWSIOT-48 |
Add support for CC3235 |
Bugs Resolved
2.10
New Features
AWSIOT-58 |
Add print to the beginning of the AWS example thread |
AWSIOT-53 |
Support the SimpleLink 2.30 (Q3 2018) SDKs |
Bugs Resolved
AWSIOT-56 |
clean up code of iot_tls_connect() and iot_tls_destroy() may free the same object twice |
2.00
New Features
AWSIOT-54 |
Update to v3.0.1 tag in aws-iot-device-sdk-embedded-C repo |
AWSIOT-51 |
Add support for MSP432E4 |
AWSIOT-50 |
Support the SimpleLink 2.20 (Q2 2018) SDKs |
AWSIOT-9 |
Switch to PEM formatted certificates |
Bugs Resolved
AWSIOT-46 |
Update sl_WlanConnect() call to use the user configured SECURITY_TYPE macro |
AWSIOT-41 |
Update Shadow Console example README file's command to have extra arg |
AWSIOT-38 |
Correct filename in banner comment of certs.h |
1.10
New Features
AWSIOT-30 |
Examples shouldn't call Display_ APIs from main |
AWSIOT-25 |
Add installer description for .zip files in QSG |
AWSIOT-23 |
Update to CC3220 1.40 SDK |
AWSIOT-22 |
Demonstrate how to enable power management in the examples |
AWSIOT-15 |
Example code should retry NTP server when it doesn't respond |
Bugs Resolved
AWSIOT-37 |
Add FREERTOS_INSTALL_DIR variable into products.mak |
AWSIOT-34 |
Change examples to call sl_stop() with a 200ms wait time |
AWSIOT-31 |
AWS examples should not define OVERWRITE_CERTS in compiler options |
AWSIOT-24 |
Hard fault occurs when calling AWS connect/disconnect/connect sequence |
1.00
New Features
AWSIOT-4 |
Update to CC3220 SDK 1.30 |
AWSIOT-3 |
AWS timer and network layer should use POSIX APIs |
AWSIOT-2 |
Update aws_iot_connect() to call TLS_setCerts() to set them as specified in the app code |
Bugs Resolved