AWS IoT Plugin Change Log
Table of Contents
2.20
New Features
ID | Summary |
---|---|
AWSIOT-62 | Support the SimpleLink 2.40 (Q4 2018) SDKs |
AWSIOT-48 | Add support for CC3235 |
Bugs Resolved
ID | Summary |
---|---|
None | None |
2.10
New Features
ID | Summary |
---|---|
AWSIOT-58 | Add print to the beginning of the AWS example thread |
AWSIOT-53 | Support the SimpleLink 2.30 (Q3 2018) SDKs |
Bugs Resolved
ID | Summary |
---|---|
AWSIOT-56 | clean up code of iot_tls_connect() and iot_tls_destroy() may free the same object twice |
2.00
New Features
ID | Summary |
---|---|
AWSIOT-54 | Update to v3.0.1 tag in aws-iot-device-sdk-embedded-C repo |
AWSIOT-51 | Add support for MSP432E4 |
AWSIOT-50 | Support the SimpleLink 2.20 (Q2 2018) SDKs |
AWSIOT-9 | Switch to PEM formatted certificates |
Bugs Resolved
ID | Summary |
---|---|
AWSIOT-46 | Update sl_WlanConnect() call to use the user configured SECURITY_TYPE macro |
AWSIOT-41 | Update Shadow Console example README file's command to have extra arg |
AWSIOT-38 | Correct filename in banner comment of certs.h |
1.10
New Features
ID | Summary |
---|---|
AWSIOT-30 | Examples shouldn't call Display_ APIs from main |
AWSIOT-25 | Add installer description for .zip files in QSG |
AWSIOT-23 | Update to CC3220 1.40 SDK |
AWSIOT-22 | Demonstrate how to enable power management in the examples |
AWSIOT-15 | Example code should retry NTP server when it doesn't respond |
Bugs Resolved
ID | Summary |
---|---|
AWSIOT-37 | Add FREERTOS_INSTALL_DIR variable into products.mak |
AWSIOT-34 | Change examples to call sl_stop() with a 200ms wait time |
AWSIOT-31 | AWS examples should not define OVERWRITE_CERTS in compiler options |
AWSIOT-24 | Hard fault occurs when calling AWS connect/disconnect/connect sequence |
1.00
New Features
ID | Summary |
---|---|
AWSIOT-4 | Update to CC3220 SDK 1.30 |
AWSIOT-3 | AWS timer and network layer should use POSIX APIs |
AWSIOT-2 | Update aws_iot_connect() to call TLS_setCerts() to set them as specified in the app code |
Bugs Resolved
ID | Summary |
---|---|
None | None |