SimpleLink CC32XX SDK AWS IoT Plugin 2.10.00.04 Release Notes

Table of Contents

Introduction

The AWS IoT Plugin enables users to create AWS IoT applications. It includes the necessary AWS IoT sources, as well as documentation and examples.

Documentation

The following documentation is provided with this release.

What’s New

2.10.00.04

New Features

ID Summary
AWSIOT-58 Add print to the beginning of the AWS example thread
AWSIOT-53 Support the SimpleLink 2.30 (Q3 2018) SDKs

Bugs Resolved

ID Summary
AWSIOT-56 clean up code of iot_tls_connect() and iot_tls_destroy() may free the same object twice

Upgrade and Compatibility Information

This release updates dependencies (SimpleLink SDK and AWS IoT C SDK versions), so refer to documentation in those products for any upgrade and/or compatibility notes.

The AWS IoT Plugin examples were updated to accomodate any changes and/or breaks in dependencies, so you may consider reviewing example differences if upgrading is introducing issues in existing code bases.

Host Support

Dependencies

This release requires the following software components and tools versions to successfully function:

See the CC32XX SDK documentation for IDE and toolchain dependencies

Device Support

This release supports the following devices:

Validation Information

This release was validated using the following software components. Please use the versions below, or compatible:

Known Issues

Versioning

All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases. Pre-releases are denoted with a suffix (e.g. 2.00.00.00_eng).

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. aws_cc32xx_2_10_00_04.

Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.

Last updated: 2018-11-07