SimpleLink CC3220 SDK AWS IoT Plugin 1.10.00.07 Release Notes
Table of Contents
Introduction
The AWS Plugin enables users to create AWS applications. It includes the necessary AWS sources, as well as documentation and examples.
Documentation
The following documentation is provided with this release.
What’s New
1.10.00.07
Defects
The following Defects were resolved
ID | Summary |
---|---|
AWSIOT-37 | Add FREERTOS_INSTALL_DIR variable into products.mak |
AWSIOT-34 | Change examples to call sl_stop() with a 200ms wait time |
AWSIOT-31 | AWS examples should not define OVERWRITE_CERTS in compiler options |
AWSIOT-24 | Hard fault occurs when calling AWS connect/disconnect/connect sequence |
Enhancements
The following Enhancements were resolved
ID | Summary |
---|---|
AWSIOT-30 | Examples shouldn't call Display_ APIs from main |
AWSIOT-25 | Add installer description for .zip files in QSG |
AWSIOT-23 | Update to CC3220 1.40 SDK |
AWSIOT-22 | Demonstrate how to enable power management in the examples |
AWSIOT-15 | Example code should retry NTP server when it doesn't respond |
Upgrade and Compatibility Information
TBD
Host Support
- Windows
- Linux
Dependencies
This release requires the following software components and tools versions to successfully function:
- CC3220 SDK 1.40.01.00
See the CC3220 SDK documentation for IDE and toolchain dependencies
Device Support
This release supports the following devices:
- CC3220
Validation Information
This release was validated using the following software components. Please use the versions below, or compatible:
- CC3220 SDK 1.40.01.00
Known Issues
- None
Versioning
All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases. Pre-releases are denoted with a suffix (e.g. 1.10.00.00_eng).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. aws_cc3220_1_10_00_07.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Last updated: 2017-07-19