Readme.txt for BSP for LM3S3748.
The BSP requires the IAR Embedded Workbench v5.1x.

Supported hardware:
===================
The sample project for Luminary LM3S3748 is prepared
to run on an Luminary LM3S3748 eval board,
but may be used on other target hardware as well.
By default, the project is configured to use the 
J-Link JTAG emulator.

Configurations
==============
- Debug_FLASH:
  This configuration is prepared for debugging and
  can be downloaded into internal FLASH using J-Link
  and CSpy.

- Release_FLASH:
  This configuration is prepared to build a "release"
  output which can be downloaded into FLASH
  using CSPy and IAR Flashloader.