See http://www.freertos.org/portLM3Sxxxx_Eclipse.html for documentation on
using this demo with GCC and/or Eclipse.

See http://www.freertos.org/portlm3sx965.html for documentation on using this
demo with either Keil or IAR development tools.




Each real time kernel port consists of three files that contain the core kernel
components and are common to every port, and one or more files that are 
specific to a particular microcontroller and or compiler.

+ The FreeRTOS/Source directory contains the three files that are common to 
every port.  The kernel is contained within these three files.

+ The FreeRTOS/Source/Portable directory contains the files that are specific to 
a particular microcontroller and or compiler.

+ The FreeRTOS/Source/include directory contains the real time kernel header 
files.

See the readme file in the FreeRTOS/Source/Portable directory for more 
information.