#	FreeRTOS.org V4.8.1 - Copyright (C) 2003-2008 Richard Barry.
#
#	This file is part of the FreeRTOS.org distribution.
#
#	FreeRTOS.org is free software; you can redistribute it and/or modify
#	it under the terms of the GNU General Public License as published by
#	the Free Software Foundation; either version 2 of the License, or
#	(at your option) any later version.
#
#	FreeRTOS.org is distributed in the hope that it will be useful,
#	but WITHOUT ANY WARRANTY; without even the implied warranty of
#	MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
#	GNU General Public License for more details.
#
#	You should have received a copy of the GNU General Public License
#	along with FreeRTOS.org; if not, write to the Free Software
#	Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
#
#	A special exception to the GPL can be applied should you wish to distribute
#	a combined work that includes FreeRTOS.org, without being obliged to provide
#	the source code for any proprietary components.  See the licensing section 
#	of http://www.FreeRTOS.org for full details of how and when the exception
#	can be applied.
#
#	***************************************************************************
#	See http://www.FreeRTOS.org for documentation, latest information, license 
#	and contact details.  Please ensure to read the configuration and relevant 
#	port sections of the online documentation.
#	***************************************************************************


#/************************************************************************* 
# * Please ensure to read http://www.freertos.org/portLM3Sxxxx_Eclipse.html
# * which provides information on configuring and running this demo for the
# * various Luminary Micro EKs.
# *************************************************************************/

RTOS_SOURCE_DIR=../../../Source
DEMO_COMMON_DIR=../../Common/Minimal
DEMO_INCLUDE_DIR=../../Common/include
UIP_COMMON_DIR=../../Common/ethernet/uIP/uip-1.0/uip
LUMINARY_DRIVER_DIR=../../Common/drivers/LuminaryMicro

CC=arm-none-eabi-gcc
OBJCOPY=arm-none-eabi-objcopy
LDSCRIPT=standalone.ld

# should use --gc-sections but the debugger does not seem to be able to cope with the option.
LINKER_FLAGS=-nostartfiles -Xlinker -oRTOSDemo.axf -Xlinker -M -Xlinker -Map=rtosdemo.map -Xlinker --no-gc-sections

DEBUG=-g
OPTIM=-O0


CFLAGS=$(DEBUG) -I . -I $(RTOS_SOURCE_DIR)/include -I $(RTOS_SOURCE_DIR)/portable/GCC/ARM_CM3 \
		-I $(DEMO_INCLUDE_DIR) -D GCC_ARMCM3_LM3S102 -D inline= -mthumb -mcpu=cortex-m3 $(OPTIM) -T$(LDSCRIPT) \
		-D PACK_STRUCT_END=__attribute\(\(packed\)\) -D ALIGN_STRUCT_END=__attribute\(\(aligned\(4\)\)\) -D sprintf=usprintf -D snprintf=usnprintf -D printf=uipprintf \
		-I $(UIP_COMMON_DIR) -I ./webserver -ffunction-sections -fdata-sections -I $(LUMINARY_DRIVER_DIR)

SOURCE=	main.c \
		timertest.c \
		./ParTest/ParTest.c \
		rit128x96x4.c \
		osram128x64x4.c \
		formike128x128x16.c \
		$(LUMINARY_DRIVER_DIR)/ustdlib.c \
		$(DEMO_COMMON_DIR)/BlockQ.c \
		$(DEMO_COMMON_DIR)/blocktim.c \
		$(DEMO_COMMON_DIR)/death.c \
		$(DEMO_COMMON_DIR)/integer.c \
		$(DEMO_COMMON_DIR)/PollQ.c \
		$(DEMO_COMMON_DIR)/semtest.c \
		$(DEMO_COMMON_DIR)/GenQTest.c \
		$(DEMO_COMMON_DIR)/QPeek.c \
		$(DEMO_COMMON_DIR)/recmutex.c \
		./webserver/uIP_Task.c \
		./webserver/emac.c \
		./webserver/httpd.c \
		./webserver/httpd-cgi.c \
		./webserver/httpd-fs.c \
		./webserver/http-strings.c \
		$(UIP_COMMON_DIR)/uip_arp.c \
		$(UIP_COMMON_DIR)/psock.c \
		$(UIP_COMMON_DIR)/timer.c \
		$(UIP_COMMON_DIR)/uip.c \
		$(RTOS_SOURCE_DIR)/list.c \
		$(RTOS_SOURCE_DIR)/queue.c \
		$(RTOS_SOURCE_DIR)/tasks.c \
		$(RTOS_SOURCE_DIR)/portable/GCC/ARM_CM3/port.c \
		$(RTOS_SOURCE_DIR)/portable/MemMang/heap_2.c

LIBS= $(LUMINARY_DRIVER_DIR)/arm-none-eabi-gcc/libdriver.a $(LUMINARY_DRIVER_DIR)/arm-none-eabi-gcc/libgr.a

OBJS = $(SOURCE:.c=.o)

all: RTOSDemo.bin
	 
RTOSDemo.bin : RTOSDemo.axf
	$(OBJCOPY) RTOSDemo.axf -O binary RTOSDemo.bin

RTOSDemo.axf : $(OBJS) startup.o Makefile
	$(CC) $(CFLAGS) $(OBJS) startup.o $(LIBS) $(LINKER_FLAGS)

$(OBJS) : %.o : %.c Makefile FreeRTOSConfig.h
	$(CC) -c $(CFLAGS) $< -o $@

startup.o : startup.c Makefile
	$(CC) -c $(CFLAGS) -O1 startup.c -o startup.o
		
clean :
	cs-rm $(OBJS)