Software Architecture¶
Block Diagram and Interface Model¶
This section describes the high-level TI 15.4-Stack CoProcessor-based system architecture, the various software components, and the overall system architecture (see Figure 12.). The TI 15.4-Stack CoProcessor is an entity that implements the IEEE 802.15.4e/g standard in a dedicated system on a chip and provides a serial interface to an external processor for control and processing of the CoProcessor operations. A description of the API is provided in the TI-15.4-Stack-CoP-Interface-Guide inside the /docs folder of the TI 15.4-Stack Linux SDK installation.
The TI 15.4-Stack CoProcessor approach is a scalable architecture split that fits perfectly for configurations where the host application runs protocol stack layers over the IEEE 802.15.4 e/g MAC/PHY (for example, generic IP over 6LoWPAN, Zigbee® IP, or Zigbee Pro) or even an application that must use the MAC/PHY as a data link.
With the TI 15.4-Stack Linux Example Application, the external host software is running on a Linux-based platform. The high-level software partitioning of layers can be conceptually applied to non-Linux hosts. The software components developed and described in this document are specific to a Linux- host implementation for an x86 or Arm® based platform.
The interface between the host and the TI 15.4-Stack CoProcessor is defined at different logical layers in this split architecture: a physical layer (for example, a USB or a universal asynchronous receiver/transmitter [UART]), a logical data-link layer, and a presentation layer.
The physical layer interface is used to transport the serial frames over the physical link. Several physical interfaces can be used (for example, USB or UART). This serial protocol is known as the management and test (MT) protocol.
The frames transported over the physical serial link follow the format
specified in the TI-15.4-Stack-CoP-Interface-Guide in the /docs
folder
within the TI 15.4-Stack Linux SDK installation.
The Collector Example Application delivered with this package illustrates an example of how to implement a high-level application that is intended to use the TI 15.4-Stack CoProcessor services.
Software system components:
TI 15.4-Stack CoProcessor Embedded Example Application: This is embedded software running on a SimpleLink CC13xx/CC26x2 device. This example application implements a 802.15.4e/g MAC/PHY layer and provides a (serial port) MT- based interface to the applications running on the Linux host.
NPI Server v2: The network processor interface (NPI) server provides a socket-based communication channel to the TI 15.4-Stack CoProcessor that abstracts the physical serial-communication mechanism (for example, UART or USB).
Note
The NPI server is an optional module; therefore, TI 15.4-Stack can interface directly to the Linux kernel through the dev interface as well.
Linux kernel: This provides a device-driver model for the serial interface that is available as a character device over the selected physical port (for example, USB). In the USB case for instance, the TI 15.4-Stack CoProcessor implements a CDC USB driver class; therefore, the kernel should provide a USB modem (ACM) service over /dev.
TI 15.4-Stack Application: This application module implements a specific application using the 802.15.4e/g protocol and the MT structure-based model as an application-level interface.
- Application: The TI 15.4-Stack Linux SDK Sample Application provides a starting point to use the TI 15.4-Stack CoProcessor by illustrating how to initialize the network, join a network, and perform data communication between the personal area network (PAN) Coordinator and the devices (that is, implementing a star-network topology).
- API MAC: This is the application programming interface (API) for the TI 802.15.4 MAC software. This API provides an interface to the management and data services of the 802.15.4 stack using the CoProcessor embedded example application. This module supports two communication methods. Method 1 is direct through a /dev/tty (serial-port) interface, and Method 2 uses a TCP/IP stream socket that connects to the NPI Server. The NPI server translates the TCP/IP connection into a /dev/tty (serial port) interface.