87 #ifndef ti_drivers_watchdog_WatchdogMSP432E4__include 88 #define ti_drivers_watchdog_WatchdogMSP432E4__include uint32_t intNum
Definition: WatchdogMSP432E4.h:167
Watchdog driver interface.
Watchdog hardware attributes for MSP432E4.
Definition: WatchdogMSP432E4.h:165
uint32_t intPriority
Definition: WatchdogMSP432E4.h:168
const Watchdog_FxnTable WatchdogMSP432E4_fxnTable
Watchdog function table for MSP432E4.
uint32_t baseAddr
Definition: WatchdogMSP432E4.h:166
uint32_t reloadValue
Definition: WatchdogMSP432E4.h:169
bool isOpen
Definition: WatchdogMSP432E4.h:178
Watchdog Object for MSP432E4.
Definition: WatchdogMSP432E4.h:177
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:362