59 #ifndef ti_drivers_crc_CRCMSP432E4__include 60 #define ti_drivers_crc_CRCMSP432E4__include CRC_ByteSwap byteSwapInput
Definition: CRCMSP432E4.h:93
uint32_t finalXorValue
Definition: CRCMSP432E4.h:87
CRC_ReturnBehavior
The way in which CRC function calls return after completing.
Definition: CRC.h:329
uint32_t timeout
Definition: CRCMSP432E4.h:85
void * resultLocation
Definition: CRCMSP432E4.h:89
uint32_t seed
Definition: CRCMSP432E4.h:86
CRC_ByteSwap
These byte swapping configurations are primarily for dealing with endianness mismatch. Not all implementations support all configurations.
Definition: CRC.h:384
CRC_DataSize
The CRC driver will consume data in blocks of this size. Not all implementations support all sizes...
Definition: CRC.h:395
uint32_t resultProcessedPartial
Definition: CRCMSP432E4.h:91
uint32_t resultRawPartial
Definition: CRCMSP432E4.h:90
void(* CRC_CallbackFxn)(CRC_Handle handle, int_fast16_t status, void *result)
The definition of a callback function used by the CRC driver when used in CALLBACK mode...
Definition: CRC.h:412
CRC_DataSize dataSize
Definition: CRCMSP432E4.h:92
uint8_t isOpen
Definition: CRCMSP432E4.h:95
CRC_ReturnBehavior returnBehavior
Definition: CRCMSP432E4.h:94
CRC_CallbackFxn callbackFxn
Definition: CRCMSP432E4.h:84
uint32_t configRegister
Definition: CRCMSP432E4.h:88
CRCMSP432E4 Hardware Attributes.
Definition: CRCMSP432E4.h:83
uint8_t ongoingPartial
Definition: CRCMSP432E4.h:96