Data Structures
AESCBCMSP432E4.h File Reference

Detailed Description

AESCBC driver implementation for the MSP432E4 family.

The generic driver interface can be found in AESCBC.h. This file should only be included in the board file to fill the AESCBC_Config struct.

Features

Limitations

Performance

Polling mode offers better performance than blocking and callback mode because no DMA and no interrupt handling is involved. It is recommended to use polling mode for messages shorter than 512 bytes.

Measurements have been taken with 16 bytes key length. Encryption and decryption show equal performance.

Length (bytes) Polling mode (microseconds) Blocking/callback mode
16 41 73
32 42 73
64 46 73
128 52 82
256 66 87
512 93 101
1024 148 128
4096 475 292
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/AESCBC.h>
Include dependency graph for AESCBCMSP432E4.h:

Go to the source code of this file.

Data Structures

struct  AESCBCMSP432E4_HWAttrs
 Hardware-specific configuration attributes. More...
 
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale