MSP432E4 DriverLib API Guide  1.11.00.03
MSP432E4 DriverLib API Reference

The Texas Instruments MSP432E4 Peripheral Driver Library is a set of drivers for accessing the peripherals found on the MSP432E4 family of microcontrollers. While they are not drivers in the pure operating system sense (that is, they do not have a common interface and do not connect into a global device driver infrastructure), they do provide a mechanism that makes it easy to use the device's peripherals.

The capabilities and organization of the drivers are governed by the following design goals:

Some consequences of these design goals are:

For many applications, the drivers can be used as is. But in some cases, the drivers will have to be enhanced or rewritten in order to meet the functionality, memory, or processing requirements of the application. If so, the existing driver can be used as a reference on how to operate the peripheral.

The following modules are available:

© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale