MSP432E4 DriverLib API Guide  1.11.00.03
Functions
sw_crc.h File Reference
#include <stdint.h>
Include dependency graph for sw_crc.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Functions

uint8_t Crc8CCITT (uint8_t ui8Crc, const uint8_t *pui8Data, uint32_t ui32Count)
 
uint16_t Crc16 (uint16_t ui16Crc, const uint8_t *pui8Data, uint32_t ui32Count)
 
uint16_t Crc16Array (uint32_t ui32WordLen, const uint32_t *pui32Data)
 
void Crc16Array3 (uint32_t ui32WordLen, const uint32_t *pui32Data, uint16_t *pui16Crc3)
 
uint32_t Crc32 (uint32_t ui32Crc, const uint8_t *pui8Data, uint32_t ui32Count)
 
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale