Release Notes
Table of Contents
Introduction
This is a GA release of the Core SDK 4.10.02.00 for MSP432E4 devices.
Documentation
Open the documentation overview web page file in the SDK’s Doc folder for a full list of documentation.
What’s New
A summary of changes made in the current release of this product can be found in the product Change Log.
This release continues to preview a new tool coming out called SysConfig which allows graphical configuration of TI’s drivers. A number of improvements have been made since the second preview version was provided in Core SDK 3.60.00. Click here for more information.
A json example is included in this release.
Upgrade and Compatibility Information
This release breaks compatibility with previous releases of the Core SDK in the following ways:
TIDRIVERS-3397 – IAR linker scripts do not properly reserve HEAP and STACK space. The IAR linker scripts in prior releases did not reserve the memory for stack and heap. The sections were placed at the end of RAM and it was possible for other sections to overlow into them. We suggest that you compare your linker script with the latest linker scripts in this release.
TIDRIVERS-3620 – removed deprecated TIMER_ and CAPTURE_ #defines from Timer.h and Capture.h. These #defines were replaced with Timer_ and Capture_ counterparts to match the coding conventions several releases ago. The TIMER_ and CAPTURE_ version were maintainted for backwards compatbility.
Host Support
See the SDK release notes for a description of which host operating systems are supported in this release.
Dependencies
See the SDK release notes for a description of which components and tools are required to work with this product.
Device Support
See the SDK release notes for a list of TI devices that are supported in this product.
Validation Information
The Core SDK was validated with the following components:
- Code Composer Studio 9.0.0
- ARM 18.12.1.LTS
- GNU Code Generation Tools
- ARM GCC 7-2017-q4-major
- IAR Code Generation Tools
- ARM 8.32.2
- FreeRTOS 10.1.1
- XDCTools 3.51.02
Known Issues
ID | Summary |
---|---|
TIDRIVERS-3636 | I2C_transfer() occasionally fails when called from an interrupt context |
TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
A summary of changes made in previous releases of this product can be found in the product Change Log