Network Services 2.60.00.07 Release Notes
Table of Contents
Introduction
The Network Services Component is a portable networking API that abstracts different network stacks found on TI devices. A BSD/POSIX socket API is provided as well.
Network Services also includes a SNTP client, HTTP 1.x client/server, and MQTT client/server.
Documentation
The following documentation is provided with this release.
What’s New
2.60.00.07
Defects
The following Defects were resolved
ID | Summary |
---|---|
NS-209 | HTTPClient documentation missing define explanations |
NS-188 | MQTTClient documentation missing functions |
Enhancements
The following Enhancements were resolved
ID | Summary |
---|---|
NS-224 | Move JSON library from Network Services to TI Utilties |
NS-222 | Explicitly document that NS requires an RTOS |
NS-217 | The HTTP Server shall support secure connections (HTTPS) |
Upgrade and Compatibility Information
- To address NS-224, the JSON builder/parser that was previously managed as part of the Network Services Component is now managed in the TI Utilities Component. You will now need to look there for documentation.
If updating from a previous version of NS, see the changelog for potential upgrade and compatibility information.
Host Support
- Windows
- Linux
- Mac
Toolchain Support
Network Services supports building libraries for the following ISA/toolchain combinations, your SDK may provide a subset of these libraries:
ISA | TI/CCS | IAR | GCC |
---|---|---|---|
C674x | 8.3.2 | N/A | N/A |
C66 | 8.3.2 | N/A | N/A |
Arm9 | 18.12.1.LTS | N/A | N/A |
A8F | N/A | N/A | gcc-arm-none-eabi-7-2017-q4-major |
A9F | N/A | N/A | gcc-arm-none-eabi-7-2017-q4-major |
A15F | N/A | N/A | gcc-arm-none-eabi-7-2017-q4-major |
A53F | N/A | N/A | gcc-linaro-7.2.1-2017.11-x86_64_aarch64-elf |
M4 | 18.12.1.LTS | 8.32.2 | gcc-arm-none-eabi-7-2017-q4-major |
M4F | 18.12.1.LTS | 8.32.2 | gcc-arm-none-eabi-7-2017-q4-major |
R5F | 18.12.1.LTS | N/A | N/A |
Device Support
Please refer to the SDK Release Notes for device support.
Known Issues
- The Network Services Component is still fairly new, and there remains an expectation that issues will be found requiring minor API evolutions in the next few releases before stabilizing. We don’t expect significant changes, but it is likely there may be a few compatibility breaks. Please report issues on the TI E2E forums.
Versioning
All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 2.10.00.00_eng).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Technical Support
Last updated: 2019-02-21