Release Notes
Table of Contents
Introduction
This is a GA release of the Core SDK 3.80.00.22 for MSP432E4 devices.
Documentation
Open the documentation overview web page file in the SDK’s Doc folder for a full list of documentation.
What’s New
A summary of changes made in the current release of this product can be found in the product Change Log.
This release continues to preview a new tool coming out called SysConfig which allows graphical configuration of TI’s drivers. A number of improvements have been made since the second preview version was provided in Core SDK 3.60.00. For more information, see the README file included in the syscfg directory as well as the Wiki page located here.
Upgrade and Compatibility Information
This release breaks compatibility with previous releases of the Core SDK in the following ways:
The UARTMon module has been removed. This module was not documented and there were not examples that used it.
The ti/drivers/SDSPI ti/drivers/sdspi/* drivers have been removed. These drivers had been deprecated for several quarters with warning messages for any code that used them. The ti/drivers/SD and ti/drivers/sd/* drivers should be used instead.
Host Support
See the SDK release notes for a description of which host operating systems are supported in this release.
Dependencies
See the SDK release notes for a description of which components and tools are required to work with this product.
Device Support
See the SDK release notes for a list of TI devices that are supported in this product.
Validation Information
The Core SDK was validated with the following components:
- Code Composer Studio 8.3.0
- ARM 18.1.4.LTS
- GNU Code Generation Tools
- ARM GCC 7-2017-q4-major
- IAR Code Generation Tools
- ARM 8.20.2
- FreeRTOS 10.0.0
- XDCTools 3.51.01
Known Issues
ID | Summary |
---|---|
TIRTOS-1435 | clock_nanosleep() with CLOCK_REALTIME broken on msp432 |
TIDRIVERS-1808 | UART_write() should return error if UART is still busy |
TIDRIVERS-1796 | ADCBufMSP432E4.h port definitions do not support inputs greater than 15 due to a bug in the code that causes incorrect values in sequence control and the sequence extension registers. |
TIDRIVERS-1683 | ADC driver only initializes one sequencer per module, even when user wants to use multiple sequencers |
TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
A summary of changes made in previous releases of this product can be found in the product Change Log