Change Log
Table of Contents
Core SDK 3.80.00 (Current Release)
New Features
ID | Summary |
---|---|
TIRTOS-1588 | CoreSDK shall provide an HTTP Server Example |
TIRTOS-1584 | Updated examples to use Board_init() instead of Board_initGeneral() |
TIRTOS-1572 | Add C11 aligned_alloc() to FreeRTOS memory support |
TIRTOS-1453 | Watchdog example must not clear the watchdog in the ISR |
TIRTOS-1417 | Update MSP432E4 to mbedtls 2.7 LTS stream |
TIRTOS-1326 | Update examples to use BASSENSORS BoosterPack instead of SENSORS-BOOSTXL |
TIDRIVERS-3335 | use common attribute ((align(x))) syntax when alignment is needed |
TIDRIVERS-2929 | Redesign SHA2 top-level API |
TIDRIVERS-2047 | Implement MSP432E4 AESCTR driver |
TIDRIVERS-2045 | Implement MSP432E AESGCM driver |
TIDRIVERS-1824 | Implement MSP432E4 SHA2 driver |
TIDRIVERS-1823 | Add AESCCM driver for MSP432E4 |
TIDRIVERS-1822 | Add AESCBC driver for MSP432E4 |
TIDRIVERS-1727 | Add function to PWM to set load and match in one call |
TIDRIVERS-1723 | Remove SDSPI driver from build (has been deprecated for several quarters) |
TIDRIVERS-1540 | NVSSPI25X should implement polling delay in doErase() to prevent CPU starvation |
TIDRIVERS-650 | Improve External Flash erase time for NVSSPI25X driver |
Bugs Resolved
ID | Summary |
---|---|
TIRTOS-1767 | usleep(n) should sleep “at least” n microseconds |
TIRTOS-1760 | http client examples fail to account for string null-terminator when setting USER_AGENT header |
TIRTOS-1607 | Get pthread priority incorrect after priority change [FreeRTOS] |
TIRTOS-1527 | clock_settime should not discard tv_nsec |
TIDRIVERS-3388 | Improve Precision of ConvertToMicrovolts() functions for ADC and ADCBuf driver |
TIDRIVERS-3366 | The Display driver incorrectly sets the LCD SPI clock frequency to 4Mhz instead of the 1MHz rated value |
TIDRIVERS-2069 | SPIFFS_unlock() improperly uses lock->count |
TIDRIVERS-1825 | ADCBufMSP432E4 definitions for A22 and A23 are swapped |
TIDRIVERS-1814 | I2C drivers incorrectly handle error on last byte transmitted |
Core SDK 3.70.00 (Aug 23 2018)
New Features
ID | Summary |
---|---|
TIRTOS-1543 | Update examples and board files to support Sharp128 Display as the default (was Sharp96) |
TIRTOS-1430 | Call pthread_exit() in run stub to handle termination sequence |
TIRTOS-1140 | Add MSP432E Secure HTTP Client example |
TIRTOS-1016 | examplesgen – revise the process of importing examples to IAR |
TIDRIVERS-1687 | Add CAN TI-Driver for MSP432E4 SDK |
TIDRIVERS-1421 | SPI drivers for MSP432E and CC13X2/CC26X2 should use the DMA driver in ping-pong mode |
Bugs Resolved
ID | Summary |
---|---|
TIRTOS-1550 | The main_tirtos.c file in many examples has flawed logic |
TIRTOS-1528 | time() should be implemented in posix for FreeRTOS |
TIRTOS-1522 | calloc() in FreeRTOS posix compiles into an infinite loop in GCC with -O2 |
TIRTOS-1512 | pthread key data destructor never invoked [FreeRTOS] |
TIDRIVERS-1805 | Calling clock_settime delayed from init in FreeRTOS can cause error when clock_gettime is used |
TIDRIVERS-1712 | I2CMSP432E4 improperly transmits I2C master code in high-speed mode |
TIDRIVERS-1696 | UART flow control not working for MSP432E4 and CC32XX |
TIDRIVERS-1681 | NVSSPI25X_close() does not wait for the external flash to be ready |
TIDRIVERS-1649 | UART driver has a race condition in callback mode |
TIDRIVERS-1604 | Clock timeout value lost after first run of clock function [FreeRTOS] |
Core SDK 3.60.00 (May 24 2018)
New Features
ID | Summary |
---|---|
TIRTOS-1493 | Add ENFILE to errno |
TIRTOS-1451 | Increase buffer size of udpecho example |
TIDRIVERS-1578 | ADCBufMSP432E4 sysconfig must generate Board_ADCBUFXCHANNELX |
TIDRIVERS-1450 | SPI drivers need to support NOTCONNECTED option for unused pins |
TIDRIVERS-1443 | Support 3.3Mbps I2C bit rate for MSP432E4 |
Bugs Resolved
ID | Summary |
---|---|
TIRTOS-1508 | Align default pthread stack size for all kernels |
TIRTOS-1506 | Python 3-requiring example scripts should provide better error msg for python 2 users |
TIRTOS-1436 | Thread handle set too late in pthread_create() [FreeRTOS] |
TIRTOS-1433 | Clock period ignored when calling ClockP_create() [FreeRTOS] |
TIRTOS-1432 | Clock start flag and period are ignored when calling ClockP_create() |
TIRTOS-1429 | Deadlock risk in _pthread_removeThreadKeys() [SYS/BIOS] |
TIDRIVERS-1591 | UART drivers stack usage in callback mode |
TIDRIVERS-1565 | ClockP_create() for FreeRTOS does not support a period of 0 |
TIDRIVERS-1563 | SPI driver for MSP432E4 does not wait for the Busy status to clear before disabling the controller |
TIDRIVERS-1485 | The scheduler cannot be called from inside a HwiP_disable in a task context |
TIDRIVERS-1475 | Period calculation in PWM drivers (CC32XX, MSP432, MSP432E4) are off by 1 |
TIDRIVERS-1472 | ADCBufMSP432E4 is hardcoded to use TIMER1_BASE |
TIDRIVERS-1441 | ClockP_usleep() for FreeRTOS calculates delay incorrectly |
Core SDK 3.50.01 (Mar 10 2018)
New Features
ID | Summary |
---|---|
TIDRIVERS-1470 | Add TimerMSP432E4_allocateTimerResource/TimerMSP432E4_freeTimerResource to ADCBufMSP432E4 driver |
TIDRIVERS-1322 | Add MSP432E4 support to Timer TI Driver |
Bugs Resolved
ID | Summary |
---|---|
TIDRIVERS-1472 | ADCBufMSP432E4 is hardcoded to use TIMER1_BASE |
Core SDK 3.50.00 (Feb 22 2018)
New Features
ID | Summary |
---|---|
TIRTOS-1421 | Update FreeRTOSConfig.h assorted files to use v10 license |
TIRTOS-1377 | Update Core SDK products to use FreeRTOS version 10 |
TIRTOS-1368 | FreeRTOS/POSIX clock_gettime() needs to be updated for FreeRTOS v10.0 |
TIRTOS-337 | Convert tcpecho/udpecho host-side utilities to python |
TIDRIVERS-1415 | Extend NVSMSP432E4 to be able to write bytes for use with SPIFFS |
TIDRIVERS-1402 | Support 1Mbps I2C bitrate for capable devices |
TIDRIVERS-1310 | Extend the NVS driver example to show how to add a custom region |
TIDRIVERS-1232 | Add MSP432E4 support to ADCBuf TI-Driver |
TIDRIVERS-1231 | Add MSP432E4 support to ADC TI-Driver |
TIDRIVERS-1036 | Port ADCBuf driver to MSP432E |
TIDRIVERS-1035 | Port ADC driver to MSP432E |
TIDRIVERS-591 | TI-DRIVERS should upgrade to FatFs v0.13a |
TIDRIVERS-441 | Add SPIFFS, a lightweight file system that uses NVS to interface with on-chip or off-chip FLASH |
Bugs Resolved
ID | Summary |
---|---|
TIRTOS-1346 | Incorrect thread protection in removeThreadKeys() [FreeRTOS] |
TIRTOS-1337 | Dereference of freed memory in pthread_join() [FreeRTOS] |
TIRTOS-1336 | pthread_detach() needs thread protection [FreeRTOS] |
TIRTOS-1335 | Memory leak in pthread_create() on FreeRTOS |
TIRTOS-1319 | Incorrect thread protection in mq_open() |
TIRTOS-1023 | pthread_exit-related memory leak |
TIDRIVERS-1413 | ADCMSP432P/E drivers globalSemaphore should be created in init() |
TIDRIVERS-1325 | I2CMSP432E4.h missing PR4 & PR5 pin definitions |
Core SDK 3.40.00 (Nov 20 2017)
New Features
ID | Summary |
---|---|
TIRTOS-1312 | Update POSIX pthread support to show ‘fxn’ in UIA execution graph |
TIDRIVERS-1280 | UART drivers should have error function in HwAttrs |
TIDRIVERS-1183 | Improve RAM footprint of No-RTOS HwiP dispatch table |
TIDRIVERS-856 | Add support in MSP432P4 ADCBuf Driver for Internal Sources - Battery Monitor and Temperature Sensor (see adcInternalSource in ADCBufMSP432_HWAttrs for more details) |
TIDRIVERS-704 | Convert SDSPI implementations to use SDFatFS interface |
Bugs Resolved
ID | Summary |
---|---|
TIRTOS-1345 | Timed functions expecting abstime on CLOCK_REALTIME are broken |
TIRTOS-1280 | POSIX barrier broken on FreeRTOS |
TIDRIVERS-1284 | NoRTOS SemaphoreP_post can permanently disable power policy |
TIDRIVERS-1225 | NVS drivers pre-erase 2 sectors when write is equal to sector size |
Core SDK 3.35.00 (Oct 12 2017)
New Features
First Release.