Network Services 2.30.00.10 Release Notes
Table of Contents
Introduction
The Network Services Component is a portable networking API that abstracts different network stacks found on TI devices. A BSD/POSIX socket API is provided as well.
Network Services also includes a SNTP client, HTTP 1.x client, MQTT client/server, and JSON parser/builder.
Documentation
The following documentation is provided with this release.
What’s New
2.30.00.10
Defects
The following Defects were resolved
ID | Summary |
---|---|
NS-136 | accept() should return ENFILE when no more sockets available |
NS-135 | SlNetUtils_getHostByName() can fail when searching multiple interfaces |
NS-133 | Internal symbol to HTTPClient.c should be made static |
NS-130 | inet_ntop() should expect/accept addresses in network byte order |
NS-128 | Enable HTTPClient to send custom headers in HTTP requests |
NS-126 | Memory Leak in the JSON lib |
NS-125 | Closing secure sockets causes a memory leak |
NS-118 | getaddrinfo: IPv6 DNS resolution failure eclipses prior IPv4 DNS success |
NS-104 | Add getaddrinfo() and freeaddrinfo() |
NS-94 | getaddrinfo() doesn't support family type AF_INET6 |
Enhancements
The following Enhancements were resolved
ID | Summary |
---|---|
NS-78 | Add gai_strerror() |
Upgrade and Compatibility Information
The Network Services Modules have been “rebooted” to improve alignment across TI’s various networking stacks. As a result, NS 2.x is completely incompatible with NS 1.x releases, and there are currently gaps between the features available in NS 1.x and 2.x.
Host Support
- Windows
- Linux
- Mac
Device Support
This release supports the following devices/platforms:
- MSP432E4
- CC3220
Validation Information
Network Services product was validated for the following platforms.
- SimpleLink MSP432E4 LaunchPad
- SimpleLink WiFi CC3220SF LaunchPad
Known Issues
- The Network Services Component is still fairly new, and there remains an expectation that issues will be found requiring minor API evolutions in the next few releases before stabilizing. We don’t expect significant changes, but it is likely there may be a few compatibility breaks. Please report issues on the TI E2E forums.
Versioning
All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 2.10.00.00_eng).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Technical Support
Last updated: 2018-05-21