MSP432E4 USB Library Release Notes
Introduction
The Texas Instrument USB Library is a set of data types and functions for creating USB device, host or On-The-Go (OTG) applications.
This is 1.00.00.01 version of the MSP432E4 USB Library.
Documentation
What’s New
- Implemented USB Library files and examples for the following:
- CDC Serial Host
- Single CDC Serial Device
- HID Temperature Sensor Device
- HID Mouse Device
- Java based HIDDemo tool for communicating with HID Temperature Device
- Updated documentation
History
- SDK version 1.60.00.10
- Implemented USB Library for MSP432E4 Devices
- RTOS and No RTOS examples showcasing USB Library features
- User’s Guide describing how to use the library
- API Guide showing all APIs provided in the library
Upgrade and Compatibility Information
No code compatibility breaks since only new library files and examples added. Existing library files and examples should still work without issues.
Host Support
- Windows 7, Windows 8, Windows 10
- Ubuntu 14.04 64-bit, Ubuntu 16.04 64-bit
- macOS Sierra
Dependencies
This release requires the following other software components and tools.
- CCS 7.3.0
- TI Code Generation Tools
- ARM version 16.9.4.LTS or later
- GNU Code Generation Tools
- ARM gcc-arm-none-eabi-6-2017-q1-update
- IAR Code Generation Tools
- ARM 8.11.3
- Keil uVision
- 5.23
- TexasInstruments.MSP432E4_DFP.3.2.0.pack
Device Support
- MSP432E401Y
- MSP432E411Y
Known Issues
No known issues.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.