85 #ifndef ti_drivers_watchdog_WatchdogMSP432E4__include 86 #define ti_drivers_watchdog_WatchdogMSP432E4__include uint32_t intNum
Definition: WatchdogMSP432E4.h:165
Watchdog driver interface.
Watchdog hardware attributes for MSP432E4.
Definition: WatchdogMSP432E4.h:163
uint32_t intPriority
Definition: WatchdogMSP432E4.h:166
const Watchdog_FxnTable WatchdogMSP432E4_fxnTable
Watchdog function table for MSP432E4.
uint32_t baseAddr
Definition: WatchdogMSP432E4.h:164
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:346
uint32_t reloadValue
Definition: WatchdogMSP432E4.h:167
struct WatchdogMSP432E4_HWAttrs WatchdogMSP432E4_HWAttrs
Watchdog hardware attributes for MSP432E4.
bool isOpen
Definition: WatchdogMSP432E4.h:176
Watchdog Object for MSP432E4.
Definition: WatchdogMSP432E4.h:175
struct WatchdogMSP432E4_Object WatchdogMSP432E4_Object
Watchdog Object for MSP432E4.