66 #ifndef ti_drivers_sd_SDSPI__include 67 #define ti_drivers_sd_SDSPI__include uint_least8_t spiIndex
Definition: SDSPI.h:104
uint16_t spiCsGpioIndex
Definition: SDSPI.h:105
SPI_Handle spiHandle
Definition: SDSPI.h:115
SDSPI Object.
Definition: SDSPI.h:113
struct SDSPI_HWAttrs_ SDSPI_HWAttrs
SPI Global configuration.
Definition: SPI.h:706
The definition of a SD function table that contains the required set of functions to control a specif...
Definition: SD.h:266
enum SD_CardType_ SD_CardType
SD Card type inserted.
const SD_FxnTable SDSPI_fxnTable
SemaphoreP_Handle lockSem
Definition: SDSPI.h:114
SD_CardType cardType
Definition: SDSPI.h:116
struct SDSPI_Object_ SDSPI_Object
SDSPI Object.
bool isOpen
Definition: SDSPI.h:117