I2C.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2017, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!*****************************************************************************
33  * @file I2C.h
34  *
35  * @brief I2C driver interface
36  *
37  * The I2C driver interface provides device independent APIs, data types,
38  * and macros. The I2C header file should be included in an application as
39  * follows:
40  * @code
41  * #include <ti/drivers/I2C.h>
42  * @endcode
43  *
44  * # Overview #
45  * This section assumes that you have background knowledge and understanding
46  * about how the I2C protocol operates. For the full I2C specifications and
47  * user manual (UM10204), see the NXP Semiconductors website.
48  *
49  * The I2C driver has been designed to operate as a single I2C master by
50  * performing I2C transactions between the target and I2C slave peripherals.
51  * The I2C driver does not support I2C slave mode.
52  * I2C is a communication protocol - the specifications define how data
53  * transactions are to occur via the I2C bus. The specifications do not
54  * define how data is to be formatted or handled, allowing for flexible
55  * implementations across different peripheral vendors. As a result, the
56  * I2C handles only the exchange of data (or transactions) between master
57  * and slaves. It is the left to the application to interpret and
58  * manipulate the contents of each specific I2C peripheral.
59  *
60  * The I2C driver has been designed to operate in an RTOS environment. It
61  * protects its transactions with OS primitives supplied by the underlying
62  * RTOS.
63  *
64  * # Usage #
65  *
66  * The I2C driver includes the following APIs:
67  * - I2C_init(): Initialize the I2C driver.
68  * - I2C_Params_init(): Initialize an #I2C_Params structure with default
69  * vaules.
70  * - I2C_open(): Open an instance of the I2C driver.
71  * - I2C_control(): Performs implemenation-specific features on a given
72  * I2C peripheral.
73  * - I2C_transfer(): Transfer the data.
74  * - I2C_close(): De-initialize the I2C instance.
75  *
76  *
77  * ### I2C Driver Configuration #
78  *
79  * In order to use the I2C APIs, the application is required
80  * to provide device-specific I2C configuration in the Board.c file.
81  * The I2C driver interface defines a configuration data structure:
82  *
83  * @code
84  * typedef struct I2C_Config_ {
85  * I2C_FxnTable const *fxnTablePtr;
86  * void *object;
87  * void const *hwAttrs;
88  * } I2C_Config;
89  * @endcode
90  *
91  * The application must declare an array of I2C_Config elements, named
92  * I2C_config[]. Each element of I2C_config[] must be populated with
93  * pointers to a device specific I2C driver implementation's function
94  * table, driver object, and hardware attributes. The hardware attributes
95  * define properties such as the I2C peripheral's base address and
96  * pins. Each element in I2C_config[] corresponds to
97  * an I2C instance, and none of the elements should have NULL pointers.
98  * There is no correlation between the index and the
99  * peripheral designation (such as I2C0 or I2C1). For example, it is
100  * possible to use I2C_config[0] for I2C1.
101  *
102  * Because the I2C configuration is very device dependent, you will need to
103  * check the doxygen for the device specific I2C implementation. There you
104  * will find a description of the I2C hardware attributes. Please also
105  * refer to the Board.c file of any of your examples to see the I2C
106  * configuration.
107  *
108  * ### Initializing the I2C Driver #
109  *
110  * I2C_init() must be called before any other I2C APIs. This function
111  * iterates through the elements of the I2C_config[] array, calling
112  * the element's device implementation I2C initialization function.
113  *
114  * ### I2C Parameters
115  *
116  * The #I2C_Params structure is passed to the I2C_open() call. If NULL
117  * is passed for the parameters, I2C_open() uses default parameters.
118  * An #I2C_Params structure is initialized with default values by passing
119  * it to I2C_Params_init().
120  * Some of the I2C parameters are described below. To see brief descriptions
121  * of all the parameters, see #I2C_Params.
122  *
123  * #### I2C Transfer Mode
124  * The I2C driver supports two transfer modes of operation: blocking and
125  * callback:
126  * - #I2C_MODE_BLOCKING: The call to I2C_transfer() blocks until the
127  * transfer completes.
128  * - #I2C_MODE_CALLBACK: The call to I2C_transfer() returns immediately.
129  * When the transfer completes, the I2C driver will call a user-
130  * specified callback function.
131  *
132  * The transfer mode is determined by the #I2C_Params.transferMode parameter
133  * passed to I2C_open(). The I2C driver defaults to blocking mode, if the
134  * application does not set it.
135  *
136  * In blocking mode, a task calling I2C_transfer() is blocked until the
137  * transaction completes. Other tasks requesting I2C transactions while
138  * a transaction is currently taking place, are also placed into a
139  * blocked state.
140  *
141  * In callback mode, an I2C_transfer() functions asynchronously, which
142  * means that it does not block a calling task's execution. In this
143  * mode, the user must set #I2C_Params.transferCallbackFxn to a user-
144  * provided callback function. After an I2C transaction has completed,
145  * the I2C driver calls the user- provided callback function.
146  * If another I2C transaction is requested, the transaction is queued up.
147  * As each transfer completes, the I2C driver will call the user-specified
148  * callback function. The user callback will be called from either hardware
149  * or software interrupt context, depending upon the device implementation.
150  *
151  * Once an I2C driver instance is opened, the
152  * only way to change the transfer mode is to close and re-open the I2C
153  * instance with the new transfer mode.
154  *
155  * #### Specifying an I2C Bus Frequency
156  * The I2C controller's bus frequency is determined by #I2C_Params.bitRate
157  * passed to I2C_open(). The standard I2C bus frequencies are 100 kHz and
158  * 400 kHz, with 100 kHz being the default.
159  *
160  * ### Opening the I2C Driver #
161  * After initializing the I2C driver by calling I2C_init(), the application
162  * can open an I2C instance by calling I2C_open(). This function
163  * takes an index into the I2C_config[] array and an I2C parameters data
164  * structure. The I2C instance is specified by the index of the I2C in
165  * I2C_config[]. Only one I2C index can be used at a time;
166  * calling I2C_open() a second time with the same index previosly
167  * passed to I2C_open() will result in an error. You can,
168  * though, re-use the index if the instance is closed via I2C_close().
169  *
170  * If no I2C_Params structure is passed to I2C_open(), default values are
171  * used. If the open call is successful, it returns a non-NULL value.
172  *
173  * Example opening an I2C driver instance in blocking mode:
174  * @code
175  * I2C_Handle i2c;
176  *
177  * // NULL params are used, so default to blocking mode, 100 KHz
178  * i2c = I2C_open(Board_I2C0, NULL);
179  *
180  * if (!i2c) {
181  * // Error opening the I2C
182  * }
183  * @endcode
184  *
185  * Example opening an I2C driver instance in callback mode and 400KHz bit rate:
186  *
187  * @code
188  * I2C_Handle i2c;
189  * I2C_Params params;
190  *
191  * I2C_Params_init(&params);
192  * params.transferMode = I2C_MODE_CALLBACK;
193  * params.transferCallbackFxn = myCallbackFunction;
194  * params.bitRate = I2C_400kHz;
195  *
196  * handle = I2C_open(Board_I2C0, &params);
197  * if (!i2c) {
198  * // Error opening I2C
199  * }
200  * @endcode
201  *
202  * ### Transferring data #
203  * An I2C transaction with an I2C peripheral is started by calling
204  * I2C_transfer(). Three types of transactions are supported: Write, Read,
205  * or Write/Read. Each transfer is completed before another transfer is
206  * initiated.
207  *
208  * For Write/Read transactions, the specified data is first written to the
209  * peripheral, then a repeated start is sent by the driver, which initiates
210  * the read operation. This type of transfer is useful if an I2C peripheral
211  * has a pointer register that needs to be adjusted prior to reading from
212  * the referenced data register.
213  *
214  * The details of each transaction are specified with an #I2C_Transaction data
215  * structure. This structure defines the slave I2C address, pointers
216  * to write and read buffers, and their associated byte counts. If
217  * no data needs to be written or read, the corresponding byte counts should
218  * be set to zero.
219  *
220  * If an I2C transaction is requested while a transaction is currently
221  * taking place, the new transaction is placed onto a queue to be processed
222  * in the order in which it was received.
223  *
224  * The below example shows sending three bytes of data to a slave peripheral
225  * at address 0x50, in blocking mode:
226  *
227  * @code
228  * unsigned char writeBuffer[3];
229  * I2C_Transaction i2cTransaction;
230  *
231  * i2cTransaction.slaveAddress = 0x50;
232  * i2cTransaction.writeBuf = writeBuffer;
233  * i2cTransaction.writeCount = 3;
234  * i2cTransaction.readBuf = NULL;
235  * i2cTransaction.readCount = 0;
236  *
237  * status = I2C_transfer(i2c, &i2cTransaction);
238  * if (!status) {
239  * // Unsuccessful I2C transfer
240  * }
241  * @endcode
242  *
243  * The next example shows reading of five bytes of data from the I2C
244  * peripheral, also in blocking mode:
245  *
246  * @code
247  * unsigned char readBuffer[5];
248  * I2C_Transaction i2cTransaction;
249  *
250  * i2cTransaction.slaveAddress = 0x50;
251  * i2cTransaction.writeBuf = NULL;
252  * i2cTransaction.writeCount = 0;
253  * i2cTransaction.readBuf = readBuffer;
254  * i2cTransaction.readCount = 5;
255  *
256  * status = I2C_transfer(i2c, &i2cTransaction);
257  * if (!status) {
258  * // Unsuccessful I2C transfer
259  * }
260  * @endcode
261  *
262  * This example shows writing of two bytes and reading of four bytes in a
263  * single transaction.
264  *
265  * @code
266  * unsigned char readBuffer[4];
267  * unsigned char writeBuffer[2];
268  * I2C_Transaction i2cTransaction;
269  *
270  * i2cTransaction.slaveAddress = 0x50;
271  * i2cTransaction.writeBuf = writeBuffer;
272  * i2cTransaction.writeCount = 2;
273  * i2cTransaction.readBuf = readBuffer;
274  * i2cTransaction.readCount = 4;
275  *
276  * status = I2C_transfer(i2c, &i2cTransaction);
277  * if (!status) {
278  * // Unsuccessful I2C transfer
279  * }
280  * @endcode
281  *
282  * This final example shows usage of asynchronous callback mode, with queuing
283  * of multiple transactions. Because multiple transactions are simultaneously
284  * queued, separate I2C_Transaction structures must be used. (This is a
285  * general rule, that I2C_Transaction structures cannot be reused until
286  * it is known that the previous transaction has completed.)
287  *
288  * First, for the callback function (that is specified in the I2C_open() call)
289  * the "arg" in the I2C_Transaction structure is a semaphore handle. When
290  * this value is non-NULL, sem_post() is called in the callback using
291  * the specified handle, to signal completion to the task that queued the
292  * transactions:
293  *
294  * @code
295  * Void callbackFxn(I2C_Handle handle, I2C_Transaction *msg, Bool transfer) {
296  * if (msg->arg != NULL) {
297  * sem_post((sem_t *)(msg->arg));
298  * }
299  * }
300  * @endcode
301  *
302  * Snippets of the task code that initiates the transactions are shown below.
303  * Note the use of multiple I2C_Transaction structures, and passing of the
304  * handle of the semaphore to be posted via i2cTransaction2.arg.
305  * I2C_transfer() is called three times to initiate each transaction.
306  * Since callback mode is used, these functions return immediately. After
307  * the transactions have been queued, other work can be done, and then
308  * eventually sem_wait() is called to wait for the last I2C
309  * transaction to complete. Once the callback posts the semaphore the task
310  * will be moved to the ready state, so the task can resume execution.
311  *
312  * @code
313  * Void taskfxn(arg0, arg1) {
314  *
315  * I2C_Transaction i2cTransaction0;
316  * I2C_Transaction i2cTransaction1;
317  * I2C_Transaction i2cTransaction2;
318  *
319  * ...
320  * i2cTransaction0.arg = NULL;
321  * i2cTransaction1.arg = NULL;
322  * i2cTransaction2.arg = semaphoreHandle;
323  *
324  * ...
325  * I2C_transfer(i2c, &i2cTransaction0);
326  * I2C_transfer(i2c, &i2cTransaction1);
327  * I2C_transfer(i2c, &i2cTransaction2);
328  *
329  * ...
330  *
331  * sem_wait(semaphoreHandle);
332  *
333  * ...
334  * }
335  * @endcode
336  *
337  * # Implementation #
338  *
339  * This top-level I2C module serves as the main interface for RTOS
340  * applications. Its purpose is to redirect the module's APIs to specific
341  * peripheral implementations which are specified using a pointer to an
342  * #I2C_FxnTable.
343  *
344  * The I2C driver interface module is joined (at link time) to an
345  * array of I2C_Config data structures named *I2C_config*.
346  * *I2C_config* is typically defined in the Board.c file used for the
347  * application. If there are multiple instances of I2C peripherals on the
348  * device, there will typically be multiple I2C_Config structures defined in
349  * the board file. Each entry in *I2C_config* contains a:
350  * - (I2C_FxnTable *) to a set of functions that implement a I2C peripheral
351  * - (void *) data object that is associated with the I2C_FxnTable
352  * - (void *) hardware attributes that are associated to the I2C_FxnTable
353  *
354  *******************************************************************************
355  */
356 
357 #ifndef ti_drivers_I2C__include
358 #define ti_drivers_I2C__include
359 
360 #ifdef __cplusplus
361 extern "C" {
362 #endif
363 
364 #include <stdbool.h>
365 #include <stddef.h>
366 #include <stdint.h>
367 
385 #define I2C_CMD_RESERVED (32)
386 
399 #define I2C_STATUS_RESERVED (-32)
400 
414 #define I2C_STATUS_SUCCESS (0)
415 
422 #define I2C_STATUS_ERROR (-1)
423 
431 #define I2C_STATUS_UNDEFINEDCMD (-2)
432 
442 /* Add I2C_CMD_<commands> here */
443 
451 typedef struct I2C_Config_ *I2C_Handle;
452 
464 typedef struct I2C_Transaction_ {
465  void *writeBuf;
466  size_t writeCount;
468  void *readBuf;
469  size_t readCount;
471  uint_least8_t slaveAddress;
473  void *arg;
474  void *nextPtr;
476 
485 typedef enum I2C_TransferMode_ {
489 
506 typedef void (*I2C_CallbackFxn)(I2C_Handle handle, I2C_Transaction *transaction,
507  bool transferStatus);
508 
515 typedef enum I2C_BitRate_ {
518 } I2C_BitRate;
519 
542 typedef struct I2C_Params_ {
543  I2C_TransferMode transferMode;
546  void *custom;
548 } I2C_Params;
549 
554 typedef void (*I2C_CancelFxn) (I2C_Handle handle);
555 
560 typedef void (*I2C_CloseFxn) (I2C_Handle handle);
561 
566 typedef int_fast16_t (*I2C_ControlFxn) (I2C_Handle handle, uint_fast16_t cmd,
567  void *controlArg);
568 
573 typedef void (*I2C_InitFxn) (I2C_Handle handle);
574 
579 typedef I2C_Handle (*I2C_OpenFxn) (I2C_Handle handle, I2C_Params *params);
580 
585 typedef bool (*I2C_TransferFxn) (I2C_Handle handle,
586  I2C_Transaction *transaction);
587 
593 typedef struct I2C_FxnTable_ {
596 
599 
602 
605 
608 
611 } I2C_FxnTable;
612 
624 typedef struct I2C_Config_ {
627 
629  void *object;
630 
632  void const *hwAttrs;
633 } I2C_Config;
634 
655 extern void I2C_cancel(I2C_Handle handle);
656 
666 extern void I2C_close(I2C_Handle handle);
667 
705 extern int_fast16_t I2C_control(I2C_Handle handle, uint_fast16_t cmd,
706  void *controlArg);
707 
716 extern void I2C_init(void);
717 
739 extern I2C_Handle I2C_open(uint_least8_t index, I2C_Params *params);
740 
752 extern void I2C_Params_init(I2C_Params *params);
753 
805 extern bool I2C_transfer(I2C_Handle handle, I2C_Transaction *transaction);
806 
807 #ifdef __cplusplus
808 }
809 #endif
810 
811 #endif /* ti_drivers_I2C__include */
I2C Parameters.
Definition: I2C.h:542
size_t readCount
Definition: I2C.h:469
I2C transaction.
Definition: I2C.h:464
I2C_BitRate_
I2C bitRate.
Definition: I2C.h:515
void * object
Definition: I2C.h:629
I2C_OpenFxn openFxn
Definition: I2C.h:607
void I2C_Params_init(I2C_Params *params)
Initialize an I2C_Params struct to its defaults.
void(* I2C_CloseFxn)(I2C_Handle handle)
A function pointer to a driver-specific implementation of I2C_close().
Definition: I2C.h:560
void * nextPtr
Definition: I2C.h:474
I2C_TransferMode transferMode
Definition: I2C.h:543
void(* I2C_InitFxn)(I2C_Handle handle)
A function pointer to a driver-specific implementation of I2C_init().
Definition: I2C.h:573
struct I2C_Transaction_ I2C_Transaction
I2C transaction.
struct I2C_Config_ * I2C_Handle
A handle that is returned from an I2C_open() call.
Definition: I2C.h:451
size_t writeCount
Definition: I2C.h:466
void const * hwAttrs
Definition: I2C.h:632
int_fast16_t I2C_control(I2C_Handle handle, uint_fast16_t cmd, void *controlArg)
Perform implementation-specific features on a given I2C_Handle.
Definition: I2C.h:516
I2C_CloseFxn closeFxn
Definition: I2C.h:598
void(* I2C_CancelFxn)(I2C_Handle handle)
A function pointer to a driver-specific implementation of I2C_cancel().
Definition: I2C.h:554
struct I2C_Params_ I2C_Params
I2C Parameters.
void * readBuf
Definition: I2C.h:468
I2C_InitFxn initFxn
Definition: I2C.h:604
I2C_CancelFxn cancelFxn
Definition: I2C.h:595
I2C_TransferMode_
I2C transfer mode.
Definition: I2C.h:485
enum I2C_TransferMode_ I2C_TransferMode
I2C transfer mode.
I2C_CallbackFxn transferCallbackFxn
Definition: I2C.h:544
bool(* I2C_TransferFxn)(I2C_Handle handle, I2C_Transaction *transaction)
A function pointer to a driver-specific implementation of I2C_transfer().
Definition: I2C.h:585
I2C_Handle I2C_open(uint_least8_t index, I2C_Params *params)
Initialize a given I2C peripheral as identified by an index value. The I2C_Params structure defines t...
The definition of an I2C function table that contains the required set of functions to control a spec...
Definition: I2C.h:593
struct I2C_FxnTable_ I2C_FxnTable
The definition of an I2C function table that contains the required set of functions to control a spec...
enum I2C_BitRate_ I2C_BitRate
I2C bitRate.
void I2C_close(I2C_Handle handle)
Close an I2C peripheral specified by an I2C_Handle.
I2C_BitRate bitRate
Definition: I2C.h:545
Definition: I2C.h:487
void * writeBuf
Definition: I2C.h:465
struct I2C_Config_ I2C_Config
I2C global configuration.
Definition: I2C.h:517
void I2C_cancel(I2C_Handle handle)
Cancel all I2C transfers.
void * arg
Definition: I2C.h:473
uint_least8_t slaveAddress
Definition: I2C.h:471
I2C global configuration.
Definition: I2C.h:624
void(* I2C_CallbackFxn)(I2C_Handle handle, I2C_Transaction *transaction, bool transferStatus)
I2C callback function.
Definition: I2C.h:506
void I2C_init(void)
Initializes the I2C module.
I2C_FxnTable const * fxnTablePtr
Definition: I2C.h:626
void * custom
Definition: I2C.h:546
bool I2C_transfer(I2C_Handle handle, I2C_Transaction *transaction)
Perform an I2C transaction with an I2C slave peripheral.
int_fast16_t(* I2C_ControlFxn)(I2C_Handle handle, uint_fast16_t cmd, void *controlArg)
A function pointer to a driver-specific implementation of I2C_control().
Definition: I2C.h:566
I2C_ControlFxn controlFxn
Definition: I2C.h:601
I2C_Handle(* I2C_OpenFxn)(I2C_Handle handle, I2C_Params *params)
A function pointer to a driver-specific implementation of I2C_open().
Definition: I2C.h:579
I2C_TransferFxn transferFxn
Definition: I2C.h:610
Definition: I2C.h:486
Copyright 2017, Texas Instruments Incorporated