Release Notes
Table of Contents
Introduction
This is a GA release of the Core SDK 3.40.01.02 for MSP432E4 devices.
Documentation
Open the documentation overview web page file in the SDK’s Doc folder for a full list of documentation.
What’s New
- This release updates to the newest code gen tools. See the Validation Information section for details on what versions of each code gen tools was used to test this release.
New Features
ID | Summary |
---|---|
TIRTOS-1312 | Update POSIX pthread support to show ‘fxn’ in UIA execution graph |
TIDRIVERS-1280 | UART drivers should have error function in HwAttrs |
TIDRIVERS-1183 | Improve RAM footprint of No-RTOS HwiP dispatch table |
TIDRIVERS-856 | Add support in MSP432P4 ADCBuf Driver for Internal Sources - Battery Monitor and Temperature Sensor (see adcInternalSource in ADCBufMSP432_HWAttrs for more details) |
TIDRIVERS-704 | Convert SDSPI implementations to use SDFatFS interface |
Bugs Resolved
ID | Summary |
---|---|
TIRTOS-1345 | Timed functions expecting abstime on CLOCK_REALTIME are broken |
TIRTOS-1280 | POSIX barrier broken on FreeRTOS |
TIDRIVERS-1284 | NoRTOS SemaphoreP_post can permanently disable power policy |
TIDRIVERS-1225 | NVS drivers pre-erase 2 sectors when write is equal to sector size |
Upgrade and Compatibility Information
This release breaks compatibility with previous releases of the Core SDK in the following ways:
- Please see the Network Services (NS) and Network Developers Kit (NDK) components’ release notes for their respective updates on any compatibility breaks.
Host Support
See the SDK release notes for a description of which host operating systems are supported in this release.
Dependencies
See the SDK release notes for a description of which components and tools are required to work with this product.
Device Support
See the SDK release notes for a list of TI devices that are supported in this product.
Validation Information
The Core SDK was validated with the following components:
- Code Composer Studio 7.4.0
- ARM 16.9.6.LTS
- GNU Code Generation Tools
- gcc-arm-none-eabi-6-2017-q1-update
- IAR Code Generation Tools
- ARM 8.11.4
- FreeRTOS 9.0.0
- XDCTools 3.50.04
Known Issues
ID | Summary |
---|---|
TIRTOS-476 | POSIX threads render as single task in execution graph |
TIDRIVERS-1267 | MSP432E4 PWM driver always inserts one full period of ‘high’ before beginning duty cycle. |
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
Core SDK 3.35.00 (Oct 12 2017)
New Features
First Release.