Release Notes

Table of Contents

Introduction

This is a GA release of the Core SDK 3.35.00.13 for MSP432E4 devices.

Documentation

Open the documentation overview web page file in the SDK’s Doc folder for a full list of documentation.

What’s New

New Features

ID Summary
None None

Bugs Resolved

ID Summary
None None

Upgrade and Compatibility Information

This release breaks compatibility with previous releases of the Core SDK in the following ways: None

Host Support

See the SDK release notes for a description of which host operating systems are supported in this release.

Dependencies

See the SDK release notes for a description of which components and tools are required to work with this product.

Device Support

See the SDK release notes for a list of TI devices that are supported in this product.

Validation Information

The Core SDK was validated with the following components:

Known Issues

ID Summary
TIRTOS-1280 POSIX barrier broken on FreeRTOS
TIRTOS-476 POSIX threads render as single task in execution graph

Versioning

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

Prior Release Changes

None