Network Services 2.00.00.16 Release Notes

Table of Contents

Introduction

The Network Services product is a portable networking API that abstracts different network stacks found on TI devices. A BSD/POSIX socket API is provided as well.

Future releases intend to add support for application layer networking protocols, such as HTTP/1.1, HTTP/2 and SNTP clients.

Documentation

The following documentation is provided with this release.

What’s New

2.00.00.16

Defects

The following Defects were resolved

ID Summary
NS-47 Add debug/release libraries support to NS product

Enhancements

The following Enhancements were resolved

ID Summary
NS-74 Introduce SlNetSock abstraction over network and TLS stacks

Upgrade and Compatibility Information

The Network Services Modules are being “rebooted” to improve alignment across TI’s various networking stacks. As a result, NS 2.x is completely incompatible with NS 1.x releases, and there are currently gaps between the features available in NS 1.x and 2.x.

We will be continuing to add features to NS 2.x, including HTTP/SNTP clients, and others, using the portable SlNetSock APIs so consistent APIs and features will be available a family of TI devices.

Host Support

Dependencies

This release requires the following software components and tools versions to successfully function:

Pre-built binaries were built with the following toolchains:

Required Hardware

Device Support

This release supports the following devices/platforms:

Validation Information

Network Services product was validated for the following platforms using the software components mentioned in the Dependencies Section.

Known Issues

Versioning

All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.40.00.00_eng).

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. ns_2_00_00_16.

Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.

Technical Support

Last updated: 2017-10-10