Release Notes
Table of Contents
Introduction
This is a GA release of the Core SDK 4.40.00.03 for MSP432P4 devices.
Documentation
Open the documentation overview web page file in the SDK’s Doc folder for a full list of documentation.
What’s New
A summary of changes made in the current release of this product can be found in the product Change Log.
This is a maintenance release. No new features were added to this release.
Upgrade and Compatibility Information
This release breaks compatibility with previous releases of the Core SDK in the following ways:
IAR RTOS plugin .dll
The ROV tool for IAR requires an update to work properly. If you are an ROV user, follow the instructions on this forum page: https://e2e.ti.com/support/processors/f/791/t/832561. If you don’t use ROV, you can proceed with the standard debugging sessions. The ROV tool does not affect any other funcationality.
Host Support
See the SDK release notes for a description of which host operating systems are supported in this release.
Dependencies
See the SDK release notes for a description of which components and tools are required to work with this product.
Device Support
See the SDK release notes for a list of TI devices that are supported in this product.
Validation Information
The Core SDK was validated with the following components:
- Code Composer Studio 9.3.0
- ARM 18.12.4.LTS
- GNU Code Generation Tools
- ARM GCC 7-2017-q4-major
- IAR Code Generation Tools
- ARM 8.32.2
- FreeRTOS 10.1.1
- XDCTools 3.60.02
Known Issues
| ID | Summary |
|---|---|
| TIRTOS-1435 | clock_nanosleep() with CLOCK_REALTIME broken on msp432 |
| TIDRIVERS-3636 | I2C_transfer() occasionally fails when called from an interrupt context |
| TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
A summary of changes made in previous releases of this product can be found in the product Change Log