Release Notes
Table of Contents
Introduction
This is a GA release of the Core SDK 3.20.02.00 for MSP432 devices.
Documentation
Open the documentation overview web page file in the SDK’s Doc folder for a full list of documentation.
What’s New in 3.20.0x
- Added support for the drivers and examples working without an RTOS. A ‘NoRTOS’ version of the driver porting layer (DPL) was added.
- NVS API has been updated and finalized. The earlier version of NVS was tagged as “preliminary”. The API has been modified and this tag has been removed.
- Added support for MSP432P4111.
New Features in 3.20.02
None
Bugs Resolved in 3.20.02
TIDRIVERS-1136 |
NoRTOS SemaphoreP_pend should use local ClockP structure |
This release breaks compatibility with previous releases of the Core SDK in the following ways:
- GCC compiler update. This release depends on the gcc-arm-none-eabi-6-2017-q1-update tools. These tools are shipped with CCS 7.2 but also available on the Linaro site. Wiki link describing steps to migrate existing Cortex-M GCC projects to SYS/BIOS v6.51
- IAR tools update. This release depends on the IAR 8.11 Arm tools. The default size for wchar_t size changed. All files need to be recompiled with the 8.11 compiler.
- New DeviceFamily_ preprocessor constant. A new constant has been added to the projects to select a given device family. This constant is used within drivers to select the correct driverlib include files and in #ifdef blocks to manage device-specific code. Build options for existing projects that reference the driverlib header files may need to be updated to include -DDeviceFamily_XYZ on the command line. Currently supported options are:
- DeviceFamily_MSP432P401x
- DeviceFamily_MSP432P4x1
- NVS API change. The non-volatile storage (NVS) API has been formally reviewed and updated. Code that was using the “preliminary” NVS API will have to be updated to use the official API.
- DPL API change. The device porting layer (DPL) is used internally by the device drivers. Some of the DPL APIs were updated as part of the NoRTOS feature addition. Since this is an internal API, user code should not be affected.
Host Support
See the SDK release notes for a description of which host operating systems are supported in this release.
Dependencies
See the SDK release notes for a description of which components and tools are required to work with this product.
Device Support
See the SDK release notes for a list of TI devices that are supported in this product.
The Core SDK was validated with the following components:
- Code Composer Studio 7.2.0
- GNU Code Generation Tools
- gcc-arm-none-eabi-6-2017-q1-update
- IAR Code Generation Tools
- FreeRTOS 9.0.0
- XDCTools 3.50.02
Known Issues
TIRTOS-751 |
CCS does not import config project if a different version's config project is present |
TIRTOS-476 |
POSIX threads render as single task in execution graph |
TIDRIVERS-1088 |
NOLOAD directive in GNU linker script bug cause NVS FLASH buffer to get initialized |
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
Core SDK 3.20.00 (Jun 05 2017)
New Features
TIRTOS-1066 |
Set configUSE_TIME_SLICING to ‘0’ in all FreeRTOSConfig.h files |
TIRTOS-1056 |
Remove spiloopback4wiremode example |
TIRTOS-1036 |
Supply Portable example with native RTOS APIs |
TIRTOS-1009 |
Add examples for NVS for internal and external SPI FLASH when available |
TIRTOS-991 |
Optimize DPL for size |
TIRTOS-988 |
Provide all single-task driver examples also for Non-RTOS |
TIRTOS-952 |
MSP432 GCC startup files require define from GCC standard libraries |
TIRTOS-948 |
pthread_cond_timedwait should support CLOCK_MONOTONIC |
TIRTOS-644 |
Redundant FreeRTOS C stack definitions |
TIRTOS-615 |
Create example for UARTMon module |
TIDRIVERS-1008 |
Need Posix sleep and usleep for NoRTOS |
TIDRIVERS-971 |
Provide NVS driver for SPI FLASH |
TIDRIVERS-916 |
Board.html should specify pin functions for communication buses |
TIDRIVERS-900 |
Various driver pin encodings need to be explained better |
TIDRIVERS-891 |
Rename ADC_convertRawToMicroVolts to ADC_convertToMicroVolts |
TIDRIVERS-887 |
Capture Driver top level implementation review and fix |
TIDRIVERS-884 |
MSP432 TI Driver SPI 4 wire example update |
TIDRIVERS-881 |
Construct and destruct APIs for DPL |
TIDRIVERS-488 |
Review TI-RTOS SemaphoreP implementation with goal to reduce stack usage |
Bugs Resolved
TIRTOS-1031 |
FreeRTOS mq_getattr() should not disable scheduler |
TIRTOS-1027 |
i2cmsp432 does not work if write/read on same transaction |
TIRTOS-1012 |
MSP432 linker files must ALIAS SRAM_CODE & SRAM_DATA |
TIRTOS-954 |
Update ADC examples to show microvolt values |
TIRTOS-936 |
TI-RTOS examples suppress ULP warnings |
TIDRIVERS-1077 |
TimerMSP432 bug fixes (update Timer_getCount() and Timer_start()) |
TIDRIVERS-1062 |
MSP432 Timer_open should check registers to see if timer is already in use |
TIDRIVERS-1054 |
Correct the IEEE RX command definition |
TIDRIVERS-1027 |
SemaphoreP_pend for FreeRTOS does not work with tick rate less than 1 msec |
TIDRIVERS-1014 |
PWMMSP432 setPeriod() bug |
TIDRIVERS-1013 |
FreeRTOS posix mqueue.h mode_t needs to be uint32_t |
TIDRIVERS-1005 |
SemaphoreP_Params_init() should set mode to COUNTING |
TIDRIVERS-960 |
ADC14 single driver, ADCMSP432.c only supports performance levels 0 and 1 |
TIDRIVERS-934 |
Timeouts for Posix FreeRTOS need to handle wrapping |
TIDRIVERS-929 |
PowerMSP432.c has non-MAP_ function calls |
Core SDK 3.10.02 (Mar 1 2017)
New Features
None
Bugs Resolved
TIRTOS-992 |
FreeRTOS POSIX mq_send and mq_receive should be callable from ISR context |
Core SDK 3.10.01 (Feb 24 2017)
New Features
None
Bugs Resolved
TIRTOS-984 |
Update imports.mak to match components in CCSv7.1 GA |
TIRTOS-982 |
Code built on MSP432 DriverLib will run DriverLib out of flash memory instead of ROM |
Core SDK 3.10.00 (Feb 15 2017)
New Features
TIRTOS-946 |
Release.cfg should use policyMin instead of policySpin |
TIRTOS-925 |
IAR Examples.html should reference .eww and not .ipcf files any longer |
TIRTOS-849 |
Capture example needs to be replaced by CapturePWM |
TIRTOS-842 |
Need Mailbox example in the product |
TIRTOS-750 |
The CoreSDK is carrying around unnecessary files/directories |
Bugs Resolved
TIRTOS-945 |
pthread_setschedparam not supported in Freertos POSIX |
TIRTOS-933 |
CCS platform warning with TI-RTOS examples |
TIRTOS-903 |
Inconsistent declaration for timer_create, TI-RTOS and FreeRTOS |
TIRTOS-900 |
Display driver not printing float values |
TIRTOS-897 |
Makefile for FreeRTOS kernel has bad error message if FREERTOS_INSTALL_DIR is not set |
TIRTOS-891 |
RTOS build in IAR should be an .ewp and preferably a dependent project like in CCS |
TIRTOS-785 |
Board_ADCBUFCHANNEL0 should be changed to Board_ADCBUF0CHANNEL0 for consistency |
TIRTOS-776 |
Posix usleep() function implemented in millisecond and not in microseconds |
TIRTOS-749 |
C++ constructors on FreeRTOS with GCC are not called |
TIRTOS-709 |
RTOS config projects are available only in makefile for IAR |
TIRTOS-415 |
IAR tools must be installed in non-default location to work with gmake |
TIDRIVERS-890 |
exit() support is missing in gcc libraries for FreeRTOS |
TIDRIVERS-837 |
FreeRTOS Posix timer APIs need to check if in an ISR |
TIDRIVERS-745 |
Change reverse() in source\ti\mw\lcd\SharpGrLib.c to SharpGrLib_reverse() |
Core SDK 3.01.01 (Dec 9 2016)
New Features
TIRTOS-838 |
Update the IAR/Arm compiler tools to version 7.80.x |
TIRTOS-832 |
kernel examples should get stack size from linker.cmd files like driver examples |
TIRTOS-821 |
remove ‘eclipse’ directory from the product, CCSv7 needs only .metadata folder |
Bugs Resolved
TIRTOS-814 |
Update primary_heap size logic in TI and GCC linker .cmd files |
TIRTOS-606 |
Makefiles should support tools directory names that contain spaces |
TIDRIVERS-796 |
Display_getType compile error for Display_DISABLE_ALL |
Core SDK 3.01.00 (Nov 9 2016)
New Features
TIRTOS-759 |
Update TI tools to 16.9.0 to be ready for CCSv7.0 |
TIRTOS-756 |
Update examples to use Display_printf instead of print0, etc. |
TIRTOS-745 |
Display_Type_UART should disable RX to allow power savings |
TIRTOS-705 |
Power Management doc needs updating for CoreSDK |
TIRTOS-543 |
Update all Drivers examples with Display module usage as necessary |
TIRTOS-248 |
Move TI-RTOS driver documentation out of the user guide and into doxygen |
TIDRIVERS-738 |
Deprecate ti.drivers.Config as apps should supply libs on command line |
TIDRIVERS-735 |
Remove instrumented driver libraries and provide only release libraries |
TIDRIVERS-601 |
Update Power APIs for MISRA compliance |
TIDRIVERS-569 |
Update UART Display driver to function like an LCD |
Bugs Resolved
TIRTOS-552 |
Spiloopback example master/slave needs synchronization |