TI 3.2.0 Release Notes
Table of Contents
Introduction
Z-Stack 3.x is a component of the SimpleLink CC26x2 and CC13x2 SDKs. This component enables development of Zigbee 3.0 specification based products. Z-Stack is TI’s Zigbee® 3.0 compliant protocol suite for the CC26X2 and CC13X2. Z-Stack contained in this release is based on ZigBee 3.0 specification with the added benefit of running on top of TI-RTOS.
Documentation
- Z-Stack Quick Start Guide
- TI Z-Stack User’s Guide
- Z-Stack Monitor and Test API
- Z-Stack ZCL APIs
- Z-Stack Application APIs
- Z-Stack Migration Guides
What’s New
- Added CIE, IASZone, WarningDevice projects
- Added factory reset to sample apps on power up if left button is held
- Added ability to choose whether or not binds from remote devices (i.e. non-parent, non-authenticated, etc) are accepted
- Code Cleanup, removed many deprecated compile flags and unused legacy code blocks
- Enhancements to Green Power Proxy
Fixed Issues
- CC1352P-2 TX power fix
- Added Green Power Basic Proxy functionality to GenericApp projects
- BDB F&B bug regarding duplicate binding
- BDB F&B bug regarding broken when Touchlink is enabled but classical commissioning is used
- Touchlink bug regarding F&B not running when using Touchlink commissioning
- Touchlink bug regarding neighbor table entries not being populated in the nwk join callback
- Bug with IAS Zone Enroll Response payload parsing
- Bug in GPD projects that was disallowing the removal of NV_RESTORE
- Fixed some ZED power consumption corner cases upon nwk rejoin
- Fix for bug with ZED rejoin poll rate restoration
- Fixed bug in Z-Stack Application API that was incorrectly casting poll rate as a uint16_t instead of a uint32_t
- Fix for ZED consuming power prior to starting nwk commissioning (no nwk state)
- Fix for CC1352P-2 GPD apps to use the correct PA settings
- Fix for ZNP application to send MT Reset msg on power up
- Fix bug with BDB reporting not working with attributes defined as function CBs
- Fixes for GP Sink UI lockup
Known Issues
- CC26X2 and CC13X2 supports R21 Zigbee core (platform not certified yet)
- Green Power Device and Sink can only communicate with intermediate Green Power Proxy (no direct communication yet)
Upgrade and Compatibility Information
- None
Operating System Support
The TI Z-Stack is supported on the Microsoft Windows®7 SP1 or later
Dependencies
The Zigbee component of the SimpleLink CC26x2 and CC13x2 SDK was built & tested on a Windows host platform using the following Integrated Development Environments (IDEs) and components. Using an IDE or toolchain version not listed below may result in compatibility issues with this SDK release. Refer to the individual component release notes in the Document Overview for each component’s supported code generation tools.
- IAR Embedded Workbench: EWARM-8.20.2
- TI Code Composer Studio: CCS-8.2.0
- TI Code Generation Tools for ARM: 18.1.2.LTS
- XDCTools: 3.50.07.20
Device Support
Development Board Support
Validation
The Z-Stack sample applications were built & tested with versions of the following Integrated Development Environments (IDEs) and tool chains listed in the top-level SDK release notes:
- Code Composer Studio using the TI C Compiler for ARM
- IAR Embedded Workbench for ARM
This release is for evaluation and development purposes only. End products being developed with this protocol stack version will require a future update prior to obtaining Zigbee and/or regulatory certification.
Versioning
This product follows a version format, M.mm.pp.bb, where:
- M is a 1 digit major number,
- mm is a 2 digit minor number,
- pp is a 2 digit patch number,
- bb is a 2 digit incrementing build counter.