HCI Interface

HCI Overview

The HCI is a standardized Bluetooth interface for sending commands, receiving events, and for sending and receiving data. It is typically realized as a serial interface, using either RS232 or USB communication devices. As the name implies, the HCI is used to bridge the Host and Controller devices. Commands and Events can either be specified, or can be vendor specific for extensibility. The following sections summarize the HCI protocol, the specification defined commands and events used by BLE, and a detailed description of the vendor specific commands and events defined by Texas Instruments Inc. For complete details on the HCI as specified by the Special Interest Group (SIG), please see the Core specification [1].

Specification Interface

HCI Interface Protocol

The HCI supports four types of packets: Command Packet, Asynchronous Data Packet, Synchronous Data Packet, and Event Packet. The packet type is a one byte value that precedes the HCI packet. The packet type has the following values:

Packet Packet Type
Command 0x01
Asynchronous Data 0x02
Synchronous Data 0x03
Event 0x04
Extended Command 0x09

The contents of each packet are shown as follows (please see section 5.4 of [1], Vol. 2, Part E for additional details).

Command Packet

The command packet is comprised of the opcode, the number of parameters, and parameters themselves.

../_images/command-packet.png

Fig. 5 Command Packet

Asynchronous Data Packet

The asynchronous data packet is comprised of the connection handle, fragmentation bits, the number of data bytes, and the data bytes themselves.

../_images/async-data-packet.png

Fig. 6 Asynchronous Data Packet

Synchronous Data Packet

This synchronous data packet is not used in BLE.

Event Packet

The event packet is comprised of the event code, the number of event parameters, and the event parameters themselves.

../_images/event-packet.png

Fig. 7 Event Packet

Extended Command

This packet is used to allow more than the HCI limit of 256 bytes. It includes a two-byte length field which states the payload length:

Offset Description
0 packet type (0x09)
1 LSB opcode
2 MSB opcode
3 LSB payload length
4 MSB payload length
5..(length-3) Payload

See each individual command for payload formatting.

HCI Commands

HCI commands use a 16-bit opcode for identification. The opcode is subdivided into two parts: a 10-bit Opcode Command Field (OCF) and a 6-bit Opcode Group Field (OGF).

../_images/hci-command-opcode.png

Fig. 8 HCI Command Opcode

The OGF values are defined by the Bluetooth (BT) Core specification. The LE specification has its own OGF value. Also, there is an escape OGF value so that vendor specific OCF codes can be used. The following OGF values are valid for BLE: # Link Control Commands: 1 # Link Policy Commands: 2 # Controller and Baseband Commands: 3 # Informational Parameters: 4 # Status Parameters: 5 # Testing Commands: 6 # LE Only Commands: 8 # Vendor Specific Commands: 63

The following table, Table 2, lists all specification LE HCI commands and their opcodes. Note that while all commands can be sent by the application processor to the Network Processor using HCI, not all events will be returned as they will be trapped and possibly discarded by the Host layer of the BLE Stack. Therefore, it is not possible to support an external BLE Host in the Network Processor configuration. Network Processor based designs should use the respective Vendor Extension commands detailed in the following sections to implement an off-chip application.

LE Commands OGF OCF Opcdoe
LE Set Event Mask 8 1 0x2001
LE Read Buffer Size 8 2 0x2002
LE Read Local Supported Features 8 3 0x2003
LE Set Random Address 8 5 0x2005
LE Set Advertising Parameters 8 6 0x2006
LE Read Advertising Channel TX Power 8 7 0x2007
LE Set Advertising Data 8 8 0x2008
LE Set Scan Response Data 8 9 0x2009
LE Set Advertise Enable 8 10 0x200A
LE Set Scan Parameters 8 11 0x200B
LE Set Scan Enable 8 12 0x200C
LE Create Connection 8 13 0x200D
LE Create Connection Cancel 8 14 0x200E
LE Read White List Size 8 15 0x200F
LE Clear White Lis 8 16 0x2010
LE Add Device To White List 8 17 0x2011
LE Remove Device From White List 8 18 0x2012
LE Connection Update 8 19 0x2013
LE Set Host Channel Classification 8 20 0x2014
LE Read Channel Map 8 21 0x2015
LE Read Remote Used Features 8 22 0x2016
LE Encrypt 8 23 0x2017
LE Rand 8 24 0x2018
LE Start Encryption 8 25 0x2019
LE Long Term Key Requested Reply 8 26 0x201A
LE Long Term Key Requested Negative Reply 8 27 0x201B
LE Read Supported States 8 28 0x201C
LE Receiver Test 8 29 0x201D
LE Transmitter Test 8 30 0x201E
LE Test End Command 8 31 0x201F
LE Remote Connection Parameter Request Reply 8 32 0x2020
LE Remote Connection Parameter Request Negative Reply 8 33 0x2021
LE Set Data Length 8 34 0x2022
LE Read Suggested Default Data Length 8 35 0x2023
LE Write Suggested Default Data Length 8 36 0x2024
LE Read Local P256 Public Key 37 0x2025 LE Generate DHKey 8 38 0x2026
LE Add Device to Resolving List 8 39 0x2027
LE Remove Device from Resolving List 8 40 0x2028
LE Clear Resolving List 8 41 0x2029
LE Read Resolving List Size 8 42 0x202A
LE Read Peer Resolvable Address 8 43 0x202B
LE Read Local Resolvable Address 8 44 0x202C
LE Set Address Resolution Enable 8 45 0x202D
LE Set Resolvable Private Address Timeout 8 46 0x202E
LE Read Maximum Data Length 8 47 0x202F
BT Commands for LE OGF OCF Opcode
Disconnect 1 6 0x0406
Read Remote Version Information 1 29 0x041D
Set Event Mask 3 1 0x0C01
Reset 3 3 0x0C03
Read Transmit Power Level 3 45 0x0C2D
Set Controller To Host Flow Control (optional) 3 49 0x0C31
Host Buffer Size (optional) 3 51 0x0C33
Host Number Of Completed Packets (optional) 3 53 0x0C35
Set Event Mask Page 3 63 0x0C63
Read Authenticated Payload Timeout 4 123 0x0C7B
Write Authenticated Payload Timeout 4 124 0x0C7C
Read Local Version Information 4 1 0x1001
Read Local Supported Commands (optional) 4 2 0x1002
Read Local Supported Features 4 3 0x1003
Read BD_ADDR 4 9 0x1009
Read RSSI 5 5 0x1405

HCI Events

HCI events use an 8-bit event code. All event codes are unique for BT and BLE. Only event code 255 is reserved for vendor specific events. There is only one event code for all LE events. The first event parameter is used as the subevent code to distinguish the LE event types.

The following table lists all the BLE events and their event codes, and subevent codes when applicable:

LE Events Event Code Subevent Code
LE Connection Complete 0x3E 0x01
LE Advertising Report 0x3E 0x02
LE Connection Update Complete 0x3E 0x03
LE Read Remote Used Features Complete 0x3E 0x04
LE Long Term Key Requested 0x3E 0x05
LE Remote Connection Parameter Request 0x3E 0x06
LE Data Length Change 0x3E 0x07
LE Read Local P256 Public Key Complete 0x3E 0x08
LE Generate DHKey Complete 0x3E 0x09
LE Enhanced Connection Complete 0x3E 0x0A
LE Direct Advertising Report 0x3E 0x0B
BT Events Event Code
Disconnection Complete 0x05
Encryption Change 0x08
Read Remote Version Information Complete 0x0C
Command Complete 0x0E
Command Status 0x0F
Hardware Error (optional) 0x10
Number Of Completed Packets 0x13
Data Buffer Overflow 0x1A
Encryption Key Refresh Complete 0x30
Authenticated Payload Timeout Expired 0x57

Vendor Specific Interface

As mentioned, vendors can specify their own HCI commands and events by using the predefined vendor specific opcode and vendor specific event code.

Vendor Specific Commands

A vendor specific opcode is indicated by an OGF value of 63. The vendor can use the remaining 10 bits (i.e. the OCF) as they like. TI defines its vendor specific OCF values by subdividing the 10 bits into a 3 MSB Command Subgroup (CSG) and a 7 LSB Command (CMD). The CSG is used by the HCI to route the commands to a designated subsystem within the BLE stack. In this way, vendor specific commands can be specified for any BLE stack layer.

../_images/vendor-specific-opcode-0-6.png

Fig. 9 HCI Vendor Specific Command Opcode, CSG=0..6

The Command Subgroups are defined as follows:

CSG Subgroup
0 HCI
1 L2CAP
2 ATT
3 GATT
4 GAP
5 UTIL
6 Reserved
7 User Profile

For Command Subgroups 0 to 6, the remaining 7 bits of Command provide up to 128 commands for each subgroup. For Subgroup 7, the remaining 7 bits specify one of 128 profiles and indicates that the subsequent byte is to be used as the command for that particular profile (i.e. up to 256 commands per profile).

../_images/vendor-specific-opcode-7.png

Fig. 10 HCI Vendor Specific Command Opcode, CSG=7

The following table lists all TI-specific HCI commands:

Vendor Specific Command OGF CSG CMD Opcode
HCI_EXT_SetRxGainCmd 63 0 0 0xFC00
HCI_EXT_SetTxPowerCmd 63 0 1 0xFC01
HCI_EXT_OnePktPerEvtCmd 63 0 2 0xFC02
HCI_EXT_ClkDivideOnHaltCmd 63 0 3 0xFC03
HCI_EXT_DeclareNvUsageCmd 63 0 4 0xFC04
HCI_EXT_DecryptCmd 63 0 5 0xFC05
HCI_EXT_SetLocalSupportedFeaturesCmd 63 0 6 0xFC06
HCI_EXT_SetFastTxRespTimeCmd 63 0 7 0xFC07
HCI_EXT_ModemTestTxCmd 63 0 8 0xFC08
HCI_EXT_ModemHopTestTxCmd 63 0 9 0xFC09
HCI_EXT_ModemTestRxCmd 63 0 10 0xFC0A
HCI_EXT_EndModemTestCmd 63 0 11 0xFC0B
HCI_EXT_SetBDADDRCmd 63 0 12 0xFC0C
HCI_EXT_SetSCACmd 63 0 13 0xFC0D
HCI_EXT_EnablePTMCmd 63 0 14 0xFC0E
HCI_EXT_SetFreqTuneCmd 63 0 15 0xFC0F
HCI_EXT_SaveFreqTuneCmd 63 0 16 0xFC10
HCI_EXT_SetMaxDtmTxPowerCmd 63 0 17 0xFC11
HCI_EXT_MapPmIoPortCmd 63 0 18 0xFC12
HCI_EXT_DisconnectImmedCmd 63 0 19 0xFC13
HCI_EXT_PacketErrorRateCmd 63 0 20 0xFC14
HCI_EXT_PERbyChanCmd 63 0 21 0xFC15
HCI_EXT_ExtendRfRangeCmd 63 0 22 0xFC16
HCI_EXT_HaltDuringRfCmd 63 0 25 0xFC19
HCI_EXT_SetSlaveLatencyOverrideCmd 63 0 26 0xFC1A
HCI_EXT_BuildRevisionCmd 63 0 27 0xFC1B
HCI_EXT_DelaySleepCmd 63 0 28 0xFC1C
HCI_EXT_ResetSystemCmd 63 0 29 0xFC1D
HCI_EXT_OverlappedProcessingCmd 63 0 30 0xFC1E
HCI_EXT_NumComplPktsLimitCmd 63 0 31 0xFC1F
HCI_EXT_GetConnInfoCmd 63 0 32 0xFC20
HCI_EXT_SetMaxDataLenCmd 63 0 33 0xFC21
HCI_EXT_SetDtmTxPktCntCmd 63 0 36 0xFC24
HCI_EXT_EnhancedModemTestTxCmd 63 0 39 0xFC27
HCI_EXT_EnhancedModemHopTestTxCmd 63 0 40 0xFC28
HCI_EXT_EnhancedModemTestRxCmd 63 0 41 0xFC29
HCI_EXT_LLTestModeCmd 63 0 112 0xFC70
L2CAP_DisconnectReq 63 1 6 0xFC86
L2CAP_InfoReq 63 1 10 0xFC8A
L2CAP_ConnParamUpdateReq 63 1 18 0xFC92
L2CAP_ConnectReq 63 1 20 0xFC94
L2CAP_ConnectRsp 63 1 21 0xFC95
L2CAP_FlowCtrlCredit 63 1 22 0xFC96
L2CAP_SendData 63 1 112 0xFCF0
L2CAP_RegisterPsm 63 1 113 0xFCF1
L2CAP_DeregisterPsm 63 1 114 0xFCF2
L2CAP_PsmInfo 63 1 115 0xFCF3
L2CAP_PsmChannels 63 1 116 0xFCF4
L2CAP_ChannelInfo 63 1 117 0xFCF5
ATT_ErrorRsp 63 2 1 0xFD01
ATT_ExchangeMTUReq 63 2 2 0xFD02
ATT_ExchangeMTURsp 63 2 3 0xFD03
ATT_FindInfoReq 63 2 4 0xFD04
ATT_FindInfoRsp 63 2 5 0xFD05
ATT_FindByTypeValueReq 63 2 6 0xFD06
ATT_FindByTypeValueRsp 63 2 7 0xFD07
ATT_ReadByTypeReq 63 2 8 0xFD08
ATT_ReadByTypeRsp 63 2 9 0xFD09
ATT_ReadReq 63 2 10 0xFD0A
ATT_ReadRsp 63 2 11 0xFD0B
ATT_ReadBlobReq 63 2 12 0xFD0C
ATT_ReadBlobRsp 63 2 13 0xFD0D
ATT_ReadMultiReq 63 2 14 0xFD0E
ATT_ReadMultiRsp 63 2 15 0xFD0F
ATT_ReadByGrpTypeReq 63 2 16 0xFD10
ATT_ReadByGrpTypeRsp 63 2 17 0xFD11
ATT_WriteReq 63 2 18 0xFD12
ATT_WriteRsp 63 2 19 0xFD13
ATT_PrepareWriteReq 63 2 22 0xFD16
ATT_PrepareWriteRsp 63 2 23 0xFD17
ATT_ExecuteWriteReq 63 2 24 0xFD18
ATT_ExecuteWriteRsp 63 2 25 0xFD19
ATT_HandleValueNoti 63 2 27 0xFD1B
ATT_HandleValueInd 63 2 29 0xFD1D
ATT_HandleValueCfm 63 2 30 0xFD1E
GATT_ExchangeMTU 63 3 2 0xFD82
GATT_DiscAllCharDescs 63 3 4 0xFD84
GATT_DiscPrimaryServiceByUUID 63 3 6 0xFD86
GATT_DiscCharsByUUID 63 3 8 0xFD88
GATT_ReadCharValue 63 3 10 0xFD8A
GATT_ReadLongCharValue 63 3 12 0xFD8C
GATT_ReadMultiCharValues 63 3 14 0xFD8E
GATT_DiscAllPrimaryServices 63 3 16 0xFD90
GATT_WriteCharValue 63 3 18 0xFD92
GATT_WriteLongCharValue 63 3 22 0xFD96
GATT_Notification 63 3 27 0xFD9B
GATT_Indication 63 3 29 0xFD9D
GATT_FindIncludedServices 63 3 48 0xFDB0
GATT_DiscAllChars 63 3 50 0xFDB2
GATT_ReadUsingCharUUID 63 3 52 0xFDB4
GATT_WriteNoRsp 63 3 54 0xFDB6
GATT_SignedWriteNoRsp 63 3 56 0xFDB8
GATT_ReliableWrites 63 3 58 0xFDBA
GATT_ReadCharDesc 63 3 60 0xFDBC
GATT_ReadLongCharDesc 63 3 62 0xFDBE
GATT_WriteCharDesc 63 3 64 0xFDC0
GATT_WriteLongCharDesc 63 3 66 0xFDC2
GATT_AddService 63 3 124 0xFDFC
GATT_DelService 63 3 125 0xFDFD
GATT_AddAttribute 63 3 126 0xFDFE
GAP_DeviceInit 63 4 0 0xFE00
GAP_TerminateLinkReq 63 4 10 0xFE0A
GAP_Authenticate 63 4 11 0xFE0B
GAP_PasskeyUpdate 63 4 12 0xFE0C
GAP_SlaveSecurityRequest 63 4 13 0xFE0D
GAP_Signable 63 4 14 0xFE0E
GAP_Bond 63 4 15 0xFE0F
GAP_TerminateAuth 63 4 16 0xFE10
GAP_UpdateLinkParamReq 63 4 17 0xFE11
GAP_UpdateLinkParamReqReply 63 4 18 0xFE12
Gap_RegisterConnEvent 63 4 19 0xFE13
GapConfig_SetParameter 63 4 47 0xFE2F
GAP_SetParamValue 63 4 48 0xFE30
GAP_GetParamValue 63 4 49 0xFE31
GAPBondMgr_SetParameter 63 4 54 0xFE36
GAPBondMgr_GetParameter 63 4 55 0xFE37
GAPBondMgr_ServiceChangeInd 63 4 56 0xFE38
SM_RegisterTask 63 4 57 0xFE39
SM_GetEccKeys 63 4 58 0xFE3A
SM_GetDHKey 63 4 59 0xFE3B
SM_GetScConfirmOob 63 4 60 0xFE3C
GapAdv_create 63 4 62 0xFE3E
GapAdv_enable 63 4 63 0xFE3F
GapAdv_disable 63 4 64 0xFE40
GapAdv_destroy 63 4 65 0xFE41
GapAdv_setParam 63 4 66 0xFE42
GapAdv_getParam 63 4 67 0xFE43
GapAdv_loadData 63 4 68 0xFE44
GapAdv_setEventMask 63 4 69 0xFE45
GAPBondMgr_Pair 63 4 72 0xFE48
GAPBondMgr_FindAddr 63 4 73 0xFE49
GAPBondMgr_PasscodeRsp 63 4 74 0xFE4A
GapScan_enable 63 4 81 0xFE51
GapScan_disable 63 4 82 0xFE52
GapScan_setPhyParams 63 4 83 0xFE53
GapScan_getPhyParams 63 4 84 0xFE54
GapScan_setParam 63 4 85 0xFE55
GapScan_getParam 63 4 86 0xFE56
GapScan_setEventMask 63 4 87 0xFE57
GapScan_getAdvReport 63 4 88 0xFE58
GapInit_setPhyParam 63 4 96 0xFE60
GapInit_getPhyParam 63 4 97 0xFE61
GapInit_connect 63 4 98 0xFE62
GapInit_connectWl 63 4 99 0xFE63
GapInit_cancelConnect 63 4 100 0xFE64
UTIL_Reserved 63 5 0 0xFE80
UTIL_NV_Read 63 5 1 0xFE81
UTIL_NV_Write 63 5 2 0xFE82
UTIL_ForceBoot 63 5 3 0xFE83
UTIL_BuildRevision 63 5 4 0xFE84
UTIL_GetMemStats 63 5 7 0xFE87

Vendor Specific Events

A vendor specific event code is indicated by a value of 255. The vendor must then use event parameters (following the length byte) to specify vendor specific events. TI defines the following two bytes as the Event Opcode.

../_images/vendor-specific-event-1.png

The Event Opcode was chosen to mirror the Command Opcode by dividing it into two parts: a 6 bit Event Opcode Group Field (EOGF), and a 10 bit Event Opcode Event Field (EOEF).

../_images/vendor-specific-event-2.png

The EOEF is again chosen to mirror the Command OCF by dividing it into two parts: the Event Subgroup (ESG) and the Event.

../_images/vendor-specific-event-3.png

The EOGF is defined as follows:

EOGF Group
0 Embedded Opcode
1 Core Opcode
2 Profile Request
3 Profile Response
4-63 Reserved

The ESG is defined as in Table 4. The Events are as defined in the following table. Please note that the value of the Events cannot be less than 0x400 as the first 1024 values are reserved. The reason for this has to do with Client/Server Request/Response Tunneling, which is described in the following section. Tunneling requires embedding Command Opcodes in HCI Events. When this is done, the EOGF is zero, and the remaining 10 bits is the Command Opcode. In order to prevent Command and Event Opcode overlap, the first 1024 values are reserved in the Event Opcode space. Also note that the Event Code (EC) is always 0xFF since normally only Controller events are returned via the HCI.

Vendor Specific Event EC EOGF ESG Event Opcode
HCI_EXT_SetRxGainDone 0xFF 1 0 0 0x0400
HCI_EXT_SetTxPowerDone 0xFF 1 0 1 0x0401
HCI_EXT_OnePacketPerEventDone 0xFF 1 0 2 0x0402
HCI_EXT_DecryptCommandDone 0xFF 1 0 5 0x0405
HCI_EXT_WriteLocalFeatureSupportDone 0xFF 1 0 6 0x0406
HCI_EXT_SetFastTxResponseTimeDone 0xFF 1 0 7 0x0407
HCI_EXT_ModemTestTxDone 0xFF 1 0 8 0x0408
HCI_EXT_ModemHopTestTxDone 0xFF 1 0 9 0x0409
HCI_EXT_ModemTestRxDone 0xFF 1 0 10 0x040A
HCI_EXT_EndModemTestDone 0xFF 1 0 11 0x040B
HCI_EXT_SetBDADDRDone 0xFF 1 0 12 0x040C
HCI_EXT_SetSCADone 0xFF 1 0 13 0x040D
HCI_EXT_EnablePTMDone 0xFF 1 0 14 0x040E
HCI_EXT_SetMaxDtmTxPowerDone 0xFF 1 0 17 0x0411
HCI_EXT_MapPmIoPortDone 0xFF 1 0 18 0x0412
HCI_EXT_DisconnectImmedDone 0xFF 1 0 19 0x0413
HCI_EXT_PER 0xFF 1 0 20 0x0414
HCI_EXT_PerByChanDone 0xFF 1 0 21 0x0415
HCI_EXT_OverrideSLDone 0xFF 1 0 26 0x041A
HCI_EXT_BuildRevisionDone 0xFF 1 0 27 0x041B
HCI_EXT_ResetSystemDone 0xFF 1 0 29 0x041D
HCI_EXT_NumComplPktsLimitDone 0xFF 1 0 31 0x041F
HCI_EXT_GetConnInfoDone 0xFF 1 0 32 0x0420
HCI_EXT_SetMaxDataLengthDone 0xFF 1 0 33 0x0421
HCI_EXT_SetDtmTxPktCntDone 0xFF 1 0 36 0x0424
HCI_EXT_LE_ADV_EVENT 0xFF 1 0 37 0x0425
HCI_EXT_LE_SCAN_EVENT 0xFF 1 0 38 0x0426
HCI_EXT_EnhancedModemTestTxDone 0xFF 1 0 39 0x0427
HCI_EXT_EnhancedModemHopTestTxDone 0xFF 1 0 40 0x0428
HCI_EXT_EnhancedModemTestRxDone 0xFF 1 0 41 0x0429
HCI_EXT_LLTestModeDone 0xFF 1 0 112 0x0470
L2CAP_CmdReject 0xFF 1 1 1 0x0481
L2CAP_InfoRsp 0xFF 1 1 11 0x048B
L2CAP_ConnParamUpdateRsp 0xFF 1 1 19 0x0493
L2CAP_ConnectReq 0xFF 1 1 20 0x0494
L2CAP_ChannelEstablished 0xFF 1 1 96 0x04E0
L2CAP_ChannelTerminated 0xFF 1 1 97 0x04E1
L2CAP_OutOfCredit 0xFF 1 1 98 0x04E2
L2CAP_PeerCreditThreshold 0xFF 1 1 99 0x04E3
L2CAP_SendSduDone 0xFF 1 1 100 0x04E4
L2CAP_SendData 0xFF 1 1 112 0x04F0
ATT_ErrorRsp 0xFF 1 2 1 0x0501
ATT_ExchangeMTUReq 0xFF 1 2 2 0x0502
ATT_ExchangeMTURsp 0xFF 1 2 3 0x0503
ATT_FindInfoReq 0xFF 1 2 4 0x0504
ATT_FindInfoRsp 0xFF 1 2 5 0x0505
ATT_FindByTypeValueReq 0xFF 1 2 6 0x0506
ATT_FindByTypeValueRsp 0xFF 1 2 7 0x0507
ATT_ReadByTypeReq 0xFF 1 2 8 0x0508
ATT_ReadByTypeRsp 0xFF 1 2 9 0x0509
ATT_ReadReq 0xFF 1 2 10 0x050A
ATT_ReadRsp 0xFF 1 2 11 0x050B
ATT_ReadBlobReq 0xFF 1 2 12 0x050C
ATT_ReadBlobRsp 0xFF 1 2 13 0x050D
ATT_ReadMultiReq 0xFF 1 2 14 0x050E
ATT_ReadMultiRsp 0xFF 1 2 15 0x050F
ATT_ReadByGrpTypeReq 0xFF 1 2 16 0x0510
ATT_ReadByGrpTypeRsp 0xFF 1 2 17 0x0511
ATT_WriteReq 0xFF 1 2 18 0x0512
ATT_WriteRsp 0xFF 1 2 19 0x0513
ATT_PrepareWriteReq 0xFF 1 2 22 0x0516
ATT_PrepareWriteRsp 0xFF 1 2 23 0x0517
ATT_ExecuteWriteReq 0xFF 1 2 24 0x0518
ATT_ExecuteWriteRsp 0xFF 1 2 25 0x0519
ATT_HandleValueNoti 0xFF 1 2 27 0x051B
ATT_HandleValueInd 0xFF 1 2 29 0x051D
ATT_HandleValueCfm 0xFF 1 2 30 0x051E
ATT_FlowCtrlViolatedEvt_t 0xFF 1 2 126 0x057E
ATT_MtuUpdatedEvt 0xFF 1 2 127 0x057F
GATT_ClientCharCfgUpdated 0xFF 1 3 0 0x0580
GAP_DeviceInitDone 0xFF 1 4 0 0x0600
GAP_LinkEstablished 0xFF 1 4 5 0x0605
GAP_LinkTerminated 0xFF 1 4 6 0x0606
GAP_LinkParamUpdate 0xFF 1 4 7 0x0607
GAP_SignatureUpdated 0xFF 1 4 9 0x0609
GAP_AuthenticationComplete 0xFF 1 4 10 0x060A
GAP_PasskeyNeeded 0xFF 1 4 11 0x060B
GAP_SlaveRequestedSecurity 0xFF 1 4 12 0x060C
GAP_BondComplete 0xFF 1 4 14 0x060E
GAP_PairingRequested 0xFF 1 4 15 0x060F
SM_GetEccKeys 0xFF 1 4 16 0x0610
SM_GetDHKey 0xFF 1 4 17 0x0611
GAP_LinkParamUpdateRequest 0xFF 1 4 18 0x0612
GAP_Advertiser/Scanner_Event 0xFF 1 4 19 0x0613
GAP_ConnectingCancelled 0xFF 1 4 21 0x0615
GAP_ConnectionEventNotice 0xFF 1 4 22 0x0616
CommandStatus 0xFF 1 4 127 0x067F
UTIL_GetMemStats 0xFF 1 5 1 0x0681
UTIL_SystemError 0xFF 1 5 2 0x0682

You will note that there are two EOGF values for Profiles. At this time, no profiles are defined well enough to document here. These values are defined in anticipation of not only needing large numbers of profiles and their commands, but also of needing the direction the command is travelling when embedded in an HCI Command or Event. You can see that ATT does not have this issue as these commands are already defined using even values for commands and odd values for events, and thus, direction is distinguishable. For profiles, it is not yet known how the commands and events will be defined.

Request and Response Tunneling

In the Client/Server model defined and supported by the BLE stack, the Client sends Requests to the Server and the Server sends Responses back to the Client. The Requests sent by the Client may be handled by a Server on the same device, or they may travel OTA to the Server on another device. Similarly, the Response sent by the Server may be handled by a Client on the same device, or may be sent OTA to a Client on another device from which the request came. But in either case, as long as the Requests and Responses remain within the scope of the BLE stack software (i.e. the BLE Server database is on the device), the BLE stack remains unconcerned about whether the Requests and Responses are sent/received by the same device or are from another device. Please see Fig. 14.

../_images/tunneling-1.png

Fig. 14 Request/Response with Server Database in BLE Stack

However, when using the Network Processor Configuration with HCI such that the Server database is not located on the device, then Requests and Reponses have to be mapped into HCI Commands and Events. The HCI is specified such that only Commands are sent from the Host to the Controller, and only Events are sent from the Controller to the Host. If the Server database is located on say a PC, then when an OTA Request is received by the Server device, it must be sent to the PC via the HCI. Even though the Request started out on one end as an HCI Command, it must be provided to the remote PC as an HCI event on the other. Similarly, when the PC sends the Response on one end, which will be an HCI Event to the remote PC on the other, it must be sent to the device as an HCI Command. Thus, the Request, which starts out as an HCI Command, must be embedded in an HCI Event when received by the remote PC, and the Response, which starts out as an HCI Command, must be embedded in an HCI Event when received by the remote PC. In this way, Requests and Responses are being tunneled in HCI Commands and Events. Please see Fig. 15.

../_images/tunneling-2.png

Fig. 15 Request/Response with Server Database not in BLE Stack