Changelog
Table of Contents
New Features
BLE5-Stack
| ID | Summary |
|---|---|
| None | None |
BLE-Stack
| ID | Summary |
|---|---|
| BLESTACK-4752 | RTLS Ctrl: Add support for changing connection parameters |
TI Proprietary-RF
| ID | Summary |
|---|---|
| EZLINKPROP-672 | Create off-chip OAD examples on CC2640R2 |
| EZLINKPROP-671 | Create on-chip OAD example on CC2640R2 |
| EZLINKPROP-670 | Add additional examples for CC2640R2 |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-3801 | Integrate CC13xx/26xx DriverLib 3.05.12 |
Fixed Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLESTACK-4868 | GAP_ADV_ENABLE_OPTIONS_USE_DURATION times out and terminates connection |
| BLESTACK-4834 | Queued Parameter Updates cause an exception due to double free |
| BLESTACK-4756 | simple_peripheral re-connection after bond cleared terminate due to MIC error |
| BLESTACK-4726 | LL scheduler drops connections when another device is walking out of range |
| BLESTACK-4725 | The Data RX path(llCombinePDU) supports only 1 data stream at a time |
BLE-Stack
| ID | Summary |
|---|---|
| BLESTACK-4869 | GAPBONDMGR: Update authentication parameters when transitioning between authenticated/non-authenticated pairing |
| BLESTACK-4830 | [RTLS] When using TOF_MODE_RAW with out of box example, the number of sync-words is limited to 64 |
| BLESTACK-4710 | The Data RX path(llCombinePDU) supports only 1 data stream at a time |
| BLESTACK-4684 | LL scheduler drops connections when another device is walking out of range |
| BLESTACK-4620 | Att read request wont respond when trying to read with insufficient authentication |
| BLESTACK-4346 | HCI_EXT_GetActiveConnInfoCmd does not work for peripheral connections |
TI Proprietary-RF
| ID | Summary |
|---|---|
| None | None |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| None | None |
Known Issues and Limitations
BLE5-Stack
| ID | Summary |
|---|---|
| BLETOOLS-312 | [Btool App] SC Switching PHY: from 1M to 2M and then to coded received PHY update complete 1M,2M instead of Coded |
| BLETOOLS-14 | [BTool App] Discovered devices list is never cleared |
| BLETOOLS-5 | [BTool App] The application always starts as Central configuration even if loads host_test_peripheral.hex |
| BLESTACK-4531 | host_test app with central and broadcast cannot be built due to memory limitation, with CCS |
| BLESTACK-4058 | Host test does not support HCI_LE_Rand |
| BLESTACK-3877 | Maximum supported number of concurrent BLE connections: 2 (embedded sample applications), and 3 (Host Test).Additional connections can be supported when using Cache-As-RAM |
| BLESTACK-3834 | Periodic advertisements are not supported |
| BLESTACK-3685 | Number of simultaneous connections may be limited when attempting concurrent LE Secure Connections pairings |
| BLESTACK-3678 | Host test peripheral + central build is not supported |
| BLESTACK-2711 | Issue when Scanning for extended advertisements using the 2M PHY |
BLE-Stack
| ID | Summary |
|---|---|
| BLESTACK-5009 | Peer’s RPA is not re-generated on address resolution timeout when local IRK is all zeros |
| BLESTACK-4958 | BIM reserves extra pages of flash when not using secure OAD |
| BLESTACK-4902 | [RTLS] TOF is not stable for connection interval greater than 1 second |
| BLESTACK-4842 | RTLS passive not reporting ToF data on CCS build when optimization is enabled |
| BLESTACK-4829 | [RTLS] rtls_passive won’t re-sync when using TOF_MODE_AUTO run mode in Dynamic Sync-word mode |
| BLESTACK-4793 | RTLS Passive sync issues: missing the first word will stop Passive ToF in Dynamic Sync-word mode |
| BLESTACK-4511 | CC2640R2 OAD target boots into user app after receiving reset command during unsecure on-chip OAD with a secure BLE connection |
| BLESTACK-4505 | Enabling a specific off-chip image is not working for CC2640R2 |
| BLESTACK-4459 | Revert to factory image not working for CC2640R2 off-chip OAD |
| BLESTACK-4263 | BIM reserves extra pages of flash when not using secure OAD |
| BLESTACK-4133 | Simple Observer: Cancel the discovery during discovery process received ERROR and need to reset the board |
| BLESTACK-3934 | L2CAP recombination failing in some cases when data length update combines with L2CAP packet |
| BLESTACK-3641 | L2CAP Connection Oriented Channels are not available in multi-role configurations |
| BLESTACK-3640 | Number of simultaneous connections may be limited when attempting concurrent LE Secure Connections pairings |
| BLESTACK-2706 | Multi-role incorrectly sets gapRole_AdvEnabled when enabling non-connectable advertisements. |
TI Proprietary-RF
| ID | Summary |
|---|---|
| None | None |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-3636 | I2C_transfer() occasionally fails when called from an interrupt context |
| TIDRIVERS-3635 | UART_read returns 0 in portable after a power-cycle on CC13x0 and CC26x0 devices |
| TIDRIVERS-3626 | Sysconfig cannot configure SPI four pin mode for LPRF boards |
| TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |