Changelog
Table of Contents
New Features
BLE5-Stack
ID | Summary |
---|---|
None | None |
BLE-Stack
ID | Summary |
---|---|
BLESTACK-4568 | ToF Security |
BLESTACK-4567 | AoA tone moved up to CRC |
BLESTACK-4538 | RTLS Management |
BLESTACK-4536 | BLE3 flash optimization |
BLESTACK-4440 | Support Unlimited Scanning |
TI Proprietary-RF
ID | Summary |
---|---|
None | None |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIRTOS-1543 | Update examples and board files to support Sharp128 Display as the default (was Sharp96) |
TIRTOS-1430 | Call pthread_exit() in run stub to handle termination sequence |
TIRTOS-1016 | examplesgen – revise the process of importing examples to IAR |
TIDRIVERS-1539 | Include PDM driver assembly files and give them BSD license |
TIDRIVERS-1436 | Example pinstandby stand-by current is too high |
TIDRIVERS-1421 | SPI drivers for MSP432E and CC13X2/CC26X2 should use the DMA driver in ping-pong mode |
TIDRIVERS-953 | Implement generic AES_CBC driver |
Fixed Issues
BLE5-Stack
ID | Summary |
---|---|
BLESTACK-4564 | [clone for ble5_1_1_x] Known issue where queued param updates in slave device cause application assert |
BLESTACK-4175 | Known issue: device list can be duplicated in simple_central scanning |
BLE-Stack
ID | Summary |
---|---|
BLESTACK-4193 | Fixed issue where an incoming Slave Security Request not handled properly by the GapBondMgr and will trigger a new pair |
TI Proprietary-RF
ID | Summary |
---|---|
EZLINKPROP-544 | EasyLink: Fixed an issue where a mutex was not released prior to function returning on an error condition. |
EZLINKPROP-525 | Missing #include “cpu.h” in functions where CPUdelay() is called |
EZLINKPROP-522 | EasyLink NP: Fixed an issue where address filtering did not work for address sizes greater than 2 bytes |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIRTOS-1435 | clock_nanosleep() with CLOCK_REALTIME broken on msp432 |
TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |
TIDRIVERS-1464 | Setting CC26XX IOC config as edge triggered and muxing in a non-GPIO configuration can cause spurrious events |
Known Issues and Limitations
BLE5-Stack
ID | Summary |
---|---|
BLESTACK-4058 | Host test does not support HCI_LE_Rand |
BLESTACK-3877 | Maximum supported number of concurrent BLE connections: 2 (embedded sample applications), and 3 (Host Test).Additional connections can be supported when using Cache-As-RAM |
BLESTACK-3834 | Periodic advertisements are not supported |
BLESTACK-3685 | Number of simultaneous connections may be limited when attempting concurrent LE Secure Connections pairings |
BLESTACK-3678 | Host test peripheral + central build is not supported |
BLESTACK-2711 | Issue when Scanning for extended advertisements using the 2M PHY |
BLE-Stack
ID | Summary |
---|---|
BLESTACK-4263 | BIM reserves extra pages of flash when not using secure OAD |
BLESTACK-3934 | L2CAP recombination failing in some cases when data length update combines with L2CAP packet |
BLESTACK-3641 | L2CAP Connection Oriented Channels are not available in multi-role configurations |
BLESTACK-3640 | Number of simultaneous connections may be limited when attempting concurrent LE Secure Connections pairings |
BLESTACK-2706 | Multi-role incorrectly sets gapRole_AdvEnabled when enabling non-connectable advertisements. |
TI Proprietary-RF
ID | Summary |
---|---|
None | None |
TI-RTOS and Drivers
ID | Summary |
---|---|
None | None |