367 #ifndef ti_drivers_crypto_CryptoCC26XX__include 368 #define ti_drivers_crypto_CryptoCC26XX__include 379 #include <ti/devices/DeviceFamily.h> 380 #include DeviceFamily_constructPath(driverlib/crypto.h) 382 #if DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X2_CC26X2 383 #warning "This driver is deprecated for the CC26x2 and CC13x2 families.\ 384 It is superceded by AESECB and AESCCM." 415 #define CRYPTOCC26XX_TIMEOUT 20 417 #define CRYPTOCC26XX_STATUS_SUCCESS 0 418 #define CRYPTOCC26XX_STATUS_ERROR -1 419 #define CRYPTOCC26XX_STATUS_UNDEFINEDCMD -2 421 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT 0 422 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY 1 423 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT 2 424 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY 3 425 #define CRYPTOCC26XX_OP_AES_ECB_ENCRYPT 4 426 #define CRYPTOCC26XX_OP_AES_ECB_DECRYPT 5 427 #define CRYPTOCC26XX_OP_AES_CBC_ENCRYPT 6 428 #define CRYPTOCC26XX_OP_AES_CBC_DECRYPT 7 431 #define CRYPTOCC26XX_OP_AES_CCM CRYPTOCC26XX_OP_AES_CCM_ENCRYPT 432 #define CRYPTOCC26XX_OP_AES_CCM_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY 433 #define CRYPTOCC26XX_OP_AES_CCMINV CRYPTOCC26XX_OP_AES_CCM_DECRYPT 434 #define CRYPTOCC26XX_OP_AES_CCMINV_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY 435 #define CRYPTOCC26XX_OP_AES_ECB CRYPTOCC26XX_OP_AES_ECB_ENCRYPT 436 #define CRYPTOCC26XX_OP_AES_ECB_NOCRYPT CRYPTOCC26XX_OP_AES_ECB_DECRYPT 439 #include <ti/drivers/dpl/HwiP.h> 440 #include <ti/drivers/dpl/SemaphoreP.h> 853 int CryptoCC26XX_allocateKey(CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation,
const uint32_t *keySrc);
int CryptoCC26XX_allocateKey(CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation, const uint32_t *keySrc)
Function that allocates key, writes key into key store RAM and returns a handle to CryptoCC26XX Key...
CryptoCC26XX Transaction.
Definition: CryptoCC26XX.h:525
CryptoCC26XX Global Configuration.
Definition: CryptoCC26XX.h:740
CryptoCC26XX_Transaction * currentTransact
Definition: CryptoCC26XX.h:724
void CryptoCC26XX_Params_init(CryptoCC26XX_Params *params)
Function to initialize the CryptoCC26XX_Params struct to its defaults.
CryptoCC26XX AES-CCM Transaction.
Definition: CryptoCC26XX.h:581
struct CryptoCC26XX_Object CryptoCC26XX_Object
CryptoCC26XX Object.
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:656
int CryptoCC26XX_close(CryptoCC26XX_Handle handle)
Function to closes a given CryptoCC26XX peripheral specified by the CryptoCC26XX handle.
void * msgOut
Definition: CryptoCC26XX.h:611
struct CryptoCC26XX_AESCCM_Transaction CryptoCC26XX_AESCCM_Transaction
CryptoCC26XX AES-CCM Transaction.
CryptoCC26XX_Transaction * tailPtr
Definition: CryptoCC26XX.h:728
CryptoCC26XX Parameters.
Definition: CryptoCC26XX.h:505
uint8_t keyIndex
Definition: CryptoCC26XX.h:658
void * msgIn
Definition: CryptoCC26XX.h:644
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:582
Definition: CryptoCC26XX.h:491
SemaphoreP_Struct waitSem
Definition: CryptoCC26XX.h:736
HwiP_Struct hwi
Definition: CryptoCC26XX.h:734
SemaphoreP_Struct transSem
Definition: CryptoCC26XX.h:735
uint8_t CryptoCC26XX_Operation
CryptoCC26XX Operation Type.
Definition: CryptoCC26XX.h:481
uint8_t fieldLength
Definition: CryptoCC26XX.h:617
Power notify object structure.
Definition: Power.h:121
Definition: CryptoCC26XX.h:494
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:526
Definition: CryptoCC26XX.h:458
CryptoCC26XX_Transaction * headPtr
Definition: CryptoCC26XX.h:727
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:640
int CryptoCC26XX_loadKey(CryptoCC26XX_Handle handle, int keyIndex, const uint32_t *keySrc)
Function that writes a given key into a key store.
void * msgOut
Definition: CryptoCC26XX.h:660
uint8_t keyIndex
Definition: CryptoCC26XX.h:584
char * nonce
Definition: CryptoCC26XX.h:587
void * msgOut
Definition: CryptoCC26XX.h:645
struct CryptoCC26XX_Config CryptoCC26XX_Config
CryptoCC26XX Global Configuration.
void CryptoCC26XX_Transac_init(CryptoCC26XX_Transaction *trans, CryptoCC26XX_Operation opType)
Function to initialize the CryptoCC26XX_Transaction struct to its defaults.
int CryptoCC26XX_releaseKey(CryptoCC26XX_Handle handle, int *keyIndex)
Function that releases the specified CryptoCC26XX Key.
Definition: CryptoCC26XX.h:497
char * header
Definition: CryptoCC26XX.h:610
CryptoCC26XX Hardware Attributes.
Definition: CryptoCC26XX.h:692
Power_NotifyObj cryptoNotiObj
Definition: CryptoCC26XX.h:731
int openCnt
Definition: CryptoCC26XX.h:721
Definition: CryptoCC26XX.h:496
void const * hwAttrs
Definition: CryptoCC26XX.h:745
uint16_t headerLength
Definition: CryptoCC26XX.h:630
Definition: CryptoCC26XX.h:464
uint16_t msgInLength
Definition: CryptoCC26XX.h:628
struct CryptoCC26XX_Params CryptoCC26XX_Params
CryptoCC26XX Parameters.
struct CryptoCC26XX_Config * CryptoCC26XX_Handle
A handle that is returned from a CryptoCC26XX_open() call.
Definition: CryptoCC26XX.h:445
void * msgIn
Definition: CryptoCC26XX.h:659
uint32_t timeout
Definition: CryptoCC26XX.h:722
Definition: CryptoCC26XX.h:498
CryptoCC26XX_Mode
CryptoCC26XX Mode Settings.
Definition: CryptoCC26XX.h:453
CryptoCC26XX AES-ECB Transaction.
Definition: CryptoCC26XX.h:655
char * msgIn
Definition: CryptoCC26XX.h:604
void CryptoCC26XX_init(void)
Function to initialize CryptoCC26XX driver. Users of this module must call init(). Multiple users/libraries may call init(), though subsequent calls may be benign.
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: CryptoCC26XX.h:711
int CryptoCC26XX_transact(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto operation (encryption or decryption) in blocking mode.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:641
CryptoCC26XX_KeyStore keyStore
Definition: CryptoCC26XX.h:723
uint8_t keyIndex
Definition: CryptoCC26XX.h:642
uint16_t msgInLength
Definition: CryptoCC26XX.h:646
int powerMngrId
Definition: CryptoCC26XX.h:696
void * object
Definition: CryptoCC26XX.h:742
Definition: CryptoCC26XX.h:499
Definition: CryptoCC26XX.h:493
uint8_t CryptoCC26XX_KeyStore
CryptoCC26XX Key.
Definition: CryptoCC26XX.h:514
CryptoCC26XX_Handle CryptoCC26XX_open(unsigned int index, bool exclusiveAccess, CryptoCC26XX_Params *params)
Function to initialize a given CryptoCC26XX peripheral specified by the particular index value...
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:657
void * nonce
Definition: CryptoCC26XX.h:643
CryptoCC26XX_KeyLocation
CryptoCC26XX Key Store Location.
Definition: CryptoCC26XX.h:489
int intNum
Definition: CryptoCC26XX.h:698
struct CryptoCC26XX_HWAttrs CryptoCC26XX_HWAttrs
CryptoCC26XX Hardware Attributes.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:527
Definition: CryptoCC26XX.h:495
struct CryptoCC26XX_Transaction CryptoCC26XX_Transaction
CryptoCC26XX Transaction.
uint32_t timeout
Definition: CryptoCC26XX.h:506
CryptoCC26XX Object.
Definition: CryptoCC26XX.h:719
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:583
uint32_t baseAddr
Definition: CryptoCC26XX.h:694
struct CryptoCC26XX_AESECB_Transaction CryptoCC26XX_AESECB_Transaction
CryptoCC26XX AES-ECB Transaction.
struct CryptoCC26XX_AESCBC_Transaction CryptoCC26XX_AESCBC_Transaction
CryptoCC26XX AES-CBC Transaction.
Definition: CryptoCC26XX.h:492
int CryptoCC26XX_transactPolling(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in polling mode...
int CryptoCC26XX_transactCallback(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in callback mode...
uint8_t authLength
Definition: CryptoCC26XX.h:585
CryptoCC26XX AES-CBC Transaction.
Definition: CryptoCC26XX.h:639
Definition: CryptoCC26XX.h:490