OAD Type Comparison¶
There are two methods of implementing an over the air download update: On-chip and Off-chip. The key difference between the two methods is where the downloaded image is to be stored during the OAD process. During on-chip OAD, the downloaded image is written to internal flash, allowing for a single chip OAD solution. Off-chip stores the downloaded image in an external flash part, requiring a two chip OAD solution. Each type of OAD has associated trade offs and benefits which will be discussed in their respective sections. Despite their differences, both OAD methods share the same over the air profile and image header.
OAD Type | Advantages | Limitations |
On-chip |
|
|
Off-chip |
|
|