BLE-Stack 3.01.01 to BLE-Stack 3.02.00¶
This section will describe a way to migrate a project from BLE-Stack 3.01.01 to a BLE-Stack 3.02.00.
For this migration guide, simple_peripheral from BLE-Stack 3.01.01 will be ported over to BLE-Stack 3.02.00. Because the directory structure is nearly identical between the two releases, the recommended approach is to start with a BLE-Stack 3.02.00 project that contains the same base functionality as the porting target project and merge in any custom functionality.
If you choose to not start with an example project from BLE-Stack 3.02.00 and
instead wish to port your project by going to Properties>General>Products and
selecting the new version of the CC2640R2F SDK that you wish to point to, be
careful to examine what files are linked and what files are copied into your
workspace from the SDK and adjust your project accordingly. For example, if you
are migrating code based on the Project Zero for CC2640R2F, be sure to reference
the new ble_user_config.c
, ble_user_config.h
and board files from the
target SDK.
Choose a BLE-Stack 3.02.00 example project that contains your target project’s base functionality.
For reference, see available sample projects that start with simple_peripheral
In this example, we’re going to use simple_peripheral as the starting BLE-Stack 3.02.00 sample project.
Transfer all modified application files from BLE-Stack 3.01.01 into the BLE-Stack 3.02.00 example project.
In this example, the following files from BLE-Stack 3.01.01 were moved into simple_peripheral BLE-Stack 3.02.00 example:
simple_peripheral.c
simple_peripheral.h
simple_gatt_profile.c
simple_gatt_profile.h
Update function name from
SimplePeripheral_createTask
toSimpleBLEPeripheral_createTask
inmain.c
. Please keep in mind that all the functions in this example were updated andBLE
keyword was removed. This also applies to all of theblestack
SDK examples.A new way of processing connection events was implemented. In order to take advantage of this new functionality do the following in
simple_peripheral.c
:Define an new event
SBP_CONN_EVT
such that theSimplePeripheral_connEvtCB
function can enqueue a message for the application task to handle:#define SBP_CONN_EVT 0x0010
Add the following macros:
// Set the register cause to the registration bit-mask #define CONNECTION_EVENT_REGISTER_BIT_SET(RegisterCause) (connectionEventRegisterCauseBitMap |= RegisterCause ) // Remove the register cause from the registration bit-mask #define CONNECTION_EVENT_REGISTER_BIT_REMOVE(RegisterCause) (connectionEventRegisterCauseBitMap &= (~RegisterCause) ) // Gets whether the current App is registered to the receive connection events #define CONNECTION_EVENT_IS_REGISTERED (connectionEventRegisterCauseBitMap > 0) // Gets whether the RegisterCause was registered to recieve connection event #define CONNECTION_EVENT_REGISTRATION_CAUSE(RegisterCause) (connectionEventRegisterCauseBitMap & RegisterCause )
Add the following function prototypes:
static void SimplePeripheral_connEvtCB(Gap_ConnEventRpt_t *pReport); static void SimplePeripheral_processConnEvt(Gap_ConnEventRpt_t *pReport);
And the functions definition add it at the end of the file. The callback function will push this event to application task so that the BLE-Stack API call can happen in the application context:
/********************************************************************* * @fn SimplePeripheral_processConnEvt * * @brief Process connection event. * * @param pReport pointer to connection event report */ static void SimplePeripheral_processConnEvt(Gap_ConnEventRpt_t *pReport) { if( CONNECTION_EVENT_REGISTRATION_CAUSE(FOR_ATT_RSP)) { // The GATT server might have returned a blePending as it was trying // to process an ATT Response. Now that we finished with this // connection event, let's try sending any remaining ATT Responses // on the next connection event. // Try to retransmit pending ATT Response (if any) SimplePeripheral_sendAttRsp(); } }
/********************************************************************* * @fn SimplePeripheral_connEvtCB * * @brief Connection event callback. * * @param pReport pointer to connection event report */ static void SimplePeripheral_connEvtCB(Gap_ConnEventRpt_t *pReport) { // Enqueue the event for processing in the app context. if( SimplePeripheral_enqueueMsg(SBP_CONN_EVT, 0 ,(uint8_t *) pReport) == FALSE) { ICall_freeMsg(pReport); } }
Add the following enum
connectionEventRegisterCause_u
to handle the registration of connection events. At the same time defineconnectionEventRegisterCauseBitMap
:typedef enum { NOT_REGISTER = 0, FOR_AOA_SCAN = 1, FOR_ATT_RSP = 2, FOR_AOA_SEND = 4, FOR_TOF_SEND = 8 }connectionEventRegisterCause_u; // Handle the registration and un-registration for the connection event, since only one can be registered. uint32_t connectionEventRegisterCauseBitMap = NOT_REGISTER; //see connectionEventRegisterCause_u
Two new
connectionEvent
functions were created, also these functions can be added at the end of the file./********************************************************************* * @fn SimplePeripheral_RegistertToAllConnectionEvent() * * @brief register to receive connection events for all the connection * * @param connectionEventRegisterCause represents the reason for registration * * @return @ref SUCCESS * */ bStatus_t SimplePeripheral_RegistertToAllConnectionEvent (connectionEventRegisterCause_u connectionEventRegisterCause) { bStatus_t status = SUCCESS; // in case there is no registration for the connection event, make the registration if (!CONNECTION_EVENT_IS_REGISTERED) { status = GAP_RegisterConnEventCb(SimplePeripheral_connEvtCB, GAP_CB_REGISTER, LINKDB_CONNHANDLE_ALL); } if(status == SUCCESS) { //add the reason bit to the bitamap. CONNECTION_EVENT_REGISTER_BIT_SET(connectionEventRegisterCause); } return(status); } /********************************************************************* * @fn SimplePeripheral_UnRegistertToAllConnectionEvent() * * @brief Unregister connection events * * @param connectionEventRegisterCause represents the reason for registration * * @return @ref SUCCESS * */ bStatus_t SimplePeripheral_UnRegistertToAllConnectionEvent (connectionEventRegisterCause_u connectionEventRegisterCause) { bStatus_t status = SUCCESS; CONNECTION_EVENT_REGISTER_BIT_REMOVE(connectionEventRegisterCause); // in case there is no more registration for the connection event than unregister if (!CONNECTION_EVENT_IS_REGISTERED) { GAP_RegisterConnEventCb(SimplePeripheral_connEvtCB, GAP_CB_UNREGISTER, LINKDB_CONNHANDLE_ALL); } return(status); }
In the function
SimpleBLEPeripheral_taskFxn
update the following code:// Check for BLE stack events first if (pEvt->signature == 0xffff) { // The GATT server might have returned a blePending as it was trying // to process an ATT Response. Now that we finished with this // connection event, let's try sending any remaining ATT Responses // on the next connection event. if (pEvt->event_flag & SBP_HCI_CONN_EVT_END_EVT) { // Try to retransmit pending ATT Response (if any) SimpleBLEPeripheral_sendAttRsp(); } } else { // Process inter-task message safeToDealloc = SimpleBLEPeripheral_processStackMsg((ICall_Hdr *)pMsg); }
with this one:
if (pEvt->signature != 0xffff) { // Process inter-task message safeToDealloc = SimplePeripheral_processStackMsg((ICall_Hdr *)pMsg); }
In the function
SimplePeripheral_processGATTMsg
update the following code:if (HCI_EXT_ConnEventNoticeCmd(pMsg->connHandle, selfEntity, SBP_HCI_CONN_EVT_END_EVT) == SUCCESS)
with this one:
if( SimplePeripheral_RegistertToAllConnectionEvent(FOR_ATT_RSP) == SUCCESS)
Lastly, to process the connection event
SBP_CONN_EVT
inSimpleBLEPeripheral_processAppMsg
add this new case:case SBP_CONN_EVT: { SimplePeripheral_processConnEvt((Gap_ConnEventRpt_t *)(pMsg->pData)); ICall_free(pMsg->pData); break; }
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC2640R2 SDK.
The following drivers have changed from BLE-Stack 3.01.01. Please see the changes to these drivers by comparing the supplied headers between those in simplelink_cc2640r2_sdk_1_50_00_58 and those in the SimpleLink CC2640R2 SDK.
ECDH
AESCCM
RF
NVS
SD
Attention
The display folder should in BLE-Stack 3.02.00 be included with the path
<ti/display/Display.h>
, not<ti/mw/display/Display.h>
.#include <ti/display/Display.h>
Refer to the Upgrade and Compatibility Information for additional information and the TI-RTOS examples included with SimpleLink CC2640R2 SDK.
For additional information on how BLE-Stack 3.02.00 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview
For any utilized TI Drivers, review `TI-RTOS Kernel Users Guide`_ and Driver APIs.