Simple Peripheral Secure Firmware
Table of Contents
Introduction
The simple_peripheral project implements a simple Bluetooth low energy peripheral device with GATT services and demonstrates the TI Simple Profile. This project can be a framework for developing many different peripheral-role applications. The Simple Peripheral project is used as the baseline for explaining the stack in the BLE-Stack User’s Guide for Bluetooth 4.2.
This project uses stack and app configurations that are summarized in the table below:
App Build Configuration | Compatible Stack Configuration | Description |
---|---|---|
FlashROM_StackLibrary | FlashROM_Library | Application build configuration linked to Stack library (fully executable) |
FlashROM_Library configurations use the stack library configuration, which is explained here.
This document discusses the procedure for using secure firmware with the Simple Peripheral application when the FlashROM_StackLibrary configurations are used.
Hardware Prerequisites
The default Simple Peripheral configuration uses the LAUNCHXL-CC2640R2. This hardware configuration is shown in the below image:
For custom hardware, see the Running the SDK on Custom Boards section of the BLE-Stack User’s Guide for Bluetooth 4.2.
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the Release Notes located in the docs/blestack folder. For information on how to import this project into your IDE workspace and build/run, please refer to The CC2640R2F Platform section in the BLE-Stack User’s Guide for Bluetooth 4.2.
The following projects/scripts from the SDK are used for the secure firmware demo:
- secure_fw (examples/rtos/CC2640R2_LAUNCHXL/blestack/secure_fw)
- simple_peripheral_secure_fw ( examples/rtos/CC2640R2_LAUNCHXL/blestack/simple_peripheral_secure_fw)
- secure_fw_tool.py (tools/blestack/secure_fw) ( Please refer to Secure Firmware Generation for usage instructions)
- Python ECDSA library if not already installed (using Python v2.7.11)
Out of box demo
- Build simple_peripheral_secure_fw to generate the application .bin file.
- Either copy private key file in PEM format to the folder where the secure_fw_tool.py exists or provide path to private key file using the handle -p in the arguments for the secure_fw_tool.py to generate secure bin file. See PEM File Generation for more info.
- Use secure_fw_tool.py with the path to the above generated .bin file (see instructions in Secure Firmware Generation) to generate the secure bin file. (ble_simple_peripheral_secure_fw_cc2640r2lp_app.bin is the name of the .bin file generated on running the script out of the box)
- Flash the secure bin file to the device using SmartRF Flash Programmer 2 at address 0x00000000.
- Build secure_fw and program to device using SmartRF Flash Programmer 2 at address 0x0001F000.
- If verification is successful, device behaves similar to the simple_peripheral project with an additional “Image Verified” printed on the UART display on startup as shown below:
- If verification is unsuccessful, view the error code for the reason of the failure.
- If SECURE_FW_ERASE_FLASH is set to true in secure_fw project, upon failure to verify secure header, the entire image firmware is erased and the error to page 1 at address 0x00001000.
- If SECURE_FW_ERASE_FLASH is set to false in secure_fw project, error code can be determined in the value of the variable “errorCode” in secure_fw_main.c using the debugger.
By default, SECURE_FW_ERASE_FLASH is set to false. The description of the error codes is listed below:
Code | Error reason |
---|---|
0x01 | Invalid magic word |
0x02 | Invalid firmware version (Currently not supported) |
0x03 | Invalid start/end address |
0x04 | Invalid length |
0x05 | Cert element not found |
0x06 | Verification failed |
0x07 | Self-verification failed (This feature is not supported currently) |
Python Script Usage
The SDK includes a script(secure_fw_tool.py) for generating the metadata required for the secure image. The user may also create another script to generate the private key as described in PEM File Generation.
Secure Firmware Generation
Usage: secure_fw_tool.py [-h] [-s STARTADDR] [-m MAGICWORD] [-b SECUREBIN] Inbin privateKey endAddr
Argument | Description |
---|---|
Inbin | Path to input application image in .bin format |
privateKey | Private key file in .pem format (see PEM File Generation) |
endAddr | End address of firmware |
-h | Show this help message and exit |
-s [STARTADDR] | Start address of firmware |
-m [MAGICWORD] | Magic word to identify start of image metadata |
-b [SECUREBIN] | Path to save secure bin file |
Example: python secure_fw_tool.py < input bin file > < path to private key file in .pem format > < end address from map file > python secure_fw_tool.py ble_simple_peripheral_secure_fw_cc2640r2lp_app_FlashROM_StackLibrary.bin private.pem 0000fc44
where the end address points to an image from simple_peripheral_secure_fw project. The example above will use default parameters for rest of the optional arguments. Default values used out of the box for secure_fw_tool.py:
- Private key : 139847857b5301c29a51bb8ef4aa259a99ed4b826400505c050b46ca78db560f
- Start address : 0x00000070
- End address : 0x0000ed24(CCS) 0x0000fc44(IAR)
- Length of image : 0x00017F90
- Magic Word : 574653204C42530A
- Secure bin file name: ble_simple_peripheral_secure_fw_cc2640r2lp_app.bin
End of firmware address points to the last address used by the firmware image. The end address can be determined from the simple_peripheral_secure_fw project map file as follows:
- CCS : End address is the address pointed by the symbol __TI_CINIT_Limit
- IAR : End address is two subtracted from the last address pointed by “Initializer bytes” before “A1”: SNVSECT section
PEM File Generation
The following python code can be used to generate the private key in PEM file format that is needed by the secure_fw_tool.py script:
from ecdsa import NIST256p
from ecdsa import SigningKey
import binascii
import array
pk = '\x13\x98\x47\x85\x7b\x53\x01\xc2\x9a\x51\xbb\x8e\xf4\xaa\x25\x9a\x99\xed\x4b\x82\x64\x00\x50\x5c\x05\x0b\x46\xca\x78\xdb\x56\x0f'
sk = SigningKey.from_string(pk,curve=NIST256p)
open("private.pem","w").write(sk.to_pem())
vk = sk.get_verifying_key()
print " Public Key " , binascii.hexlify(vk.to_string())