Simple Central
Table of Contents
Introduction
The simple_central project implements a simple Bluetooth low energy central device with GATT client functionality. This project can be run on various platforms, including the CC2640R2 Launchpad. By default, the simple_central application is configured to filter and connect to peripheral devices with the TI Simple Profile UUID. To modify this behavior, set DEFAULT_DEV_DISC_BY_SVC_UUID to FALSE in simple_central.
Hardware Prerequisites
The default Simple Central configuration uses the LAUNCHXL-CC2640R2. This hardware configuration is shown in the below image:
For custom hardware, see the Running the SDK on Custom Boards section of the BLE-Stack User’s Guide for Bluetooth 4.2.
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the Release Notes located in the docs/blestack folder. For information on how to import this project into your IDE workspace and build/run, please refer to The CC2640R2F Platform section in the BLE-Stack User’s Guide for Bluetooth 4.2.
Usage
This application uses the UART peripheral to provide an interface for the application. This document will use PuTTY to serve as the display for the output of the CC2640R2 LaunchPad. Note that any other serial terminal can be used. The following default parameters are used for the UART peripheral for display:
UART Param | Default Values |
---|---|
Baud Rate | 115200 |
Data length | 8 bits |
Parity | None |
Stop bits | 1 bit |
Flow Control | None |
Once the Simple Central sample application starts, the output to the terminal will report its address and the fact that it is initialized and ready to begin discovery, as shown below:
As shown, the right button (BTN-2 on the CC2640R2 LaunchPad) can be pressed to begin discovering devices that are broadcasting BLE advertisements. This will report the number of discovered devices:
The left button (BTN-1) can be pressed to go through the available devices. When you have found the device that you are trying to connect to, press the right button to connect. This will display information such as the MTU size and the address of the connected peripheral device, as well as the first of a list of options:
The red box shows the first of 4 options, which will be described in the following sections:
- GATT Read/Write
- Toggle Read RSSI
- Connection Update
- Disconnect
These options can be selected by pressing the right button.
Option: GATT Read/Write
This option is used to send read requests to the peripheral device and to write new values to the device. Pressing the right button once will send a read request to the peripheral device and will print the returned value:
Pressing it a second time will write a new value to the characteristic:
Pressing the button additional times will continue to alternate between reads and writes. Each time a write is sent, it increments the value by 1. Note that this option requires that the device has the TI Simple Profile UUID.
Option: Toggle Read RSSI
This option is used to get the RSSI (signal strength) of the connected peripheral device. Pressing the right button will toggle RSSI reads on and off. When it is on, the RSSI value will be printed. The value will continue to be updated as the RSSI changes:
Option: Connection Update
This option updates the connection parameters. These values can be set by changing the following constants in simple_central.c:
- DEFAULT_UPDATE_MIN_CONN_INTERVAL
- DEFAULT_UPDATE_MAX_CONN_INTERVAL
- DEFAULT_UPDATE_SLAVE_LATENCY
- DEFAULT_UPDATE_CONN_TIMEOUT
The “Param Update” value indicates whether the connection parameters have been updated successfully, with 0 indicating success. If, for example, you press the right button a second time before the connection update has completed, you will see the value 58 returned, indicating that the controller is busy.
Option: Disconnect
This option will terminate the connection. The following shows a successful disconnection:
Note that this application also supports MTU exchanges. This is done automatically by the Simple Central device after a connection is formed with a peripheral device. A larger MTU can be negotiated by changing MAX_PDU_SIZE. More information on this can be found in the Configuring for Larger MTU Values section of the BLE-Stack User’s Guide for Bluetooth 4.2.