Connection Monitor (CM) Examples Guide
Table of Contents
Introduction
The Connection Monitor (CM) projects showcase how to utilize the TI Micro BLE Stack as the connection monitor role. For more information on the TI Micro BLE Stack see BLE-Stack User’s Guide for Bluetooth 4.2.
There are two projects/configurations:
App Build Configuration | Description |
---|---|
CM_FlashOnly_MultiMode | Base application showing how to use Micro BLE Stack in the Connection Monitor Role |
uNPI_CM_FlashOnly_MultiMode | Same as the CM_FlashOnly_MultiMode project, with unified NPI built in to receive data from a host |
Hardware Prerequisites
Both CM_FlashOnly_MultiMode and uNPI_CM_FlashOnly_MultiMode is designed to use LAUNCHXL-CC2640R2.
2 additional LAUNCHXL-CC2640R2 will be required to create a connection to monitor. One of these launchpads will be running host_test or simple_central to act as a central, thus will need a computer capable of running BTool. Another launchpad will be flashed with simple_peripheral to act as a peripheral for host_test to connect to. This can be replaced with another peripheral, such as a phone.
- Two LAUNCHXL-CC2640R2 is required.
- One Computer able to utilize BTool and Serial Ports is required.
- One Peripheral is required. (Or an additional LAUNCHXL-CC2640R2)
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the Release Notes located in the docs/blestack folder. For information on how to import this project into your IDE workspace and build/run, please refer to The CC2640R2F Platform section in the BLE-Stack User’s Guide for Bluetooth 4.2.
In order to utilize ‘npi_cm_host.py’ for the uNPI_CM_FlashOnly_MultiMode configuration you will need a valid installation of
Required Python Modules
The ‘npi_cm_host.py’ script utilizes modules that need to be installed
The ‘requirements.txt’ contains a list of the modules required; can be used with
pip install -r requirements.txt
‘requirements.txt’ and ‘npi_cm_host.py’ are located in
/tools/blestack/connection_monitor/
Usage
Setup and User Guide For uNPI_CM_FlashOnly_MultiMode
Set Up
The uNPI_CM_FlashOnly_MultiMode project utilizes the UART peripheral through unified NPI. This requires the computer to be connected to the launchpad through the USB debugging interface. Flash uNPI_CM_FlashOnly_MultiMode project onto a launchpad and connect it the computer.
Flash another launchpad with the host_test project, connect this launchpad to the computer and launch BTool. Instructions can be found in Host Test Guide and BTool.
Each launchpad connected to the computer will enumerate as 2 COM ports. Always use the port labeled as “XDS110 Class Application/User UART”, this interfaces Application UART.
Take note of which COM port belongs to the launchpad running uNPI_CM_FlashOnly_MultiMode and which COM port belongs to the launchpad running host_test.
Optionally, if using a third launchpad as a peripheral - flash the final launchpad with simple_peripheral. After flashing is completed, record the Bluetooth Device Address. This can be found in the UART terminal. Once the Bluetooth Device Address is noted the launchpad is only required to be powered, no need to connect to the computer through the debugger.
Running the Script Manually with No Arguments
Some modifications to ‘npi_cm_host.py’ are required prior to running the project. These modifications are to configure the script to control the correct devices and connect host_test to the right peripheral.
- Update ‘host_port’ with the COM Port of the launchpad running host_test.
- Update ‘cm_port’ with the COM Port of the launchpad running uNPI_CM_FlashOnly_MultiMode.
- Update ‘strPeerAddress’ with the Bluetooth Device Address of the peripheral to be connected to.
- Run the script using Python. This requires calling the python executable with the path to ‘npi_cm_host.py’ passed in as an argument.
if __name__ == '__main__':
global peerAddrs
version_control()
rtn_args = parse_args()
if(len(sys.argv) < 4):
print '\nUsing Default Hardcoded Values: '
print 'or enter 3 default(cm_port host_port peerAddress) arguments.'
print 'See -h help.\n'
#set your own hard coded com ports
host_port = 'COM104'
cm_port = 'COM105'
strPeerAddress = '0xB0912265CBE2'
C:\Python27\python.exe [sdk]\tools\blestack\connection_monitor\npi_cm_host.py
Note ‘sdk’ refers to the Software Development Kit installation directory.
The script will send commands to the launchpad running host_test to act as a central device and connect to the peripheral. Then it will query the central for the current connection parameters. Finally it will launch the connection monitor with the retrieved connection parameters. A continues stream of RSSI data and timestamps from the connection monitor of master and slave devices at each connection event will appear in the terminal after a short delay. The default connection interval of connection events is 100ms.
Running the Python Script or Executable with Command Line arguments
To run the script without editing the python code, the configuration information can be passed into the script as arguments. A executable is also provided, allow the user to utilize uNPI_CM_FlashOnly_MultiMode project without having Python installed. Similar to the python script, arguments need to passed in when being invoked.
The arguments are expected to be in the following order:
Argument 1 | Argument 2 | Argument 3 |
---|---|---|
CM COM PORT | host_test COM PORT | Peripheral Bluetooth Address |
[sdk]\tools\blestack\connection_monitor\npi_cm_host.exe COM4 COM5 0xB0912265CBE2
Or alternatively the same command line will also work with a direct call to the python script.
C:\Python27\python.exe [sdk]\tools\blestack\connection_monitor\npi_cm_host.py COM4 COM5 0xB0912265CBE2
Note ‘sdk’ refers to the Software Development Kit installation directory.
The script will send commands to the launchpad running host_test to act as a central device and connect to the peripheral. Then it will query the central for the current connection parameters. Finally it will launch the connection monitor with the retrieved connection parameters. A continues stream of RSSI data and timestamps from the connection monitor of master and slave devices at each connection event will appear in the terminal after a short delay. The default connection interval of connection events is 100ms.
Additional Information
The script ‘npi_cm_host.py’ contains in-line comments - these comments describe script behavior.
Setup and User Guide For CM_FlashOnly_MultiMode
Set Up
CM_FlashOnly_MultiMode does not utilize unified NPI, thus has no transport layer interface to the UART Module. In order to configure the connection monitor, connection parameters must be manually placed into application code and compiled. Connect a launchpad which will be flashed with CM_FlashOnly_MultiMode to the computer. This will be the Connection Monitor launchpad.
Another launchpad will be acting as a central device. Flash this launchpad with simple_central and connect to it’s COM Port using a serial terminal emulator such as Putty. See Simple Central Guide for instructions on how to utilize and get the project working.
Optionally, if using a third launchpad as a peripheral - flash this final launchpad with simple_peripheral. After flashing is completed, record the Bluetooth Device Address. This can be found in the UART terminal. See Simple Peripheral Guide Once the Bluetooth Device Address is noted, the launchpad is only required to be powered, no need to connect to the computer through the debugger.
Form a connection between the simple_central and simple_peripheral through the simple_central’s two button interface. In other words, scan for devices, and connect to the advertising simple_peripheral by verifying the Bluetooth Device Address noted earlier.
Once a connection is formed, use the ‘Connection Info’ menu option to extract the Connection Information required by the Connection Monitor. Ensure that the connection is maintained.
Open the CM_FlashOnly_MultiMode project; in the ‘micro_cm_demo.c’ source file, the ‘MicroCmDemo_init’ function, input the Connection Information retrieved, such as the Access Address, Connection Interval, and Hop Value.
/* Initialize Connection Monitor */
if (ubCm_init() == true)
{
/*
* The ubCM_Start() is called here to kick off CM sessions as a demo.
* This API should be called from host uNPI once the uNPI host
* if available. The currentStartTime, access address, and scan duration
* are hard-coded. They should be provided by the host. In this demo, the
* very first ubCM_start() call will cover UB_MAX_MONITOR_DURATION.
*/
ubCMConnInfo.ArrayOfConnInfo[0].accessAddr = 0x87318ba3;
ubCMConnInfo.ArrayOfConnInfo[0].currentStartTime = 0;
ubCMConnInfo.ArrayOfConnInfo[0].nextStartTime = RF_getCurrentTime() + 100 * BLE_TO_RAT;
ubCMConnInfo.ArrayOfConnInfo[0].scanDuration = UB_MAX_MONITOR_DURATION; // 40.96s
ubCMConnInfo.ArrayOfConnInfo[0].connInterval = 1600;
ubCMConnInfo.ArrayOfConnInfo[0].hopValue = 15;
ubCMConnInfo.ArrayOfConnInfo[0].combSCA = 90; // Master+Slave = 50+40
ubCMConnInfo.ArrayOfConnInfo[0].chanMap[0] = 0xFF;
ubCMConnInfo.ArrayOfConnInfo[0].chanMap[1] = 0xFF;
ubCMConnInfo.ArrayOfConnInfo[0].chanMap[2] = 0xFF;
ubCMConnInfo.ArrayOfConnInfo[0].chanMap[3] = 0xFF;
ubCMConnInfo.ArrayOfConnInfo[0].chanMap[4] = 0x1F;
Build the project and flash the Connection Monitor launchpad with the updated CM_FlashOnly_MultiMode project.
Observing the Monitored Information
Open Putty on the computer, and connect to the “XDS110 Class Application/User UART” COM Port that corresponds to the Connection Monitor launchpad. After about 40 seconds RSSI and timestamp information should appear as the Connection Monitor launchpad following the connection between the central and the peripheral.