360 #ifndef ti_drivers_uart_UARTCC26XX__include 361 #define ti_drivers_uart_UARTCC26XX__include 375 #include <ti/devices/DeviceFamily.h> 376 #include DeviceFamily_constructPath(driverlib/uart.h) 378 #include <ti/drivers/dpl/HwiP.h> 379 #include <ti/drivers/dpl/SwiP.h> 380 #include <ti/drivers/dpl/ClockP.h> 381 #include <ti/drivers/dpl/SemaphoreP.h> 414 #define UARTCC26XX_CMD_RETURN_PARTIAL_ENABLE UART_CMD_RESERVED + 0 423 #define UARTCC26XX_CMD_RETURN_PARTIAL_DISABLE UART_CMD_RESERVED + 1 431 #define UARTCC26XX_CMD_RX_FIFO_FLUSH UART_CMD_RESERVED + 2 435 #define UARTCC26XX_FIFO_SIZE 32 438 #define UARTCC26XX_RETURN_PARTIAL_ENABLE UARTCC26XX_CMD_RETURN_PARTIAL_ENABLE 439 #define UARTCC26XX_RETURN_PARTIAL_DISABLE UARTCC26XX_CMD_RETURN_PARTIAL_DISABLE uint8_t rtsPin
Definition: UARTCC26XX.h:511
UARTCC26XX Hardware attributes.
Definition: UARTCC26XX.h:485
UART_Mode readMode
Definition: UARTCC26XX.h:551
Definition: UARTCC26XX.h:522
Power_NotifyObj uartPostObj
Definition: UARTCC26XX.h:595
uint32_t baudRate
Baud rate for CC26xx UART.
Definition: UARTCC26XX.h:567
const void * writeBuf
Definition: UARTCC26XX.h:574
size_t writeSize
Definition: UARTCC26XX.h:576
Definition: UARTCC26XX.h:540
enum UART_PAR_ UART_PAR
UART parity type settings.
enum UART_LEN_ UART_LEN
UART data length settings.
const UART_FxnTable UARTCC26XX_fxnTable
RingBuf_Object ringBuffer
Definition: UARTCC26XX.h:586
enum UART_Mode_ UART_Mode
UART mode settings.
Definition: UARTCC26XX.h:536
Power notify object structure.
Definition: Power.h:115
uint8_t writeFifoThreshold
Definition: UARTCC26XX.h:585
SemaphoreP_Struct readSem
Definition: UARTCC26XX.h:601
size_t readSize
Definition: UARTCC26XX.h:583
Definition: UARTCC26XX.h:524
unsigned int readTimeout
Definition: UARTCC26XX.h:553
bool readRetPartial
Definition: UARTCC26XX.h:580
void * uartPostFxn
Definition: UARTCC26XX.h:593
UART_ReturnMode readReturnMode
Definition: UARTCC26XX.h:557
UART_Status
UART status.
Definition: UARTCC26XX.h:521
Definition: UARTCC26XX.h:526
UARTCC26XX Object.
Definition: UARTCC26XX.h:548
UART_Callback readCallback
Definition: UARTCC26XX.h:555
UART_PAR parityType
Definition: UARTCC26XX.h:570
Definition: UARTCC26XX.h:525
size_t readCount
Definition: UARTCC26XX.h:582
UART_LEN dataLength
Definition: UARTCC26XX.h:568
Definition: UARTCC26XX.h:538
UART_FifoThreshold readFifoThreshold
Definition: UARTCC26XX.h:584
Device-specific pin & GPIO driver for CC26xx family [def].
struct UARTCC26XX_HWAttrsV2 UARTCC26XX_HWAttrsV2
UARTCC26XX Hardware attributes.
HwiP_Struct hwi
Definition: UARTCC26XX.h:598
SemaphoreP_Struct writeSem
Definition: UARTCC26XX.h:600
ClockP_Struct txFifoEmptyClk
Definition: UARTCC26XX.h:602
uint32_t baseAddr
Definition: UARTCC26XX.h:486
int intNum
Definition: UARTCC26XX.h:488
UART_Status status
Definition: UARTCC26XX.h:571
Definition: UARTCC26XX.h:527
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:652
size_t writeCount
Definition: UARTCC26XX.h:575
unsigned int writeTimeout
Definition: UARTCC26XX.h:554
bool opened
Definition: UARTCC26XX.h:550
uint8_t intPriority
UART Peripheral's interrupt priority.
Definition: UARTCC26XX.h:501
size_t ringBufSize
Definition: UARTCC26XX.h:513
uint8_t rxPin
Definition: UARTCC26XX.h:509
unsigned char * ringBufPtr
Definition: UARTCC26XX.h:512
UART_STOP stopBits
Definition: UARTCC26XX.h:569
bool writeCR
Definition: UARTCC26XX.h:577
Definition: UARTCC26XX.h:523
Definition: UARTCC26XX.h:539
underlying data structure for type PIN_State
Definition: PIN.h:680
UART_Mode writeMode
Definition: UARTCC26XX.h:552
enum UART_STOP_ UART_STOP
UART stop bit settings.
enum UART_ReturnMode_ UART_ReturnMode
UART return mode settings.
SwiP_Struct swi
Definition: UARTCC26XX.h:599
void * readBuf
Definition: UARTCC26XX.h:581
UART_DataMode readDataMode
Definition: UARTCC26XX.h:558
struct UARTCC26XX_Object * UARTCC26XX_Handle
UART_DataMode writeDataMode
Definition: UARTCC26XX.h:559
PIN_State pinState
Definition: UARTCC26XX.h:589
uint8_t ctsPin
Definition: UARTCC26XX.h:510
struct UARTCC26XX_Object UARTCC26XX_Object
UARTCC26XX Object.
Definition: UARTCC26XX.h:537
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: UARTCC26XX.h:507
UART_Callback writeCallback
Definition: UARTCC26XX.h:556
uint32_t powerMngrId
Definition: UARTCC26XX.h:487
PIN_Handle hPin
Definition: UARTCC26XX.h:590
UART_FifoThreshold
UART FIFO threshold.
Definition: UARTCC26XX.h:535
void(* UART_Callback)(UART_Handle handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:438
uint8_t txPin
Definition: UARTCC26XX.h:508
enum UART_DataMode_ UART_DataMode
UART data mode settings.