SimpleLink™ CC13x2 SDK 2.20.00.71 Change log
Table of Contents
New Features
TI 15.4 Stack
TI154STACK-1947 |
DMM 15.4 FH + BLE Peripheral enabled support for SLR mode |
TI154STACK-1919 |
Enabled 15.4 Stack support on CC1352 P4 |
TI154STACK-1854 |
DMM: 15.4 Sensor Sub-1 FH + BLE Peripheral Example enabled on CC1352 |
TI Proprietary-RF
TI154STACK-1854 |
DMM: 15.4 Sensor Sub-1 FH + BLE Peripheral Example enabled on CC1352 |
EZLINKPROP-344 |
Enable whitening for SLR mode |
EZLINKPROP-333 |
Replace all CC13XX_LAUNCHXL_BOARD_H with new board definitions |
EZLINKPROP-323 |
Update termination reasons for rfPacktTx and rfPacketRx examples |
EZLINKPROP-314 |
CC1352P-2: Create baseline set of examples for P-2 |
EZLINKPROP-299 |
Proprietary 2.4GHz support in EasyLink examples for CC2640R2 |
EZLINKPROP-290 |
Increase concentrator Ack delay |
EZLINKPROP-277 |
EasyLink WSN project using SLR mode for OAD on CC13x2 |
BLE5-Stack
TI Thread
TIOP-302 |
Setup power tables and internal PA |
TI-RTOS and Drivers
This release previews a new tool coming out called SysConfig, which allows graphical configuration of TI’s drivers. For more information, see the README file included in the syscfg directory as well as the Wiki page located here.
TIRTOS-1493 |
Add ENFILE to errno |
TIRTOS-1481 |
Add examples for CC1352P-2_ LAUNCHXL LaunchPad |
TIRTOS-1480 |
Add examples for CC1352P-4_ LAUNCHXL LaunchPad |
TIRTOS-1479 |
Add board files for CC1352P-2 LaunchPad |
TIRTOS-1474 |
Add board files for CC1352P - 433 MHz (China band) Launchpad in Core SDK |
TIDRIVERS-1572 |
Add CC1352P-2 LP board file |
TIDRIVERS-1547 |
WatchdogCC26XX: Update documentation to clarify which context the callback is called in |
TIDRIVERS-1483 |
remove ti/mw directory from the Core SDK product (stale and unused) |
TIDRIVERS-1463 |
Avoid context switches in CC26X2 AESCCM, AESECB, SHA2 polling return behaviour |
TIDRIVERS-1461 |
Improve CC26X2 AESCCM, AESECB, SHA2 error handling |
TIDRIVERS-1448 |
Add support for 8kHz PCM sampling rate |
TIDRIVERS-1445 |
EC-JPAKE preprocess hash mod n for easier Thread integration |
TIDRIVERS-1427 |
CC26XX power constraints have inconsistent names |
TIDRIVERS-1403 |
Check CryptoSem inside CryptoCC26XX_init() |
TIDRIVERS-1347 |
Refactor PowerCC26X2_calibrateRCOSC.c to make use of SCLKMF |
TIDRIVERS-1313 |
Need board file and linker files for CC1352P 433MHz LP |
TIDRIVERS-1229 |
Create generic TRNG driver |
Fixed Issues
TI 15.4 Stack
TI154STACK-1954 |
Fixed issue on TI 15.4 examples where sensor joins the network when PermitJoin-Off is set when configured in FH mode |
TI154STACK-1953 |
Fixed TI 15.4 sensor to go to sleep (standby) after second orphan scan wakeup |
TI154STACK-1944 |
Fixed warnings generated in mac_radio.c when FREQ_2_4G is used |
TI154STACK-1924 |
Fixed issue with auto start in 15.4 sub-1 Stack Sensor/Collector |
TI154STACK-1823 |
Fixed default collector TX power to max on CC13x0 and CC1352R1. |
TI Proprietary-RF
EZLINKPROP-369 |
PER: High Speed Mode Throughput drops precipitously for 254 byte transmissions |
EZLINKPROP-348 |
Easylink init should exclude devices from phy modes it does not support |
EZLINKPROP-337 |
rfEasyLinkRx does not work when using optimization -Os with GCC |
EZLINKPROP-308 |
Missing Ack over air from Concentrator in SLR mode. |
EZLINKPROP-298 |
Change pastTrig when triggertype is TRIG_NOW in rfPacketTX |
EZLINKPROP-292 |
EasyLink WSN: Source code output path and chip name are incorrect |
EZLINKPROP-266 |
rfWakeonRadio examples does not work for high datarates |
EZLINKPROP-233 |
oad_protocol.h have all pointers wrongly named |
BLE5-Stack
BLESTACK-3840 |
Fixed an issue where some smartphones would disconnect when switching to the 2M PHY if the suggested Data Length Extension TX values were not the maximum 251 bytes / 2120 us |
BLESTACK-3478 |
Fixed an issue where a connection could drop if a LL connection parameter update request reject indication is received during a connection |
TI Thread
TIOP-323 |
ccs cloud cannot build projects with GCC compiler |
TIOP-321 |
CC1352P-2 power table support on CC1352P1 |
TIOP-314 |
Some settings not restored on reset |
TIOP-311 |
Temperature sensor device does not go to sleep for cc2652 as well as cc1352 |
TIOP-268 |
Examples include Thread specific RF Driver |
TI-RTOS and Drivers
TIDRIVERS-1626 |
Race condition in PowerCC26X2_calibrateRCOSC |
Known Issues
TI 15.4 Stack
TI Proprietary-RF
BLE5-Stack
BLESTACK-3844 |
AE and legacy advertising sets number is limited to 20 |
BLESTACK-3843 |
RTOS logging of certain high-priority events, such as SWIs and HWIs, may interfere with reception of a scan response chain |
BLESTACK-3842 |
The NV Driver is now used for SNV record & bond storage. It is not possible to retain OSAL SNV contents when upgrading from earlier BLE5 1.1.x releases. Two flash pages of NV are required. |
BLESTACK-3813 |
Simple Central:start RSSI reading sometimes receive RSSI –127 dbm |
BLESTACK-3530 |
While using maximum 8 simultaneous connections, connection stability may be encountered after 6 master-initiated connections |
BLESTACK-2958 |
When using multi-role, there exists an issue where a random address will display instead of the “Work With” selection in the serial terminal |
BLESTACK-2446 |
IAR: The global custom.argvars and local ble project custom.argvars cannot coexist together |
TI Thread
TI-RTOS and Drivers
TIRTOS-476 |
POSIX threads render as single task in execution graph |