Terms and Definitions¶
General Terms and Acronyms¶
- CCFG
- Customer Configuration
- Customer Configuration is set by the application and contains configuration parameters for the ROM boot code, device hardware, and device firmware. It contains lock-bits on the last page of flash. You can read more in the Customer Configuration section in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
- CCS
- Code Composer Studio
- An integrated development environment to develop applications for Texas Instruments embedded processors. Download: Code Composer Studio
- cJTAG
- Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG (compact JTAG).
- GCC
- GNU Compiler Collection
- A compiler system produced by the GNU Project, which support various programming languages such as C and C++.
- GPRAM
- General purpose RAM. This memory area is used for the cache per default, but can be configured to be used as RAM.
- HIB
- Halt In Boot
- A mechanism in CC13xx and CC26xx devices to ensure that the external emulator can take control of the device before it executes any application code.
- IAR
- Refers to IAR Systems’ IAR Embedded Workbench, which is an integrated development environment used for building and debugging embedded applications.
- JTAG
- IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG (Joint Test Action Group).
- MCU
- Microcontroller Unit
- A small computer on a single integrated circuit.
- NVS
- Non-Volatile Storage
- Storage of data in non-volatile memory (NVM). NVM retains saved data during power cycles. In the context of CC13x2 and CC26x2 devices, NVM either refers to the internal flash or some external flash.
- OAD
- Over the Air Download
- The process of performing a device firmware update over the air.
- ROM
- Read-only Memory
- Type of non-volatile memory used in computers. Once data is written to ROM, the data cannot be removed and can only be read.
- RTSC
- Real Time Software Components
- A toolset for creating reusable code, used by TI-RTOS. See RTSC and RTSC-Pedia.
- SysConfig
- System Configuration Tool
- SysConfig is a graphical interface for configuring software projects. Configuration files, C source files and header files are generated based on the parameters configured in the SysConfig dashboard. See Get started with SysConfig.
- TI-CGT
- TI Code Generation Tools
- Set of C/C++ Compilers and Assembly Language tools for many TI microcontrollers and processors. For more information, see TI Code Generation Tools.
- TI-CLANG
- TI Arm Clang Compiler Toolchain
- The TI Arm Clang Compiler Toolchain (tiarmclang) is the next generation TI Arm compiler, replacing the previous TI Arm Compiler Tools (armcl). You can use the tiarmclang compiler toolchain to build applications from C, C++, and/or assembly source files to be loaded and run on one of the Cortex-M or Cortex-R Arm processors that are supported by the toolchain. You can find more information here.
- VIMS
- Versatile Instruction Memory System
- A system control module that handles access to the device memory areas from the CPU and system bus. You can read more in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
- .bss
- Block started by symbol. This memory section usually contains uninitialized variables including the task stacks.
Thread Terms and Acronyms¶
- CCA
- Clear Channel Assessment
- Used to determine wheter an RF medium is idle or busy. A combination of carrier sensing and energy detection is used to draw a conclusion.
- CoAP
- Constrained Application Protocol
- A specialized web transfer protocol for use with constrained nodes and constrained networks, which provides a request/response interaction model between application endpoints. Defined by RFC7252.
- DHCPv6
- Dynamic Host Configuration Protocol for IPv6
- Networking protocol for configuring IPv6 nodes with IPv6 addresses. Defined by RFC3315.
- FCC
- Federal Communications Commission
- A U.S. regulatory body for regulating interstate communications by radio, television, wire, satelitte, and cable.
- FED
- Full Thread Device
- An FTD acting as an End Device. Cannot be promoted to a Router.
- FFD
- Full Functionality Device
- A device in a PAN which implements the general communication model, and can therefore operate at all levels of functionality.
- FTD
- Full Thread Device
- A Thread device which contains the full implementation of a Thread stack.
- ICMPv6
- Internet Control Message Protocol for IPv6
- Error-reporting support protocol in the IP suite, used for diagnostics or for generating error messages to the source IP address when network problems occur. Defined by RFC4443.
- IEEE
- Institute of Electrical and Electronics Engineers
- An organization composed of engineers, scientists, and students. Develops standards for the computer and electronics industry.
- MED
- Minimal End Device
- An MTD acting as an End Device. The receiver is on when idle.
- ML-EID
- Mesh-Local Endpoint Identifier
- An Endpoint Identifier that is unique to a Thread device in a Thread network, regardless of network topology.
- MTD
- Minimal Thread Device
- A Thread device which contains a subset implementation of a Thread stack.
- NCP
- Network Co-Processor
- An architectural design where the application layer runs on a host processor and Thread features on the SoC. Communication between the host and SoC is via some serial connection.
- PAN
- Personal Area Network
- A network of techology devices focues around the area of an individual person.
- PER
- Packet Error Rate
- Represents the ratio between number of incorrectly received data packets and total number of transmitted data packets, often achieved by sending sequenced data packets.
- PIB
- PAN Information Bases
- Object of data related to describe or maintain IEEE 802.15.4 PHY or MAC.
- REED
- Router-Eligible End Device
- An FTD which is not actively participating as a Router, but can be promoted to a Router.
- RLOC
- Routing Locator
- An RLOC is an IPv6 unicast address which identifies the location of a device in a Thread network. It is used for efficiently routing a message across the network, and changes to accommodate network topology changes. The lower 16 bits of the RLOC, RLOC16, is used as the device’s 802.15.4 short address.
- RFD
- Reduced Functionality Device
- A device in a PAN which implements a reduced communication model, and can therefore operate at redcued levels of functionality.
- Router
- An FTD which is actively participating in routing of the Thread network.
- SED
- Sleepy End Device
- An MTD acting as an End Device. The receiver is off when idle.
- SLAAC
- Stateless Address Autoconfiguration
- A mechanism for devices in an IPv6 network to autoconfigure its IPv6 interfaces. Defined by RFC4862.
- SoC
- System-on-Chip
- A single-chip solution that integrates all components of an electronic system. In the context of Thread, a system which combines an IEEE 802.15.4 radio and a processor.
- UDP
- User Datagram Protocol
- Transport layer protocol used for low-latency and lossy connections between application programs in IP networks. Defined by RFC768.
- ULA
- Unique Local Address
- An IPv6 address that is guaranteed to be unique for a device in a specified scope. For example, an ML-EID is a ULA for the mesh-local scope.
- URI
- Uniform Resource Identifier
- A string of characters used to unambiguously identify an abstract or physical resource. Defined by RFC3986.
TI-RTOS Terms and Acronyms¶
- HWI
- Hardware Interrupts
- A TI-RTOS hardware interrupt.
- Idle Task
- A TI-RTOS default task that is executes when no other higher priority thread needs to run.
- RCFG
- TI-RTOS in ROM configuration table.
- ROV
- Runtime Object View
- A TI-RTOS kernel plugin for CCS and IAR to view a target’s instrumentation data.
- RTC
- Real-Time Clock
- An accurate computer clock which keeps track of the current time.
- RTOS
- Real Time Operating System
- An operating system intended to serve applications with real-time requirements.
- SWI
- Software Interrupts
- A TI-RTOS software interrupt.
- TI-RTOS
- Texas Instruments Real Time Operating System
- An RTOS developed by TI for TI microcontrollers.
- Zero-Latency Interrupts
- An interrupt that will not be routed through the TI-RTOS kernel’s Hwi dispatcher. For more information, see the Hwi module documentation in the TI-RTOS Kernel API Reference .
Over-the-Air Download (OAD) Terms and Acronyms¶
- BIM
- Boot Image Manager
- A bootloader that runs after the device’s ROM startup code. The BIM is responsible for analyzing the image header of all images and determining the most suitable image to run. Once the BIM has found the proper image, it will jump to it’s program entry.
- CRC
- Cyclic Redundancy Check
- An error-detecting code used to check the integrity of blocks of data.
- ECDSA
- Elliptic Curve Digital Signature Algorithm
- A variant of the Digital Signature Algorithm (DSA) which uses elliptic curve cryptography.
- Factory Image
- The factory image is a “golden” image that resides in external flash as a fail-safe mechanism.
- HIB
- Halt In Boot
- A mechanism in CC26xx and CC13xx devices to ensure that the external emulator can take control of the device before it executes any application code.
- OAD
- Over-the-Air Download
- The process of performing a device firmware update over the air.
- OAD Target
- The device whose firmware is being upgraded over the air. This is assumed to be a CC26xx or CC13xx device running the TI protocol-specific transport for OAD.
- OAD Distributor
- The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD Target.
Sensor Controller Terms and Acronyms¶
- SC
- Sensor Controller
- A dedicated 16-bit CPU core on CC13xx and CC26xx devices, located in the auxiliary (AUX) power/clock domain. It can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power states.
- SCS
- Sensor Controller Studio
- A stand-alone IDE used to write, test and debug code for the Sensor Controller.