TI BLE5-Stack API Documentation  2.02.00.00
hci.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  Group: WCS, BTS
4  $Target Device: DEVICES $
5 
6  ******************************************************************************
7  $License: TISD 2009 $
8  ******************************************************************************
9  $Release Name: PACKAGE NAME $
10  $Release Date: PACKAGE RELEASE DATE $
11  *****************************************************************************/
12 
317 #ifndef HCI_H
318 #define HCI_H
319 
320 #ifdef __cplusplus
321 extern "C"
322 {
323 #endif
324 
325 /*
326  * INCLUDES
327  */
328 #include "bcomdef.h"
329 #include "osal.h"
330 #include "ll_common.h"
331 #include "hal_assert.h"
332 
333 /*
334  * MACROS
335  */
336 
337 /*
338  * CONSTANTS
339  */
340 
351 #define HCI_SUCCESS 0x00
352 #define HCI_ERROR_CODE_UNKNOWN_HCI_CMD 0x01
353 #define HCI_ERROR_CODE_UNKNOWN_CONN_ID 0x02
354 #define HCI_ERROR_CODE_HW_FAILURE 0x03
355 #define HCI_ERROR_CODE_PAGE_TIMEOUT 0x04
356 #define HCI_ERROR_CODE_AUTH_FAILURE 0x05
357 #define HCI_ERROR_CODE_PIN_KEY_MISSING 0x06
358 #define HCI_ERROR_CODE_MEM_CAP_EXCEEDED 0x07
359 #define HCI_ERROR_CODE_CONN_TIMEOUT 0x08
360 #define HCI_ERROR_CODE_CONN_LIMIT_EXCEEDED 0x09
361 #define HCI_ERROR_CODE_SYNCH_CONN_LIMIT_EXCEEDED 0x0A
362 #define HCI_ERROR_CODE_ACL_CONN_ALREADY_EXISTS 0x0B
363 #define HCI_ERROR_CODE_CMD_DISALLOWED 0x0C
364 #define HCI_ERROR_CODE_CONN_REJ_LIMITED_RESOURCES 0x0D
365 #define HCI_ERROR_CODE_CONN_REJECTED_SECURITY_REASONS 0x0E
366 #define HCI_ERROR_CODE_CONN_REJECTED_UNACCEPTABLE_BDADDR 0x0F
367 #define HCI_ERROR_CODE_CONN_ACCEPT_TIMEOUT_EXCEEDED 0x10
368 #define HCI_ERROR_CODE_UNSUPPORTED_FEATURE_PARAM_VALUE 0x11
369 #define HCI_ERROR_CODE_INVALID_HCI_CMD_PARAMS 0x12
370 #define HCI_ERROR_CODE_REMOTE_USER_TERM_CONN 0x13
371 #define HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES 0x14
372 #define HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF 0x15
373 #define HCI_ERROR_CODE_CONN_TERM_BY_LOCAL_HOST 0x16
374 #define HCI_ERROR_CODE_REPEATED_ATTEMPTS 0x17
375 #define HCI_ERROR_CODE_PAIRING_NOT_ALLOWED 0x18
376 #define HCI_ERROR_CODE_UNKNOWN_LMP_PDU 0x19
377 #define HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE 0x1A
378 #define HCI_ERROR_CODE_SCO_OFFSET_REJ 0x1B
379 #define HCI_ERROR_CODE_SCO_INTERVAL_REJ 0x1C
380 #define HCI_ERROR_CODE_SCO_AIR_MODE_REJ 0x1D
381 #define HCI_ERROR_CODE_INVALID_LMP_PARAMS 0x1E
382 #define HCI_ERROR_CODE_UNSPECIFIED_ERROR 0x1F
383 #define HCI_ERROR_CODE_UNSUPPORTED_LMP_PARAM_VAL 0x20
384 #define HCI_ERROR_CODE_ROLE_CHANGE_NOT_ALLOWED 0x21
385 #define HCI_ERROR_CODE_LMP_LL_RESP_TIMEOUT 0x22
386 #define HCI_ERROR_CODE_LMP_ERR_TRANSACTION_COLLISION 0x23
387 #define HCI_ERROR_CODE_LMP_PDU_NOT_ALLOWED 0x24
388 #define HCI_ERROR_CODE_ENCRYPT_MODE_NOT_ACCEPTABLE 0x25
389 #define HCI_ERROR_CODE_LINK_KEY_CAN_NOT_BE_CHANGED 0x26
390 #define HCI_ERROR_CODE_REQ_QOS_NOT_SUPPORTED 0x27
391 #define HCI_ERROR_CODE_INSTANT_PASSED 0x28
392 #define HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED 0x29
393 #define HCI_ERROR_CODE_DIFFERENT_TRANSACTION_COLLISION 0x2A
394 #define HCI_ERROR_CODE_RESERVED1 0x2B
395 #define HCI_ERROR_CODE_QOS_UNACCEPTABLE_PARAM 0x2C
396 #define HCI_ERROR_CODE_QOS_REJ 0x2D
397 #define HCI_ERROR_CODE_CHAN_ASSESSMENT_NOT_SUPPORTED 0x2E
398 #define HCI_ERROR_CODE_INSUFFICIENT_SECURITY 0x2F
399 #define HCI_ERROR_CODE_PARAM_OUT_OF_MANDATORY_RANGE 0x30
400 #define HCI_ERROR_CODE_RESERVED2 0x31
401 #define HCI_ERROR_CODE_ROLE_SWITCH_PENDING 0x32
402 #define HCI_ERROR_CODE_RESERVED3 0x33
403 #define HCI_ERROR_CODE_RESERVED_SLOT_VIOLATION 0x34
404 #define HCI_ERROR_CODE_ROLE_SWITCH_FAILED 0x35
405 #define HCI_ERROR_CODE_EXTENDED_INQUIRY_RESP_TOO_LARGE 0x36
406 #define HCI_ERROR_CODE_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST 0x37
407 #define HCI_ERROR_CODE_HOST_BUSY_PAIRING 0x38
408 #define HCI_ERROR_CODE_CONN_REJ_NO_SUITABLE_CHAN_FOUND 0x39
409 #define HCI_ERROR_CODE_CONTROLLER_BUSY 0x3A
410 #define HCI_ERROR_CODE_UNACCEPTABLE_CONN_PARAMETERS 0x3B
411 #define HCI_ERROR_CODE_DIRECTED_ADV_TIMEOUT 0x3C
412 #define HCI_ERROR_CODE_CONN_TERM_MIC_FAILURE 0x3D
413 #define HCI_ERROR_CODE_CONN_FAILED_TO_ESTABLISH 0x3E
414 #define HCI_ERROR_CODE_MAC_CONN_FAILED 0x3F
415 #define HCI_ERROR_CODE_COARSE_CLOCK_ADJUST_REJECTED 0x40
416 #define HCI_ERROR_CODE_TYPE0_SUBMAP_NOT_DEFINED 0x41
417 #define HCI_ERROR_CODE_UNKNOWN_ADVERTISING_IDENTIFIER 0x42
418 #define HCI_ERROR_CODE_LIMIT_REACHED 0x43
419 #define HCI_ERROR_CODE_OPERATION_CANCELLED_BY_HOST 0x44
420 
426 #define HCI_MAX_NUM_CMD_BUFFERS LL_MAX_NUM_CMD_BUFFERS
427 #if defined(CC2540) || defined(CC2541) || defined(CC2541S)
428 #define HCI_MAX_NUM_DATA_BUFFERS LL_MAX_NUM_DATA_BUFFERS //<! Max Num Data Buffers
429 #endif // CC2540 | CC2541 | CC2541S
430 
434 // Send Data Packet Boundary Flags
435 #define FIRST_PKT_HOST_TO_CTRL LL_DATA_FIRST_PKT_HOST_TO_CTRL
436 #define CONTINUING_PKT LL_DATA_CONTINUATION_PKT
437 #define FIRST_PKT_CTRL_TO_HOST LL_DATA_FIRST_PKT_CTRL_TO_HOST
438 
439 
441 #define HCI_RSSI_NOT_AVAILABLE LL_RSSI_NOT_AVAILABLE
442 
447 #define HCI_DISCONNECT_AUTH_FAILURE HCI_ERROR_CODE_AUTH_FAILURE
448 #define HCI_DISCONNECT_REMOTE_USER_TERM HCI_ERROR_CODE_REMOTE_USER_TERM_CONN
449 #define HCI_DISCONNECT_REMOTE_DEV_LOW_RESOURCES HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES
450 #define HCI_DISCONNECT_REMOTE_DEV_POWER_OFF HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF
451 #define HCI_DISCONNECT_UNSUPPORTED_REMOTE_FEATURE HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE
452 #define HCI_DISCONNECT_KEY_PAIRING_NOT_SUPPORTED HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED
453 #define HCI_DISCONNECT_UNACCEPTABLE_CONN_INTERVAL HCI_ERROR_CODE_UNACCEPTABLE_CONN_INTERVAL
454 
460 // Tx Power Types
461 #define HCI_READ_CURRENT_TX_POWER_LEVEL LL_READ_CURRENT_TX_POWER_LEVEL
462 #define HCI_READ_MAX_TX_POWER_LEVEL LL_READ_MAX_TX_POWER_LEVEL
463 
469 #define HCI_CTRL_TO_HOST_FLOW_CTRL_OFF 0
470 #define HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_OFF 1
471 #define HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_OFF_SYNCH_ON 2
472 #define HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_ON 3
473 
479 #define HCI_PUBLIC_DEVICE_ADDRESS LL_DEV_ADDR_TYPE_PUBLIC
480 #define HCI_RANDOM_DEVICE_ADDRESS LL_DEV_ADDR_TYPE_RANDOM
481 
487 #define HCI_CONNECTABLE_UNDIRECTED_ADV LL_ADV_CONNECTABLE_UNDIRECTED_EVT
488 #define HCI_CONNECTABLE_DIRECTED_HDC_ADV LL_ADV_CONNECTABLE_DIRECTED_HDC_EVT
489 #define HCI_SCANNABLE_UNDIRECTED LL_ADV_SCANNABLE_UNDIRECTED_EVT
490 #define HCI_NONCONNECTABLE_UNDIRECTED_ADV LL_ADV_NONCONNECTABLE_UNDIRECTED_EVT
491 #define HCI_CONNECTABLE_DIRECTED_LDC_ADV LL_ADV_CONNECTABLE_DIRECTED_LDC_EVT
492 
498 #define HCI_ADV_CHAN_37 LL_ADV_CHAN_37
499 #define HCI_ADV_CHAN_38 LL_ADV_CHAN_38
500 #define HCI_ADV_CHAN_39 LL_ADV_CHAN_39
501 #define HCI_ADV_CHAN_ALL (LL_ADV_CHAN_37 | LL_ADV_CHAN_38 | LL_ADV_CHAN_39)
502 
508 #define HCI_ADV_WL_POLICY_ANY_REQ LL_ADV_WL_POLICY_ANY_REQ
509 #define HCI_ADV_WL_POLICY_WL_SCAN_REQ LL_ADV_WL_POLICY_WL_SCAN_REQ
510 #define HCI_ADV_WL_POLICY_WL_CONNECT_IND LL_ADV_WL_POLICY_WL_CONNECT_IND
511 #define HCI_ADV_WL_POLICY_WL_ALL_REQ LL_ADV_WL_POLICY_WL_ALL_REQ
512 
518 #define HCI_ENABLE_ADV LL_ADV_MODE_ON
519 #define HCI_DISABLE_ADV LL_ADV_MODE_OFF
520 
526 #define HCI_SCAN_PASSIVE LL_SCAN_PASSIVE
527 #define HCI_SCAN_ACTIVE LL_SCAN_ACTIVE
528 
534 // Scan White List Policy
535 #define HCI_SCAN_WL_POLICY_ANY_ADV_PKTS LL_SCAN_WL_POLICY_ANY_ADV_PKTS
536 #define HCI_SCAN_WL_POLICY_USE_WHITE_LIST LL_SCAN_WL_POLICY_USE_WHITE_LIST
537 
543 // Scan Filtering
544 #define HCI_FILTER_REPORTS_DISABLE LL_FILTER_REPORTS_DISABLE
545 #define HCI_FILTER_REPORTS_ENABLE LL_FILTER_REPORTS_ENABLE
546 
552 // Scan Commands
553 #define HCI_SCAN_STOP LL_SCAN_STOP
554 #define HCI_SCAN_START LL_SCAN_START
555 
561 #define HCI_INIT_WL_POLICY_USE_PEER_ADDR LL_INIT_WL_POLICY_USE_PEER_ADDR
562 #define HCI_INIT_WL_POLICY_USE_WHITE_LIST LL_INIT_WL_POLICY_USE_WHITE_LIST
563 
569 #define HCI_ENCRYPTION_OFF LL_ENCRYPTION_OFF
570 #define HCI_ENCRYPTION_ON LL_ENCRYPTION_ON
571 
577 #define HCI_DIRECT_TEST_PAYLOAD_PRBS9 LL_DIRECT_TEST_PAYLOAD_PRBS9
578 #define HCI_DIRECT_TEST_PAYLOAD_0x0F LL_DIRECT_TEST_PAYLOAD_0x0F
579 #define HCI_DIRECT_TEST_PAYLOAD_0x55 LL_DIRECT_TEST_PAYLOAD_0x55
580 #define HCI_DIRECT_TEST_PAYLOAD_PRBS15 LL_DIRECT_TEST_PAYLOAD_PRBS15
581 #define HCI_DIRECT_TEST_PAYLOAD_0xFF LL_DIRECT_TEST_PAYLOAD_0xFF
582 #define HCI_DIRECT_TEST_PAYLOAD_0x00 LL_DIRECT_TEST_PAYLOAD_0x00
583 #define HCI_DIRECT_TEST_PAYLOAD_0xF0 LL_DIRECT_TEST_PAYLOAD_0xF0
584 #define HCI_DIRECT_TEST_PAYLOAD_0xAA LL_DIRECT_TEST_PAYLOAD_0xAA
585 
591 #define HCI_DTM_STANDARD_MODULATION_INDEX LL_DTM_STANDARD_MODULATION_INDEX
592 #define HCI_DTM_STABLE_MODULATION_INDEX LL_DTM_STABLE_MODULATION_INDEX
593 
599 #define HCI_EXT_DTM_TX_CONTINUOUS LL_EXT_DTM_TX_CONTINUOUS
600 
606 #define HCI_DISABLE_ADDR_RESOLUTION LL_DISABLE_ADDR_RESOLUTION
607 #define HCI_ENABLE_ADDR_RESOLUTION LL_ENABLE_ADDR_RESOLUTION
608 #define HCI_NETWORK_PRIVACY_MODE LL_NETWORK_PRIVACY_MODE
609 #define HCI_DEVICE_PRIVACY_MODE LL_DEVICE_PRIVACY_MODE
610 
616 #define HCI_PHY_USE_PHY_PARAM LL_PHY_USE_PHY_PARAM
617 #define HCI_PHY_USE_ANY_PHY LL_PHY_USE_ANY_PHY
618 #define HCI_PHY_1_MBPS LL_PHY_1_MBPS
619 #define HCI_PHY_2_MBPS LL_PHY_2_MBPS
620 #define HCI_PHY_CODED LL_PHY_CODED
621 
627 #define PHY_UPDATE_COMPLETE_EVENT_1M 1
628 #define PHY_UPDATE_COMPLETE_EVENT_2M 2
629 #define PHY_UPDATE_COMPLETE_EVENT_CODED 3
630 
636 #define HCI_EXT_RX_GAIN_STD LL_EXT_RX_GAIN_STD
637 #define HCI_EXT_RX_GAIN_HIGH LL_EXT_RX_GAIN_HIGH
638 
644 #if defined( CC26XX ) || defined( CC13XX )
645 #define HCI_EXT_TX_POWER_MINUS_20_DBM LL_EXT_TX_POWER_MINUS_20_DBM
646 #define HCI_EXT_TX_POWER_MINUS_18_DBM LL_EXT_TX_POWER_MINUS_18_DBM
647 #define HCI_EXT_TX_POWER_MINUS_15_DBM LL_EXT_TX_POWER_MINUS_15_DBM
648 #define HCI_EXT_TX_POWER_MINUS_12_DBM LL_EXT_TX_POWER_MINUS_12_DBM
649 #define HCI_EXT_TX_POWER_MINUS_10_DBM LL_EXT_TX_POWER_MINUS_10_DBM
650 #define HCI_EXT_TX_POWER_MINUS_9_DBM LL_EXT_TX_POWER_MINUS_9_DBM
651 #define HCI_EXT_TX_POWER_MINUS_6_DBM LL_EXT_TX_POWER_MINUS_6_DBM
652 #define HCI_EXT_TX_POWER_MINUS_5_DBM LL_EXT_TX_POWER_MINUS_5_DBM
653 #define HCI_EXT_TX_POWER_MINUS_3_DBM LL_EXT_TX_POWER_MINUS_3_DBM
654 #define HCI_EXT_TX_POWER_0_DBM LL_EXT_TX_POWER_0_DBM
655 #define HCI_EXT_TX_POWER_1_DBM LL_EXT_TX_POWER_1_DBM
656 #define HCI_EXT_TX_POWER_2_DBM LL_EXT_TX_POWER_2_DBM
657 #define HCI_EXT_TX_POWER_3_DBM LL_EXT_TX_POWER_3_DBM
658 #define HCI_EXT_TX_POWER_4_DBM LL_EXT_TX_POWER_4_DBM
659 #define HCI_EXT_TX_POWER_5_DBM LL_EXT_TX_POWER_5_DBM
660 #if defined( CC13X2P )
661 #define HCI_EXT_TX_POWER_P2_14_DBM_P4_6_DBM LL_EXT_TX_POWER_P2_14_DBM_P4_6_DBM
662 #define HCI_EXT_TX_POWER_P2_15_DBM_P4_7_DBM LL_EXT_TX_POWER_P2_15_DBM_P4_7_DBM
663 #define HCI_EXT_TX_POWER_P2_16_DBM_P4_8_DBM LL_EXT_TX_POWER_P2_16_DBM_P4_8_DBM
664 #define HCI_EXT_TX_POWER_P2_17_DBM_P4_9_DBM LL_EXT_TX_POWER_P2_17_DBM_P4_9_DBM
665 #define HCI_EXT_TX_POWER_P2_18_DBM_P4_10_DBM LL_EXT_TX_POWER_P2_18_DBM_P4_10_DBM
666 #define HCI_EXT_TX_POWER_P2_19_DBM LL_EXT_TX_POWER_P2_19_DBM
667 #define HCI_EXT_TX_POWER_P2_20_DBM LL_EXT_TX_POWER_P2_20_DBM
668 #endif // CC13X2P
669 #else // CC254x
670 #define HCI_EXT_TX_POWER_MINUS_23_DBM LL_EXT_TX_POWER_MINUS_23_DBM
671 #define HCI_EXT_TX_POWER_MINUS_6_DBM LL_EXT_TX_POWER_MINUS_6_DBM
672 #define HCI_EXT_TX_POWER_0_DBM LL_EXT_TX_POWER_0_DBM
673 #define HCI_EXT_TX_POWER_4_DBM LL_EXT_TX_POWER_4_DBM
674 #endif // CC26XX/CC13XX
675 
681 #define HCI_EXT_ENABLE_ONE_PKT_PER_EVT LL_EXT_ENABLE_ONE_PKT_PER_EVT
682 #define HCI_EXT_DISABLE_ONE_PKT_PER_EVT LL_EXT_DISABLE_ONE_PKT_PER_EVT
683 
685 
687 
691 #define HCI_EXT_ENABLE_CLK_DIVIDE_ON_HALT LL_EXT_ENABLE_CLK_DIVIDE_ON_HALT
692 #define HCI_EXT_DISABLE_CLK_DIVIDE_ON_HALT LL_EXT_DISABLE_CLK_DIVIDE_ON_HALT
693 
695 
697 
701 #define HCI_EXT_NV_IN_USE LL_EXT_NV_IN_USE
702 #define HCI_EXT_NV_NOT_IN_USE LL_EXT_NV_NOT_IN_USE
703 
709 #define HCI_EXT_ENABLE_FAST_TX_RESP_TIME LL_EXT_ENABLE_FAST_TX_RESP_TIME
710 #define HCI_EXT_DISABLE_FAST_TX_RESP_TIME LL_EXT_DISABLE_FAST_TX_RESP_TIME
711 
717 #define HCI_EXT_ENABLE_SL_OVERRIDE LL_EXT_ENABLE_SL_OVERRIDE
718 #define HCI_EXT_DISABLE_SL_OVERRIDE LL_EXT_DISABLE_SL_OVERRIDE
719 
725 #define HCI_EXT_TX_MODULATED_CARRIER LL_EXT_TX_MODULATED_CARRIER
726 #define HCI_EXT_TX_UNMODULATED_CARRIER LL_EXT_TX_UNMODULATED_CARRIER
727 
733 #define HCI_PTM_SET_FREQ_TUNE_DOWN LL_EXT_SET_FREQ_TUNE_DOWN
734 #define HCI_PTM_SET_FREQ_TUNE_UP LL_EXT_SET_FREQ_TUNE_UP
735 
737 
739 
743 #define HCI_EXT_PM_IO_PORT_P0 LL_EXT_PM_IO_PORT_P0
744 #define HCI_EXT_PM_IO_PORT_P1 LL_EXT_PM_IO_PORT_P1
745 #define HCI_EXT_PM_IO_PORT_P2 LL_EXT_PM_IO_PORT_P2
746 #define HCI_EXT_PM_IO_PORT_NONE LL_EXT_PM_IO_PORT_NONE
747 
748 #define HCI_EXT_PM_IO_PORT_PIN0 LL_EXT_PM_IO_PORT_PIN0
749 #define HCI_EXT_PM_IO_PORT_PIN1 LL_EXT_PM_IO_PORT_PIN1
750 #define HCI_EXT_PM_IO_PORT_PIN2 LL_EXT_PM_IO_PORT_PIN2
751 #define HCI_EXT_PM_IO_PORT_PIN3 LL_EXT_PM_IO_PORT_PIN3
752 #define HCI_EXT_PM_IO_PORT_PIN4 LL_EXT_PM_IO_PORT_PIN4
753 #define HCI_EXT_PM_IO_PORT_PIN5 LL_EXT_PM_IO_PORT_PIN5
754 #define HCI_EXT_PM_IO_PORT_PIN6 LL_EXT_PM_IO_PORT_PIN6
755 #define HCI_EXT_PM_IO_PORT_PIN7 LL_EXT_PM_IO_PORT_PIN7
756 
758 
764 #define HCI_EXT_PER_RESET LL_EXT_PER_RESET
765 #define HCI_EXT_PER_READ LL_EXT_PER_READ
766 
768 
770 
774 #define HCI_EXT_HALT_DURING_RF_DISABLE LL_EXT_HALT_DURING_RF_DISABLE
775 #define HCI_EXT_HALT_DURING_RF_ENABLE LL_EXT_HALT_DURING_RF_ENABLE
776 
778 
780 
784 #define HCI_EXT_SET_USER_REVISION LL_EXT_SET_USER_REVISION
785 #define HCI_EXT_READ_BUILD_REVISION LL_EXT_READ_BUILD_REVISION
786 
792 #define HCI_EXT_RESET_SYSTEM_HARD LL_EXT_RESET_SYSTEM_HARD
793 #define HCI_EXT_RESET_SYSTEM_SOFT LL_EXT_RESET_SYSTEM_SOFT
794 
796 
798 
802 #define HCI_EXT_DISABLE_OVERLAPPED_PROCESSING LL_EXT_DISABLE_OVERLAPPED_PROCESSING
803 #define HCI_EXT_ENABLE_OVERLAPPED_PROCESSING LL_EXT_ENABLE_OVERLAPPED_PROCESSING
804 
806 
808 
812 #define HCI_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT LL_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT
813 #define HCI_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT LL_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT
814 
820 #define HCI_EXT_DISABLE_SCAN_REQUEST_REPORT LL_EXT_DISABLE_SCAN_REQUEST_REPORT
821 #define HCI_EXT_ENABLE_SCAN_REQUEST_REPORT LL_EXT_ENABLE_SCAN_REQUEST_REPORT
822 
832 #define HCI_LINK_TYPE_SCO_BUFFER_OVERFLOW 0
833 #define HCI_LINK_TYPE_ACL_BUFFER_OVERFLOW 1
834 
842 #define HCI_EXT_RF_SETUP_1M_PHY LL_EXT_RF_SETUP_1M_PHY
843 #define HCI_EXT_RF_SETUP_2M_PHY LL_EXT_RF_SETUP_2M_PHY
844 #define HCI_EXT_RF_SETUP_CODED_S8_PHY LL_EXT_RF_SETUP_CODED_S8_PHY
845 #define HCI_EXT_RF_SETUP_CODED_S2_PHY LL_EXT_RF_SETUP_CODED_S2_PHY
846 
850 /*
851  * TYPEDEFS
852  */
853 
855 typedef uint8 hciStatus_t;
857 
863 typedef struct
865 {
867  uint8 BLEEventCode;
868  uint8 status;
870  uint8 role;
871  uint8 peerAddrType;
872  uint8 peerAddr[B_ADDR_LEN];
873  uint16 connInterval;
874  uint16 connLatency;
875  uint16 connTimeout;
878 
880 typedef struct
881 {
883  uint8 BLEEventCode;
884  uint8 status;
886  uint8 role;
887  uint8 peerAddrType;
888  uint8 peerAddr[B_ADDR_LEN];
889  uint16 connInterval;
890  uint16 connLatency;
891  uint16 connTimeout;
893  // Note: These fields normally follow peerAddr. Put here for Host optimization.
894  uint8 localRPA[B_ADDR_LEN];
895  uint8 peerRPA[B_ADDR_LEN];
897 
900 {
904 
906 typedef struct
907 {
908  uint8 eventType;
909  uint8 addrType;
910  uint8 addr[B_ADDR_LEN];
911  uint8 dataLen;
912  uint8 rspData[B_MAX_ADV_LEN];
913  int8 rssi;
915 
917 typedef struct
918 {
920  uint8 BLEEventCode;
921  uint8 numDevices;
924 
926 typedef struct
927 {
929  uint8 BLEEventCode;
930  uint8 eventType;
931  uint8 peerAddrType;
932  uint8 peerAddr[B_ADDR_LEN];
933  uint8 bleChan;
934  int8 rssi;
936 
938 typedef struct
939 {
941  uint8 BLEEventCode;
942  uint16 connHandle;
943  uint8 nextDataChan;
944  uint8 newChanMap[LL_NUM_BYTES_FOR_CHAN_MAP];
946 
948 typedef struct
949 {
951  uint8 BLEEventCode;
952  uint8 status;
954  uint16 connInterval;
955  uint16 connLatency;
956  uint16 connTimeout;
958 
960 typedef struct
961 {
963  uint8 BLEEventCode;
964  uint8 status;
966  uint8 features[8];
968 
970 typedef struct
971 {
973  uint8 BLEEventCode;
974  uint16 connHandle;
975  uint8 reason;
976  uint8 encEnable;
978 
980 typedef struct
981 {
983  uint8 BLEEventCode;
984  uint16 connHandle;
985  uint8 random[B_RANDOM_NUM_SIZE];
988 
990 typedef struct
991 {
993  uint8 numHandles;
997 
999 typedef struct
1000 {
1003  uint16 cmdOpcode;
1004  uint8 *pReturnParam;
1006 
1008 typedef struct
1009 {
1011  uint8 length;
1012  uint16 cmdOpcode;
1013  uint8 *pEventParam;
1015 
1017 typedef struct
1018 {
1020  uint8 cmdStatus;
1022  uint16 cmdOpcode;
1024 
1026 typedef struct
1027 {
1031 
1033 typedef struct
1034 {
1036  uint8 status;
1037  uint16 connHandle;
1038  uint8 reason;
1040 
1042 typedef struct
1043 {
1045  uint8 linkType;
1047 
1049 typedef struct
1050 {
1052  uint16 connHandle;
1054 
1056 typedef struct
1057 {
1060  uint8 status;
1061  uint16 connHandle;
1062  uint16 Interval_Min;
1063  uint16 Interval_Max;
1064  uint16 Latency;
1065  uint16 Timeout;
1067 
1069 typedef struct
1070 {
1073  uint8 status;
1074  uint16 connHandle;
1075  uint8 txPhy;
1076  uint8 rxPhy;
1078 
1080 typedef struct
1081 {
1084  uint16 connHandle;
1085  uint16 maxTxOctets;
1086  uint16 maxTxTime;
1087  uint16 maxRxOctets;
1088  uint16 maxRxTime;
1090 
1092 typedef struct
1093 {
1096  uint8 status;
1097  uint8 p256Key[LL_SC_P256_KEY_LEN];
1099 
1101 typedef struct
1102 {
1105  uint8 status;
1106  uint8 dhKey[LL_SC_DHKEY_LEN];
1108 
1110 typedef struct
1111 {
1114  uint16 connHandle;
1115  uint8 phy;
1116  uint8 dataChIndex;
1117  uint16 rssi;
1118  uint8 rssiAntenna;
1119  uint8 cteType;
1121  uint8 status;
1122  uint16 connEvent;
1123  uint8 sampleCount;
1124  int8 *iqSamples;
1126 
1128 typedef struct
1129 {
1132  uint8 status;
1133  uint16 connHandle;
1135 
1137 typedef struct
1138 {
1141  uint16 totalDataLen;
1142  uint8 eventIndex;
1143  uint16 connHandle;
1144  uint8 phy;
1145  uint8 dataChIndex;
1146  uint16 rssi;
1147  uint8 rssiAntenna;
1148  uint8 cteType;
1150  uint8 status;
1151  uint16 connEvent;
1152  uint8 dataLen;
1153  uint8 sampleRate;
1154  uint8 sampleSize;
1155  uint8 sampleCtrl;
1156  void *iqSamples;
1158 
1160 typedef struct
1161 {
1164  uint16 syncHandle;
1166  uint16 rssi;
1167  uint8 rssiAntenna;
1168  uint8 cteType;
1170  uint8 status;
1171  uint16 eventCounter;
1172  uint8 sampleCount;
1173  int8 *iqSamples;
1175 
1177 typedef struct
1178 {
1181  uint16 totalDataLen;
1182  uint8 eventIndex;
1183  uint16 syncHandle;
1185  uint16 rssi;
1186  uint8 rssiAntenna;
1187  uint8 cteType;
1189  uint8 status;
1190  uint16 eventCounter;
1191  uint8 dataLen;
1192  uint8 sampleRate;
1193  uint8 sampleSize;
1194  uint8 sampleCtrl;
1195  void *iqSamples;
1197 
1199 typedef struct
1200 {
1203  uint8 status;
1204  uint16 syncHandle;
1205  uint8 sid;
1206  uint8 addrType;
1207  uint8 address[B_ADDR_LEN];
1208  uint8 phy;
1212 
1214 typedef struct
1215 {
1218  uint16 syncHandle;
1219  int8 txPower;
1220  int8 rssi;
1221  uint8 cteType;
1222  uint8 dataStatus;
1223  uint8 dataLen;
1224  uint8 *data;
1226 
1228 typedef struct
1229 {
1232  uint16 syncHandle;
1234 
1235 
1237 typedef struct
1238 {
1239  uint8 status;
1240  uint16 dataPktLen;
1241  uint8 numDataPkts;
1243 
1245 typedef struct
1246 {
1249  uint16 connHandle;
1250  uint8 chSelAlgo;
1252 
1254 typedef struct
1255 {
1257  uint8 *pData;
1258 } hciPacket_t;
1259 
1261 typedef struct
1262 {
1264  uint8 pktType;
1265  uint16 connHandle;
1266  uint8 pbFlag;
1267  uint16 pktLen;
1268  uint8 *pData;
1269 } hciDataPacket_t;
1270 
1272 
1273 // OSAL HCI_DATA_EVENT message format. This message is used to forward incoming
1274 // data messages up to an application
1275 typedef struct
1276 {
1277  osal_event_hdr_t hdr;
1278  uint16 connHandle;
1279  uint8 pbFlag;
1280  uint16 len;
1281  uint8 *pData;
1282 } hciDataEvent_t;
1283 
1285 
1286 #if defined( CC26XX ) || defined( CC13XX )
1287 PACKED_TYPEDEF_STRUCT
1288 #else // CC254x
1289 typedef struct
1290 #endif // CC26XX/CC13XX
1291 {
1292  uint8 connId;
1293  uint8 role;
1294  uint8 addr[LL_DEVICE_ADDR_LEN];
1295  uint8 addrType;
1296 } hciConnInfo_t;
1297 
1298 #if defined( CC26XX ) || defined( CC13XX )
1299 PACKED_TYPEDEF_STRUCT
1300 #else // CC254x
1301 typedef struct
1302 #endif // CC26XX/CC13XX
1303 {
1304  uint32_t accessAddr;
1305  uint16_t connInterval;
1306  uint8_t hopValue;
1307  uint16_t mSCA;
1308  uint8_t nextChan;
1309  uint8_t chanMap[LL_NUM_BYTES_FOR_CHAN_MAP];
1310  uint8_t crcInit[LL_PKT_CRC_LEN];
1311 }hciActiveConnInfo_t;
1312 
1313 #if defined( CC26XX ) || defined( CC13XX )
1314 PACKED_TYPEDEF_STRUCT
1315 #else // CC254x
1316 typedef struct
1317 #endif // CC26XX/CC13XX
1318 {
1319  uint16 numPkts;
1320  uint16 numCrcErr;
1321  uint16 numEvents;
1322  uint16 numMMissedEvents;
1323 } hciPER_t;
1324 
1327 /*
1328  * LOCAL VARIABLES
1329  */
1330 
1331 /*
1332  * GLOBAL VARIABLES
1333  */
1334 
1336 
1347 extern void *HCI_bm_alloc( uint16 size );
1348 
1362 extern uint8 HCI_ValidConnTimeParams( uint16 connIntervalMin,
1363  uint16 connIntervalMax,
1364  uint16 connLatency,
1365  uint16 connTimeout );
1366 
1372 extern void HCI_TestAppTaskRegister( uint8 taskID );
1373 
1379 extern void HCI_GAPTaskRegister( uint8 taskID );
1380 
1386 extern void HCI_L2CAPTaskRegister( uint8 taskID );
1387 
1393 extern void HCI_SMPTaskRegister( uint8 taskID );
1394 
1400 extern void HCI_ExtTaskRegister( uint8 taskID );
1401 
1426 extern hciStatus_t HCI_SendDataPkt( uint16 connHandle,
1427  uint8 pbFlag,
1428  uint16 pktLen,
1429  uint8 *pData );
1430 
1446 extern hciStatus_t HCI_DisconnectCmd( uint16 connHandle,
1447  uint8 reason );
1448 
1450 
1468 extern hciStatus_t HCI_ReadRemoteVersionInfoCmd( uint16 connHandle );
1469 
1470 
1484 extern hciStatus_t HCI_SetEventMaskCmd( uint8 *pMask );
1485 
1486 
1500 extern hciStatus_t HCI_SetEventMaskPage2Cmd( uint8 *pMask );
1501 
1510 extern hciStatus_t HCI_ResetCmd( void );
1511 
1523 extern hciStatus_t HCI_ReadTransmitPowerLevelCmd( uint16 connHandle,
1524  uint8 txPwrType );
1525 
1527 
1541 extern hciStatus_t HCI_SetControllerToHostFlowCtrlCmd( uint8 flowControlEnable );
1542 
1562 extern hciStatus_t HCI_HostBufferSizeCmd( uint16 hostAclPktLen,
1563  uint8 hostSyncPktLen,
1564  uint16 hostTotalNumAclPkts,
1565  uint16 hostTotalNumSyncPkts );
1566 
1568 
1597 extern hciStatus_t HCI_HostNumCompletedPktCmd( uint8 numHandles,
1598  uint16 *connHandles,
1599  uint16 *numCompletedPkts );
1600 
1612 extern hciStatus_t HCI_ReadAuthPayloadTimeoutCmd( uint16 connHandle,
1613  uint16 *aptoValue );
1614 
1626 extern hciStatus_t HCI_WriteAuthPayloadTimeoutCmd( uint16 connHandle,
1627  uint16 aptoValue );
1628 
1637 extern hciStatus_t HCI_ReadLocalVersionInfoCmd( void );
1638 
1647 extern hciStatus_t HCI_ReadLocalSupportedCommandsCmd( void );
1648 
1657 extern hciStatus_t HCI_ReadLocalSupportedFeaturesCmd( void );
1658 
1667 extern hciStatus_t HCI_ReadBDADDRCmd( void );
1668 
1685 extern hciStatus_t HCI_ReadRssiCmd( uint16 connHandle );
1686 
1700 extern hciStatus_t HCI_LE_SetEventMaskCmd( uint8 *pEventMask );
1701 
1710 extern hciStatus_t HCI_LE_ReadBufSizeCmd( void );
1711 
1721 extern hciStatus_t HCI_LE_ReadLocalSupportedFeaturesCmd( void );
1722 
1724 
1736 extern hciStatus_t HCI_LE_SetRandomAddressCmd( uint8 *pRandAddr );
1737 
1755 extern hciStatus_t HCI_LE_SetAdvParamCmd( uint16 advIntervalMin,
1756  uint16 advIntervalMax,
1757  uint8 advType,
1758  uint8 ownAddrType,
1759  uint8 directAddrType,
1760  uint8 *directAddr,
1761  uint8 advChannelMap,
1762  uint8 advFilterPolicy );
1763 
1775 extern hciStatus_t HCI_LE_SetAdvDataCmd( uint8 dataLen,
1776  uint8 *pData );
1777 
1789 extern hciStatus_t HCI_LE_SetScanRspDataCmd( uint8 dataLen,
1790  uint8 *pData );
1791 
1802 extern hciStatus_t HCI_LE_SetAdvEnableCmd( uint8 advEnable );
1803 
1812 extern hciStatus_t HCI_LE_ReadAdvChanTxPowerCmd( void );
1813 
1830 extern hciStatus_t HCI_LE_SetScanParamCmd( uint8 scanType,
1831  uint16 scanInterval,
1832  uint16 scanWindow,
1833  uint8 ownAddrType,
1834  uint8 filterPolicy );
1835 
1848 extern hciStatus_t HCI_LE_SetScanEnableCmd( uint8 scanEnable,
1849  uint8 filterDuplicates );
1850 
1875 extern hciStatus_t HCI_LE_CreateConnCmd( uint16 scanInterval,
1876  uint16 scanWindow,
1877  uint8 initFilterPolicy,
1878  uint8 addrTypePeer,
1879  uint8 *peerAddr,
1880  uint8 ownAddrType,
1881  uint16 connIntervalMin,
1882  uint16 connIntervalMax,
1883  uint16 connLatency,
1884  uint16 connTimeout,
1885  uint16 minLen,
1886  uint16 maxLen );
1887 
1896 extern hciStatus_t HCI_LE_CreateConnCancelCmd( void );
1897 
1899 
1908 extern hciStatus_t HCI_LE_ReadWhiteListSizeCmd( void );
1909 
1910 
1919 extern hciStatus_t HCI_LE_ClearWhiteListCmd( void );
1920 
1921 
1933 extern hciStatus_t HCI_LE_AddWhiteListCmd( uint8 addrType,
1934  uint8 *devAddr );
1935 
1936 
1948 extern hciStatus_t HCI_LE_RemoveWhiteListCmd( uint8 addrType,
1949  uint8 *devAddr );
1950 
1952 
1970 extern hciStatus_t HCI_LE_ConnUpdateCmd( uint16 connHandle,
1971  uint16 connIntervalMin,
1972  uint16 connIntervalMax,
1973  uint16 connLatency,
1974  uint16 connTimeout,
1975  uint16 minLen,
1976  uint16 maxLen );
1977 
1979 
1991 extern hciStatus_t HCI_LE_SetHostChanClassificationCmd( uint8 *chanMap );
1992 
2004 extern hciStatus_t HCI_LE_ReadChannelMapCmd( uint16 connHandle );
2005 
2018 extern hciStatus_t HCI_LE_ReadRemoteUsedFeaturesCmd( uint16 connHandle );
2019 
2040 extern hciStatus_t HCI_LE_EncryptCmd( uint8 *key,
2041  uint8 *plainText );
2042 
2065 extern hciStatus_t HCI_LE_RandCmd( void );
2066 
2068 
2084 extern hciStatus_t HCI_LE_StartEncyptCmd( uint16 connHandle,
2085  uint8 *random,
2086  uint8 *encDiv,
2087  uint8 *ltk );
2088 
2100 extern hciStatus_t HCI_LE_LtkReqReplyCmd( uint16 connHandle,
2101  uint8 *ltk );
2102 
2103 
2114 extern hciStatus_t HCI_LE_LtkReqNegReplyCmd( uint16 connHandle );
2115 
2117 
2126 extern hciStatus_t HCI_LE_ReadSupportedStatesCmd( void );
2127 
2140 extern hciStatus_t HCI_LE_ReceiverTestCmd( uint8 rxChan );
2141 
2158 extern hciStatus_t HCI_LE_TransmitterTestCmd( uint8 txChan,
2159  uint8 dataLen,
2160  uint8 pktPayload );
2161 
2172 extern hciStatus_t HCI_LE_TestEndCmd( void );
2173 
2174 // V4.1
2175 
2177 
2199 extern hciStatus_t HCI_LE_RemoteConnParamReqReplyCmd( uint16 connHandle,
2200  uint16 connIntervalMin,
2201  uint16 connIntervalMax,
2202  uint16 connLatency,
2203  uint16 connTimeout,
2204  uint16 minLen,
2205  uint16 maxLen );
2206 
2223 extern hciStatus_t HCI_LE_RemoteConnParamReqNegReplyCmd( uint16 connHandle,
2224  uint8 reason );
2225 
2227 
2228 // V4.2 Extended Data Length
2229 
2245 extern hciStatus_t HCI_LE_SetDataLenCmd( uint16 connHandle,
2246  uint16 txOctets,
2247  uint16 txTime );
2248 
2260 extern hciStatus_t HCI_LE_ReadSuggestedDefaultDataLenCmd( void );
2261 
2277 extern hciStatus_t HCI_LE_WriteSuggestedDefaultDataLenCmd( uint16 txOctets,
2278  uint16 txTime );
2279 
2291 extern hciStatus_t HCI_LE_ReadMaxDataLenCmd( void );
2292 
2293 // V4.2 Privacy 1.2
2294 
2311 extern hciStatus_t HCI_LE_AddDeviceToResolvingListCmd( uint8 peerIdAddrType,
2312  uint8 *peerIdAddr,
2313  uint8 *peerIRK,
2314  uint8 *localIRK );
2315 
2330 extern hciStatus_t HCI_LE_RemoveDeviceFromResolvingListCmd( uint8 peerIdAddrType,
2331  uint8 *peerIdAddr );
2332 
2344 extern hciStatus_t HCI_LE_ClearResolvingListCmd( void );
2345 
2357 extern hciStatus_t HCI_LE_ReadResolvingListSizeCmd( void );
2358 
2376 extern hciStatus_t HCI_LE_ReadPeerResolvableAddressCmd( uint8 peerIdAddrType,
2377  uint8 *peerIdAddr );
2378 
2397 extern hciStatus_t HCI_LE_ReadLocalResolvableAddressCmd( uint8 localIdAddrType,
2398  uint8 *localIdAddr );
2399 
2401 
2416 extern hciStatus_t HCI_LE_SetAddressResolutionEnableCmd( uint8 addrResolutionEnable );
2417 
2419 
2435 extern hciStatus_t HCI_LE_SetResolvablePrivateAddressTimeoutCmd( uint16 rpaTimeout );
2436 
2453 extern hciStatus_t HCI_LE_SetPrivacyModeCmd( uint8 peerIdAddrType,
2454  uint8 *peerIdAddr,
2455  uint8 privacyMode );
2456 
2457 // V4.2 Secure Connections
2458 
2460 
2476 extern hciStatus_t HCI_LE_ReadLocalP256PublicKeyCmd( void );
2477 
2478 
2497 extern hciStatus_t HCI_LE_GenerateDHKeyCmd( uint8 *publicKey );
2498 
2500 
2501 // V5.0 2M and Coded PHY
2502 
2518 extern hciStatus_t HCI_LE_ReadPhyCmd( uint16 connHandle );
2519 
2520 
2536 extern hciStatus_t HCI_LE_SetDefaultPhyCmd( uint8 allPhys,
2537  uint8 txPhy,
2538  uint8 rxPhy );
2539 
2540 
2555 extern hciStatus_t HCI_LE_SetPhyCmd( uint16 connHandle,
2556  uint8 allPhys,
2557  uint8 txPhy,
2558  uint8 rxPhy,
2559  uint16 phyOpts );
2560 
2561 
2577 extern hciStatus_t HCI_LE_EnhancedRxTestCmd( uint8 rxChan,
2578  uint8 rxPhy,
2579  uint8 modIndex );
2580 
2581 
2598 extern hciStatus_t HCI_LE_EnhancedTxTestCmd( uint8 txChan,
2599  uint8 payloadLen,
2600  uint8 payloadType,
2601  uint8 txPhy );
2622 extern hciStatus_t HCI_LE_EnhancedCteRxTestCmd( uint8 rxChan,
2623  uint8 rxPhy,
2624  uint8 modIndex,
2625  uint8 expectedCteLength,
2626  uint8 expectedCteType,
2627  uint8 slotDurations,
2628  uint8 length,
2629  uint8 *pAntenna);
2630 
2651 extern hciStatus_t HCI_LE_EnhancedCteTxTestCmd( uint8 txChan,
2652  uint8 payloadLen,
2653  uint8 payloadType,
2654  uint8 txPhy,
2655  uint8 cteLength,
2656  uint8 cteType,
2657  uint8 length,
2658  uint8 *pAntenna);
2667 extern hciStatus_t HCI_LE_ReadTxPowerCmd( void );
2668 
2677 extern hciStatus_t HCI_LE_ReadRfPathCompCmd( void );
2678 
2690 extern hciStatus_t HCI_LE_WriteRfPathCompCmd( int16 txPathParam,
2691  int16 rxPathParam );
2692 
2711 extern hciStatus_t HCI_LE_SetConnectionCteReceiveParamsCmd( uint16 connHandle,
2712  uint8 samplingEnable,
2713  uint8 slotDurations,
2714  uint8 length,
2715  uint8 *pAntenna);
2716 
2717 
2734 extern hciStatus_t HCI_LE_SetConnectionCteTransmitParamsCmd( uint16 connHandle,
2735  uint8 types,
2736  uint8 length,
2737  uint8 *pAntenna);
2738 
2755 extern hciStatus_t HCI_LE_SetConnectionCteRequestEnableCmd( uint16 connHandle,
2756  uint8 enable,
2757  uint16 interval,
2758  uint8 length,
2759  uint8 type);
2760 
2774 extern hciStatus_t HCI_LE_SetConnectionCteResponseEnableCmd( uint16 connHandle,
2775  uint8 enable);
2776 
2787 extern hciStatus_t HCI_LE_ReadAntennaInformationCmd( void );
2788 
2808 extern hciStatus_t HCI_LE_SetPeriodicAdvParamsCmd( uint8 advHandle,
2809  uint16 periodicAdvIntervalMin,
2810  uint16 periodicAdvIntervalMax,
2811  uint16 periodicAdvProp );
2812 
2813 
2836 extern hciStatus_t HCI_LE_SetPeriodicAdvDataCmd( uint8 advHandle,
2837  uint8 operation,
2838  uint8 dataLength,
2839  uint8 *data );
2840 
2856 extern hciStatus_t HCI_LE_SetPeriodicAdvEnableCmd( uint8 enable,
2857  uint8 advHandle );
2858 
2876 extern hciStatus_t HCI_LE_SetConnectionlessCteTransmitParamsCmd( uint8 advHandle,
2877  uint8 cteLen,
2878  uint8 cteType,
2879  uint8 cteCount,
2880  uint8 length,
2881  uint8 *pAntenna);
2882 
2897 extern hciStatus_t HCI_LE_SetConnectionlessCteTransmitEnableCmd( uint8 advHandle,
2898  uint8 enable );
2899 
2929 extern hciStatus_t HCI_LE_PeriodicAdvCreateSyncCmd( uint8 options,
2930  uint8 advSID,
2931  uint8 advAddrType,
2932  uint8 *advAddress,
2933  uint16 skip,
2934  uint16 syncTimeout,
2935  uint8 syncCteType );
2936 
2947 extern hciStatus_t HCI_LE_PeriodicAdvCreateSyncCancelCmd( void );
2948 
2964 extern hciStatus_t HCI_LE_PeriodicAdvTerminateSyncCmd( uint16 syncHandle );
2965 
2982 extern hciStatus_t HCI_LE_AddDeviceToPeriodicAdvListCmd( uint8 advAddrType,
2983  uint8 *advAddress,
2984  uint8 advSID );
2985 
3003 extern hciStatus_t HCI_LE_RemoveDeviceFromPeriodicAdvListCmd( uint8 advAddrType,
3004  uint8 *advAddress,
3005  uint8 advSID );
3006 
3017 extern hciStatus_t HCI_LE_ClearPeriodicAdvListCmd( void );
3018 
3030 extern hciStatus_t HCI_LE_ReadPeriodicAdvListSizeCmd( void );
3031 
3049 extern hciStatus_t HCI_LE_SetPeriodicAdvReceiveEnableCmd( uint16 syncHandle,
3050  uint8 enable );
3051 
3069 extern hciStatus_t HCI_LE_SetConnectionlessIqSamplingEnableCmd( uint16 syncHandle,
3070  uint8 samplingEnable,
3071  uint8 slotDurations,
3072  uint8 maxSampledCtes,
3073  uint8 length,
3074  uint8 *pAntenna);
3075 
3076 /*
3077 ** HCI Vendor Specific Commands: Link Layer Extensions
3078 */
3079 
3092 extern hciStatus_t HCI_EXT_SetRxGainCmd( uint8 rxGain );
3093 
3094 
3112 extern hciStatus_t HCI_EXT_SetTxPowerCmd( uint8 txPower );
3113 
3114 
3127 extern hciStatus_t HCI_EXT_OnePktPerEvtCmd( uint8 control );
3128 
3130 
3149 extern hciStatus_t HCI_EXT_ClkDivOnHaltCmd( uint8 control );
3150 
3172 extern hciStatus_t HCI_EXT_DeclareNvUsageCmd( uint8 mode );
3173 
3175 
3189 extern hciStatus_t HCI_EXT_DecryptCmd( uint8 *key,
3190  uint8 *encText );
3191 
3214 extern hciStatus_t HCI_EXT_SetLocalSupportedFeaturesCmd( uint8 *localFeatures );
3215 
3241 extern hciStatus_t HCI_EXT_SetFastTxResponseTimeCmd( uint8 control );
3242 
3243 
3262 extern hciStatus_t HCI_EXT_SetSlaveLatencyOverrideCmd( uint8 control );
3263 
3264 
3288 extern hciStatus_t HCI_EXT_ModemTestTxCmd( uint8 cwMode,
3289  uint8 txChan );
3290 
3312 extern hciStatus_t HCI_EXT_ModemHopTestTxCmd( void );
3313 
3336 extern hciStatus_t HCI_EXT_ModemTestRxCmd( uint8 rxChan );
3337 
3362 extern hciStatus_t HCI_EXT_EnhancedModemTestTxCmd( uint8 cwMode,
3363  uint8 rfPhy,
3364  uint8 rfChan );
3365 
3393 extern hciStatus_t HCI_EXT_EnhancedModemHopTestTxCmd( uint8 payloadLen,
3394  uint8 payloadType,
3395  uint8 rfPhy );
3396 
3420 extern hciStatus_t HCI_EXT_EnhancedModemTestRxCmd( uint8 rfPhy,
3421  uint8 rfChan );
3422 
3433 extern hciStatus_t HCI_EXT_EndModemTestCmd( void );
3434 
3436 
3459 extern hciStatus_t HCI_EXT_SetBDADDRCmd( uint8 *bdAddr );
3460 
3462 
3488 extern hciStatus_t HCI_EXT_SetSCACmd( uint16 scaInPPM );
3489 
3505 extern hciStatus_t HCI_EXT_EnablePTMCmd( void );
3506 
3526 extern hciStatus_t HCI_EXT_SetFreqTuneCmd( uint8 step );
3527 
3542 extern hciStatus_t HCI_EXT_SaveFreqTuneCmd( void );
3543 
3564 extern hciStatus_t HCI_EXT_SetMaxDtmTxPowerCmd( uint8 txPower );
3565 
3567 
3607 extern hciStatus_t HCI_EXT_MapPmIoPortCmd( uint8 ioPort, uint8 ioPin );
3608 
3610 
3626 extern hciStatus_t HCI_EXT_DisconnectImmedCmd( uint16 connHandle );
3627 
3646 extern hciStatus_t HCI_EXT_PacketErrorRateCmd( uint16 connHandle, uint8 command );
3647 
3689 extern hciStatus_t HCI_EXT_PERbyChanCmd( uint16 connHandle, perByChan_t *perByChan );
3690 
3692 
3701 extern hciStatus_t HCI_EXT_ExtendRfRangeCmd( void );
3702 
3715 extern hciStatus_t HCI_EXT_HaltDuringRfCmd( uint8 mode );
3716 
3718 
3720 
3774 extern hciStatus_t HCI_EXT_AdvEventNoticeCmd( uint8 taskID, uint16 taskEvent );
3775 
3777 
3832 extern hciStatus_t HCI_EXT_ConnEventNoticeCmd( uint16 connHandle, uint8 taskID, uint16 taskEvent );
3833 
3855 extern hciStatus_t HCI_EXT_BuildRevisionCmd( uint8 mode, uint16 userRevNum );
3856 
3858 
3890 extern hciStatus_t HCI_EXT_DelaySleepCmd( uint16 delay );
3891 
3893 
3912 extern hciStatus_t HCI_EXT_ResetSystemCmd( uint8 mode );
3913 
3914 // @cond NODOC
3915 
3926 extern hciStatus_t HCI_EXT_LLTestModeCmd( uint8 testCase );
3927 
3928 
3939 extern hciStatus_t HCI_EXT_OverlappedProcessingCmd( uint8 mode );
3940 
3942 
3963 extern hciStatus_t HCI_EXT_NumComplPktsLimitCmd( uint8 limit,
3964  uint8 flushOnEvt );
3965 
3967 
4000 extern hciStatus_t HCI_EXT_GetConnInfoCmd( uint8 *numAllocConns,
4001  uint8 *numActiveConns,
4002  hciConnInfo_t *activeConnInfo );
4003 
4005 
4022 extern hciStatus_t HCI_EXT_SetMaxDataLenCmd( uint16 txOctets,
4023  uint16 txTime,
4024  uint16 rxOctets,
4025  uint16 rxTime );
4026 
4039 extern hciStatus_t HCI_EXT_SetDtmTxPktCntCmd( uint16 txPktCnt );
4040 
4042 
4051 extern hciStatus_t HCI_EXT_ReadRandAddrCmd( void );
4052 
4053 
4065 extern hciStatus_t HCI_EXT_SetPinOutputCmd( uint8 dio,
4066  uint8 value );
4067 
4090 extern hciStatus_t HCI_EXT_SetLocationingAccuracyCmd( uint16 handle,
4091  uint8 sampleRate1M,
4092  uint8 sampleSize1M,
4093  uint8 sampleRate2M,
4094  uint8 sampleSize2M,
4095  uint8 sampleCtrl);
4096 
4118 extern hciStatus_t HCI_EXT_GetActiveConnInfoCmd( uint8 connId, hciActiveConnInfo_t *activeConnInfo );
4119 
4120 
4142 extern hciStatus_t HCI_EXT_SetVirtualAdvAddrCmd( uint8 advHandle, uint8 *bdAddr );
4143 
4167 extern hciStatus_t HCI_EXT_SetExtScanChannels( uint8 extScanChannelsMap );
4168 
4211 extern hciStatus_t HCI_EXT_SetQOSParameters( uint8 taskType,
4212  uint8 paramType,
4213  uint32 ParamVal,
4214  uint16 taskHandle);
4215 
4232 extern hciStatus_t HCI_EXT_SetQOSDefaultParameters( uint8 defaultParamConnPriorityValue );
4233 
4244 extern hciStatus_t HCI_EXT_CoexEnableCmd( uint8 enable );
4245 
4247 
4248 #ifdef __cplusplus
4249 }
4250 #endif
4251 
4252 #endif /* HCI_H */
4253 
hciStatus_t HCI_EXT_PacketErrorRateCmd(uint16 connHandle, uint8 command)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1028
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1131
uint8 status
packet status (success or CRC error)
Definition: hci.h:1121
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:951
uint8 sampleCount
number of samples
Definition: hci.h:1123
uint8 status
status of event
Definition: hci.h:964
hciStatus_t HCI_LE_EnhancedCteTxTestCmd(uint8 txChan, uint8 payloadLen, uint8 payloadType, uint8 txPhy, uint8 cteLength, uint8 cteType, uint8 length, uint8 *pAntenna)
LE Extended CTE Connectionless IQ Report Event.
Definition: hci.h:1177
This API allows the software components in the Z-Stack to be written independently of the specifics o...
uint8 eventType
scan request event type
Definition: hci.h:930
uint16 * pNumCompletedPackets
pointer to the number of completed packets array
Definition: hci.h:995
hciStatus_t HCI_EXT_SetMaxDataLenCmd(uint16 txOctets, uint16 txTime, uint16 rxOctets, uint16 rxTime)
uint16 connHandle
connection handle
Definition: hci.h:1084
uint8 status
status of event
Definition: hci.h:952
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1231
uint8 status
status of event
Definition: hci.h:1073
uint8 phy
current phy
Definition: hci.h:1115
uint8 addrType
public or random address type
Definition: hci.h:909
uint8 pktType
packet type
Definition: hci.h:1264
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:973
uint8 clockAccuracy
connection clock accuracy
Definition: hci.h:892
uint16 rssi
current rssi
Definition: hci.h:1166
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1247
uint16 Interval_Min
minimum connection interval
Definition: hci.h:1062
hciStatus_t HCI_LE_SetDefaultPhyCmd(uint8 allPhys, uint8 txPhy, uint8 rxPhy)
hciStatus_t HCI_LE_PeriodicAdvCreateSyncCancelCmd(void)
hciStatus_t HCI_LE_ReadPeriodicAdvListSizeCmd(void)
HCI Packet event.
Definition: hci.h:1254
osal_event_hdr_t hdr
osal event header
Definition: hci.h:982
#define B_RANDOM_NUM_SIZE
BLE Random Number Size.
Definition: bcomdef.h:133
uint8 numHandles
number of handles
Definition: hci.h:993
uint8 * pReturnParam
pointer to the return parameter
Definition: hci.h:1004
hciStatus_t HCI_LE_SetConnectionCteTransmitParamsCmd(uint16 connHandle, uint8 types, uint8 length, uint8 *pAntenna)
hciStatus_t HCI_LE_RemoveDeviceFromPeriodicAdvListCmd(uint8 advAddrType, uint8 *advAddress, uint8 advSID)
hciStatus_t HCI_LE_ReadRemoteUsedFeaturesCmd(uint16 connHandle)
LE CTE Connectionless IQ Report Event.
Definition: hci.h:1160
osal_event_hdr_t hdr
osal event header
Definition: hci.h:972
uint16 dataPktLen
data packet length
Definition: hci.h:1240
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:941
uint16 rssi
current rssi
Definition: hci.h:1117
Command Status Event.
Definition: hci.h:1017
void * iqSamples
list of interleaved I/Q samples (list size is dataLen*2)
Definition: hci.h:1156
hciStatus_t HCI_LE_SetPeriodicAdvParamsCmd(uint8 advHandle, uint16 periodicAdvIntervalMin, uint16 periodicAdvIntervalMax, uint16 periodicAdvProp)
uint16 connHandle
connection handle
Definition: hci.h:1074
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1082
osal_event_hdr_t hdr
osal event header
Definition: hci.h:928
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1179
hciStatus_t HCI_LE_AddDeviceToPeriodicAdvListCmd(uint8 advAddrType, uint8 *advAddress, uint8 advSID)
hciStatus_t HCI_LE_TestEndCmd(void)
hciStatus_t HCI_LE_SetResolvablePrivateAddressTimeoutCmd(uint16 rpaTimeout)
uint8 sampleRate
sample rate (1/2/3/4 MHz)
Definition: hci.h:1192
hciStatus_t HCI_EXT_SetMaxDtmTxPowerCmd(uint8 txPower)
Hardware Error Event.
Definition: hci.h:1026
hciStatus_t HCI_EXT_ModemTestTxCmd(uint8 cwMode, uint8 txChan)
hciStatus_t HCI_LE_TransmitterTestCmd(uint8 txChan, uint8 dataLen, uint8 pktPayload)
uint8 peerAddrType
peer address type
Definition: hci.h:887
uint16 connHandle
connection handle
Definition: hci.h:1133
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1113
uint8 status
status of event
Definition: hci.h:1036
int8 txPower
Tx Power information.
Definition: hci.h:1219
hciStatus_t HCI_LE_RandCmd(void)
uint8 clockAccuracy
Peer Clock Accuracy.
Definition: hci.h:1210
LE Advertising Report Event.
Definition: hci.h:906
uint8 sampleCount
number of samples
Definition: hci.h:1172
uint8 dataChIndex
index of data channel
Definition: hci.h:1116
hciStatus_t HCI_LE_ReadRfPathCompCmd(void)
uint8 status
status of event
Definition: hci.h:1203
#define B_MAX_ADV_LEN
BLE Maximum Advertising Packet Length.
Definition: bcomdef.h:130
uint8 nextDataChan
next channel
Definition: hci.h:943
uint8 dataChIndex
index of data channel
Definition: hci.h:1145
hciStatus_t HCI_LE_ReadResolvingListSizeCmd(void)
uint8 cteType
cte type
Definition: hci.h:1148
LE CTE Connection IQ Report Event.
Definition: hci.h:1110
LE Data Length Change Event.
Definition: hci.h:1080
hciStatus_t HCI_SetEventMaskPage2Cmd(uint8 *pMask)
hciStatus_t HCI_LE_ReadLocalSupportedFeaturesCmd(void)
uint8 numDevices
number of discovered devices
Definition: hci.h:921
uint8 cteType
cte type
Definition: hci.h:1187
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1202
uint16 syncHandle
sync handle in periodic adv
Definition: hci.h:1164
uint16 connectionHandle
connection handle
Definition: hci.h:869
uint16 connHandle
connection handle
Definition: hci.h:1265
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1083
hciStatus_t HCI_EXT_EnablePTMCmd(void)
hciStatus_t HCI_LE_SetDataLenCmd(uint16 connHandle, uint16 txOctets, uint16 txTime)
hciStatus_t HCI_LE_SetConnectionCteReceiveParamsCmd(uint16 connHandle, uint8 samplingEnable, uint8 slotDurations, uint8 length, uint8 *pAntenna)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:962
uint8 sampleCtrl
sample control - default filtering or RAW_RF
Definition: hci.h:1194
hciStatus_t HCI_LE_EnhancedCteRxTestCmd(uint8 rxChan, uint8 rxPhy, uint8 modIndex, uint8 expectedCteLength, uint8 expectedCteType, uint8 slotDurations, uint8 length, uint8 *pAntenna)
LE Phy Update Complete Event.
Definition: hci.h:1069
uint16 connEvent
connection event
Definition: hci.h:1151
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1051
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1130
osal_event_hdr_t hdr
osal event header
Definition: hci.h:992
uint8 status
packet status (success or CRC error)
Definition: hci.h:1150
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1059
hciStatus_t HCI_LE_EnhancedRxTestCmd(uint8 rxChan, uint8 rxPhy, uint8 modIndex)
uint8 rssiAntenna
antenna ID
Definition: hci.h:1118
uint8 dataStatus
Periodic data status.
Definition: hci.h:1222
hciStatus_t HCI_LE_ReadAntennaInformationCmd(void)
uint8 BLEEventCode
BLE Event code.
Definition: hci.h:1095
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1010
hciStatus_t HCI_WriteAuthPayloadTimeoutCmd(uint16 connHandle, uint16 aptoValue)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1035
uint8 slotDuration
sampling slot 1us or 2us
Definition: hci.h:1169
hciStatus_t HCI_LE_SetHostChanClassificationCmd(uint8 *chanMap)
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1104
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1162
union _hciEvt_BLEConnComplete_u_ hciEvt_BLEConnComplete_u
LE Connection Complete Event.
uint16 connInterval
connection interval
Definition: hci.h:873
uint16 Interval_Max
maximum connection interval
Definition: hci.h:1063
uint8 length
length of parametric data, in bytes
Definition: hci.h:1011
hciStatus_t HCI_EXT_NumComplPktsLimitCmd(uint8 limit, uint8 flushOnEvt)
hciStatus_t HCI_LE_SetPeriodicAdvDataCmd(uint8 advHandle, uint8 operation, uint8 dataLength, uint8 *data)
Used to set the advertiser data used in periodic advertising PDUs. This command may be issued at any ...
uint16 connectionHandle
connection handle
Definition: hci.h:965
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1072
uint16 maxRxTime
maximum receive time
Definition: hci.h:1088
hciStatus_t HCI_ReadRssiCmd(uint16 connHandle)
uint8 status
status
Definition: hci.h:1096
hciStatus_t HCI_LE_PeriodicAdvCreateSyncCmd(uint8 options, uint8 advSID, uint8 advAddrType, uint8 *advAddress, uint16 skip, uint16 syncTimeout, uint8 syncCteType)
uint16 connectionHandle
connection handle
Definition: hci.h:885
uint8 sampleSize
sample size (8 or 16 bit)
Definition: hci.h:1154
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1216
uint8 rssiAntenna
antenna ID
Definition: hci.h:1186
uint16 connTimeout
connection supervision timeout
Definition: hci.h:956
uint8 encEnable
encryption enabled or not
Definition: hci.h:976
uint8 eventIndex
event number
Definition: hci.h:1142
uint16 Latency
slave latency
Definition: hci.h:1064
hciStatus_t HCI_LE_ReadSupportedStatesCmd(void)
uint16 connLatency
connection latency
Definition: hci.h:890
uint8 slotDuration
sampling slot 1us or 2us
Definition: hci.h:1149
uint8 eventIndex
event number
Definition: hci.h:1182
uint8 linkType
synchronous or asynchronous buffer overflow
Definition: hci.h:1045
Vendor Specific Command Complete Event.
Definition: hci.h:1008
osal_event_hdr_t hdr
osal event header
Definition: hci.h:950
hciStatus_t HCI_EXT_DecryptCmd(uint8 *key, uint8 *encText)
hciStatus_t HCI_EXT_SetFreqTuneCmd(uint8 step)
hciStatus_t HCI_EXT_SetDtmTxPktCntCmd(uint16 txPktCnt)
Data structure for HCI Command Complete Event Return Parameter.
Definition: hci.h:1237
uint8 slotDuration
sampling slot 1us or 2us
Definition: hci.h:1120
void * iqSamples
list of interleaved I/Q samples (list size is dataLen*2)
Definition: hci.h:1195
uint16 totalDataLen
samples data length includes in all next events
Definition: hci.h:1181
hciStatus_t HCI_LE_EnhancedTxTestCmd(uint8 txChan, uint8 payloadLen, uint8 payloadType, uint8 txPhy)
hciStatus_t HCI_SetEventMaskCmd(uint8 *pMask)
hciStatus_t HCI_LE_SetPeriodicAdvEnableCmd(uint8 enable, uint8 advHandle)
Used to request the advertiser to enable or disable the periodic advertising for the advertising set...
hciStatus_t HCI_LE_AddWhiteListCmd(uint8 addrType, uint8 *devAddr)
uint8 clockAccuracy
connection clock accuracy
Definition: hci.h:876
Disconnection Complete Event.
Definition: hci.h:1033
hciStatus_t HCI_EXT_SaveFreqTuneCmd(void)
hciStatus_t HCI_LE_ReadSuggestedDefaultDataLenCmd(void)
hciStatus_t HCI_EXT_ResetSystemCmd(uint8 mode)
hciStatus_t HCI_LE_SetConnectionCteRequestEnableCmd(uint16 connHandle, uint8 enable, uint16 interval, uint8 length, uint8 type)
osal_event_hdr_t hdr
OSAL Event header.
Definition: hci.h:1263
Authenticated Payload Timeout Expired Event.
Definition: hci.h:1049
hciStatus_t HCI_EXT_EnhancedModemTestTxCmd(uint8 cwMode, uint8 rfPhy, uint8 rfChan)
uint8 sid
Peer SID.
Definition: hci.h:1205
uint16 periodicInterval
Periodic interval.
Definition: hci.h:1209
hciStatus_t HCI_LE_ReadWhiteListSizeCmd(void)
uint16 connHandle
connection handle
Definition: hci.h:1061
uint8 sampleSize
sample size (8 or 16 bit)
Definition: hci.h:1193
uint16 maxTxTime
maximum transmission time
Definition: hci.h:1086
hciStatus_t HCI_LE_SetEventMaskCmd(uint8 *pEventMask)
int8 rssi
report RSSI
Definition: hci.h:913
uint16 connLatency
connection latency
Definition: hci.h:955
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:920
uint8 * pData
data
Definition: hci.h:1268
hciStatus_t HCI_EXT_SetRxGainCmd(uint8 rxGain)
uint8 reason
reason
Definition: hci.h:975
int8 rssi
report RSSI
Definition: hci.h:934
Periodic Advertising Sync Lost Event.
Definition: hci.h:1228
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:983
uint16 cmdOpcode
command opcode
Definition: hci.h:1022
hciStatus_t HCI_LE_SetPeriodicAdvReceiveEnableCmd(uint16 syncHandle, uint8 enable)
uint8 chSelAlgo
channel selection algorithm
Definition: hci.h:1250
LE CTE Request Failed Event.
Definition: hci.h:1128
hciStatus_t HCI_ReadRemoteVersionInfoCmd(uint16 connHandle)
uint8 * data
Periodic data received from peer.
Definition: hci.h:1224
osal_event_hdr_t hdr
OSAL event header.
Definition: hci.h:1256
uint8 channelIndex
index of channel
Definition: hci.h:1184
hciStatus_t HCI_EXT_EndModemTestCmd(void)
hciStatus_t HCI_LE_ReadTxPowerCmd(void)
hciStatus_t HCI_LE_EncryptCmd(uint8 *key, uint8 *plainText)
hciStatus_t HCI_ReadLocalVersionInfoCmd(void)
hciStatus_t HCI_LE_ReadBufSizeCmd(void)
hciStatus_t HCI_LE_ReadLocalResolvableAddressCmd(uint8 localIdAddrType, uint8 *localIdAddr)
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1140
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1094
hciStatus_t HCI_EXT_ModemHopTestTxCmd(void)
Command Complete Event.
Definition: hci.h:999
uint8 rxPhy
RX PHY.
Definition: hci.h:1076
uint16 syncHandle
sync handle
Definition: hci.h:1218
hciEvt_DevInfo_t * devInfo
pointer to the array of devInfo
Definition: hci.h:922
LE Channel Selection Algorithm Event.
Definition: hci.h:1245
uint16 connHandle
connection handle
Definition: hci.h:974
HCI Data Packet.
Definition: hci.h:1261
uint8 status
status
Definition: hci.h:1105
uint8 status
status of event
Definition: hci.h:868
uint16 connTimeout
connection supervision timeout
Definition: hci.h:891
uint16 Timeout
supervision timeout
Definition: hci.h:1065
LE Generate DHKey Complete Event.
Definition: hci.h:1101
hciStatus_t HCI_EXT_EnhancedModemHopTestTxCmd(uint8 payloadLen, uint8 payloadType, uint8 rfPhy)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1139
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1230
uint16 * pConnectionHandle
pointer to the connection handle array
Definition: hci.h:994
uint16 eventCounter
periodic adv event counter
Definition: hci.h:1190
LE Remote Connection Parameter Request Event.
Definition: hci.h:1056
hciStatus_t HCI_EXT_PERbyChanCmd(uint16 connHandle, perByChan_t *perByChan)
uint8 status
packet status (success or CRC error)
Definition: hci.h:1189
uint16 connEvent
connection event
Definition: hci.h:1122
uint16 connLatency
connection latency
Definition: hci.h:874
uint8 status
status of event
Definition: hci.h:1060
hciStatus_t HCI_ReadLocalSupportedCommandsCmd(void)
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:929
hciStatus_t HCI_EXT_ModemTestRxCmd(uint8 rxChan)
uint16 connInterval
connection interval
Definition: hci.h:889
uint8 bleChan
BLE channel.
Definition: hci.h:933
uint8 eventType
advertisement or scan response event type
Definition: hci.h:908
osal_event_hdr_t hdr
osal event header
Definition: hci.h:866
hciEvt_BLEEnhConnComplete_t enhEvt
enhanced connection complete event
Definition: hci.h:902
int8 rssi
RSSI of the received packet.
Definition: hci.h:1220
int8 * iqSamples
list of interleaved I/Q samples
Definition: hci.h:1173
uint16 connHandle
connection handle
Definition: hci.h:1143
osal_event_hdr_t hdr
osal event header
Definition: hci.h:882
hciStatus_t HCI_LE_ClearPeriodicAdvListCmd(void)
hciStatus_t HCI_LE_ClearResolvingListCmd(void)
hciStatus_t HCI_EXT_SetSlaveLatencyOverrideCmd(uint8 control)
hciStatus_t HCI_EXT_OnePktPerEvtCmd(uint8 control)
uint16 connTimeout
connection supervision timeout
Definition: hci.h:875
Type definitions and macros for BLE stack.
VS LE Scan Request Report Event.
Definition: hci.h:926
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1112
hciStatus_t HCI_EXT_SetFastTxResponseTimeCmd(uint8 control)
LE Encryption Change Event.
Definition: hci.h:970
hciStatus_t HCI_EXT_BuildRevisionCmd(uint8 mode, uint16 userRevNum)
hciStatus_t HCI_LE_ReadPhyCmd(uint16 connHandle)
uint16 syncHandle
sync handle
Definition: hci.h:1204
uint16 connInterval
connection interval
Definition: hci.h:954
uint8 phy
current phy
Definition: hci.h:1144
uint8 * pEventParam
event parameters
Definition: hci.h:1013
uint8 channelIndex
index of channel
Definition: hci.h:1165
hciEvt_BLEConnComplete_t legEvt
connection complete event
Definition: hci.h:901
hciStatus_t HCI_ReadTransmitPowerLevelCmd(uint16 connHandle, uint8 txPwrType)
uint8 cmdStatus
command status
Definition: hci.h:1020
LE Enhanced Connection Complete Event.
Definition: hci.h:880
hciStatus_t HCI_LE_SetPhyCmd(uint16 connHandle, uint8 allPhys, uint8 txPhy, uint8 rxPhy, uint16 phyOpts)
uint16 connHandle
connection handle
Definition: hci.h:1052
uint16 cmdOpcode
command opcode
Definition: hci.h:1003
hciStatus_t HCI_LE_SetConnectionlessCteTransmitEnableCmd(uint8 advHandle, uint8 enable)
Used by the Host to request that the Controller enables or disables the use of Constant Tone Extensio...
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:867
Number of Completed Packets Event.
Definition: hci.h:990
hciStatus_t HCI_LE_ReadPeerResolvableAddressCmd(uint8 peerIdAddrType, uint8 *peerIdAddr)
OSAL Event Header.
Definition: osal.h:92
uint8 cteType
CTE type received.
Definition: hci.h:1221
hciStatus_t HCI_EXT_SetLocalSupportedFeaturesCmd(uint8 *localFeatures)
hciStatus_t HCI_LE_ReceiverTestCmd(uint8 rxChan)
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:883
uint8 txPhy
TX PHY.
Definition: hci.h:1075
hciStatus_t HCI_LE_RemoveDeviceFromResolvingListCmd(uint8 peerIdAddrType, uint8 *peerIdAddr)
hciStatus_t HCI_LE_RemoveWhiteListCmd(uint8 addrType, uint8 *devAddr)
uint8 numDataPkts
number of data packets
Definition: hci.h:1241
uint16 connHandle
connection handle
Definition: hci.h:942
uint16 rssi
current rssi
Definition: hci.h:1185
LE Periodic Advertising Report event.
Definition: hci.h:1214
hciStatus_t HCI_EXT_EnhancedModemTestRxCmd(uint8 rfPhy, uint8 rfChan)
uint16 pktLen
packet length
Definition: hci.h:1267
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1103
uint8 peerAddrType
peer address type
Definition: hci.h:871
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1019
hciStatus_t HCI_LE_PeriodicAdvTerminateSyncCmd(uint16 syncHandle)
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1217
uint8 phy
Peer PHY.
Definition: hci.h:1208
hciStatus_t HCI_EXT_ConnEventNoticeCmd(uint16 connHandle, uint8 taskID, uint16 taskEvent)
uint16 cmdOpcode
command opcode
Definition: hci.h:1012
uint8 reason
reason
Definition: hci.h:1038
uint8 numHciCmdPkt
number of HCI Command Packet
Definition: hci.h:1002
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1058
LE Extended CTE Connection IQ Report Event.
Definition: hci.h:1137
uint8 hardwareCode
hardware error code
Definition: hci.h:1029
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:108
Data Buffer Overflow Event.
Definition: hci.h:1042
uint8 role
role of connection
Definition: hci.h:886
LE Connection Complete Event.
Definition: hci.h:864
uint8 numHciCmdPkt
number of HCI command packets
Definition: hci.h:1021
uint8 dataLen
Periodic data length.
Definition: hci.h:1223
uint16 encryptedDiversifier
encrypted diversifier
Definition: hci.h:986
int8 * iqSamples
list of interleaved I/Q samples
Definition: hci.h:1124
uint8 slotDuration
sampling slot 1us or 2us
Definition: hci.h:1188
hciStatus_t HCI_LE_AddDeviceToResolvingListCmd(uint8 peerIdAddrType, uint8 *peerIdAddr, uint8 *peerIRK, uint8 *localIRK)
LE Read Remote Used Features Complete Event.
Definition: hci.h:960
uint16 eventCounter
periodic adv event counter
Definition: hci.h:1171
uint8 peerAddrType
peer address type
Definition: hci.h:931
uint16 syncHandle
sync handle
Definition: hci.h:1232
uint16 totalDataLen
samples data length includes in all next events
Definition: hci.h:1141
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1180
VS LE Channel Map Update Event.
Definition: hci.h:938
hciStatus_t HCI_ReadLocalSupportedFeaturesCmd(void)
uint8 sampleRate
sample rate (1/2/3/4 MHz)
Definition: hci.h:1153
hciStatus_t HCI_LE_ReadChannelMapCmd(uint16 connHandle)
uint16 connHandle
connection handle
Definition: hci.h:1249
uint8 status
status of event
Definition: hci.h:1239
osal_event_hdr_t hdr
osal event header
Definition: hci.h:940
hciStatus_t HCI_LE_ClearWhiteListCmd(void)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1001
LE Periodic Advertising Sync Established event.
Definition: hci.h:1199
hciStatus_t HCI_LE_ReadMaxDataLenCmd(void)
hciStatus_t HCI_EXT_SetSCACmd(uint16 scaInPPM)
uint16 connHandle
connection handle
Definition: hci.h:1114
hciStatus_t HCI_LE_SetConnectionlessCteTransmitParamsCmd(uint8 advHandle, uint8 cteLen, uint8 cteType, uint8 cteCount, uint8 length, uint8 *pAntenna)
Used by the Host to set the type, length, and antenna switching pattern for the transmission of Const...
uint8 cteType
cte type
Definition: hci.h:1119
uint16 maxTxOctets
maximum transmission bytes
Definition: hci.h:1085
hciStatus_t HCI_LE_SetConnectionlessIqSamplingEnableCmd(uint16 syncHandle, uint8 samplingEnable, uint8 slotDurations, uint8 maxSampledCtes, uint8 length, uint8 *pAntenna)
uint8 addrType
Peer address type.
Definition: hci.h:1206
uint16 rssi
current rssi
Definition: hci.h:1146
hciStatus_t HCI_ReadBDADDRCmd(void)
uint8 status
packet status (success or CRC error)
Definition: hci.h:1170
uint8 rssiAntenna
antenna ID
Definition: hci.h:1147
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1071
hciStatus_t HCI_HostNumCompletedPktCmd(uint8 numHandles, uint16 *connHandles, uint16 *numCompletedPkts)
hciStatus_t HCI_ReadAuthPayloadTimeoutCmd(uint16 connHandle, uint16 *aptoValue)
LE Connection Complete Event.
Definition: hci.h:899
hciStatus_t HCI_LE_SetConnectionCteResponseEnableCmd(uint16 connHandle, uint8 enable)
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1163
LE Connection Update Complete Event.
Definition: hci.h:948
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1248
hciStatus_t HCI_EXT_SetTxPowerCmd(uint8 txPower)
uint8 status
status of event
Definition: hci.h:884
hciStatus_t HCI_LE_WriteSuggestedDefaultDataLenCmd(uint16 txOctets, uint16 txTime)
LE Read P256 Public Key Complete Event.
Definition: hci.h:1092
uint8 dataLen
samples data length
Definition: hci.h:1191
uint8 dataLen
length of report data
Definition: hci.h:911
uint8 dataLen
samples data length
Definition: hci.h:1152
uint8 status
status
Definition: hci.h:1132
uint8 * pData
data
Definition: hci.h:1257
uint8 cteType
cte type
Definition: hci.h:1168
LE Advertising Packet Report Event.
Definition: hci.h:917
uint8 rssiAntenna
antenna ID
Definition: hci.h:1167
uint16 syncHandle
sync handle in periodic adv
Definition: hci.h:1183
hciStatus_t HCI_EXT_DisconnectImmedCmd(uint16 connHandle)
uint16 connHandle
connection handle
Definition: hci.h:1037
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:963
hciStatus_t HCI_LE_WriteRfPathCompCmd(int16 txPathParam, int16 rxPathParam)
uint8 pbFlag
flag
Definition: hci.h:1266
uint16 maxRxOctets
maximum receive bytes
Definition: hci.h:1087
uint8 role
role of connection
Definition: hci.h:870
hciStatus_t HCI_ResetCmd(void)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1044
hciStatus_t HCI_LE_SetPrivacyModeCmd(uint8 peerIdAddrType, uint8 *peerIdAddr, uint8 privacyMode)
uint16 connectionHandle
connection handle
Definition: hci.h:953
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1201
LE Long Term Key Requested Event.
Definition: hci.h:980
osal_event_hdr_t hdr
osal event header
Definition: hci.h:919
uint8 sampleCtrl
sample control - default filtering or RAW_RF
Definition: hci.h:1155
uint16 connHandle
connection handle
Definition: hci.h:984
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale