Changelog
Table of Contents
New Features
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-2966 | [MESH] Added support for BLE Mesh |
| BLE_AGAMA-2958 | Support Periodic Advertisement feature |
| BLE_AGAMA-2957 | Support Connectionless AoA feature |
| BLE_AGAMA-2950 | Scheduler Improvements - Connections Scheduling Fairness & Connection Priority Support |
| BLE_AGAMA-2817 | Add Authenticated Pairing Only mode |
| BLE_AGAMA-1785 | Expand multirole maximum number of connections to 16 |
EasyLink
| ID | Summary |
|---|---|
| EZLINKPROP-958 | [SPS] Limited Support for SysConfig Device/Board Migration Feature |
| EZLINKPROP-942 | EasyLink to support CC2652 SIP module in SDK |
TI-OpenThread
| ID | Summary |
|---|---|
| TIOP-1000 | Enable initial migration between boards for SysConfig |
TI 15.4-Stack
| ID | Summary |
|---|---|
| TI154STACK-3725 | Limited Support for SysConfig Device/Board Migration Feature |
| TI154STACK-3682 | Calculate Beacon Interval in SysConfig |
TI Z-Stack
| ID | Summary |
|---|---|
| ZIGBEE-1095 | CC2652RSIP Sysconfig Device/Board Migration Support |
DMM
| ID | Summary |
|---|---|
| DMM-1060 | Update the name DMMPolicy_updateStackState() API to DMMPolicy_updateApplicationState() |
| DMM-1059 | Update the name of DMMPolicy_StackRole_reservedx() API to DMMPolicy_StackRole_customx() |
| DMM-1052 | Support TI Clang Compiler for DMM Examples |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIRTOS-2064 | Add RPC framework to enable 2-chip solutions |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFDRIVER-323 | Make RF temperature compensation generic (SIP, HPOSC, custom calibration) |
| RFCORE-642 | [HID fast mode]: Added support for HID Fast Mode RF commands |
| RFCORE-697 | Create new multimode CPE patch containing HID Fast Mode Commands |
| RFCORE-686 | Agama: Release WMBUS C,T,S mode patch update |
| SRFSTUDIO-2882 | SYSCFG: Add support for cc13x2x7_cc26x2x7 |
| SRFSTUDIO-2906 | Add proprietary settings (100 kbps GFSK, 250 kbps GFSK) for SIP |
| SRFSTUDIO-2908 | Add Agama 704 pre-silicon IEEE 802.15.4 settings |
| SRFSTUDIO-2907 | Add characterized WMBUS settings |
Fixed Issues
BLE5-Stack
| ID | Summary |
|---|---|
| SCCM-64 | Corrected the security payload offset calculation in the image header for Off-Chip OAD |
| SCCM-63 | Enforced the program entry address to be within the OAD image range for On-Chip and Off-Chip OAD |
| SCCM-62 | Corrected the input parameter size for hash calculation to 32-bit for Off-Chip OAD |
| SCCM-61 | Add protections against zero image length and zero hash value for Off-Chip OAD |
| SCCM-60 | Enabled authentication of the persistent application image type for On-Chip OAD |
| BLE_AGAMA-2887 | Enabling co-ex for host test causes ICall_abort |
| BLE_AGAMA-2802 | Update persistent app projects to allow for authentication |
| BLE_AGAMA-2732 | Connection dropped with two Android master devices where second continuously reconnects |
| BLE_AGAMA-2715 | Invalid Adv Handle Returned by function llDmmSetThreshold |
| BLE_AGAMA-2638 | [AoA - PHY tests] The LE Test packet interval in LE Direct Test Mode is not spec compliant |
| BLE_AGAMA-2636 | [AoA - PHY tests] The IQ reports stops being sent by the device |
| BLE_AGAMA-2635 | [AoA - PHY tests] The Tx tests fail if payload length less to 38 bytes |
| BLE_AGAMA-2615 | Unable to re-start advertisement with multi role when connected to another Peripheral and using filter accept list |
| BLE_AGAMA-2613 | Fixed issue where file ti_ble_config.h always includes simple_gatt_profile |
| BLE_AGAMA-2546 | [GATT Builder] No error raised if several Callback functions have the same name |
| BLE_AGAMA-2513 | Device stops advertising when more than 5 connections are present |
| BLE_AGAMA-2500 | Under certain conditions, device becomes unresponsive after receiving connection request |
| BLE_AGAMA-2497 | Fixed buffer overflow bug in the OAD implementation |
| BLE_AGAMA-2479 | Fixed comments in ATT_HANDLE_VALUE_NOTI definition (att.h) |
| BLE_AGAMA-2344 | Occasional duplicate advertisement on the same channel |
| BLE_AGAMA-2061 | [Stability] Simple Peripheral fails to maintain more than 2 connections for more than 3H |
| BLE_AGAMA-1674 | Added API descriptions for items in out-of-band (OOB) pairing |
EasyLink
| ID | Summary |
|---|---|
| EZLINKPROP-987 | PER is not displayed for rtos GCC |
TI-OpenThread
| ID | Summary |
|---|---|
| SCCM-64 | Corrected the security payload offset calculation in the image header for Off-Chip OAD |
| SCCM-63 | Enforced the program entry address to be within the OAD image range for On-Chip and Off-Chip OAD |
| SCCM-62 | Corrected the input parameter size for hash calculation to 32-bit for Off-Chip OAD |
| SCCM-61 | Add protections against zero image length and zero hash value for Off-Chip OAD |
TI 15.4-Stack
| ID | Summary |
|---|---|
| TI154STACK-3693 | Collector only tracking first sensor and unable to disassociate second sensor after reset |
| TI154STACK-3665 | MAC acknowledges data frame with dst addrmode of 0 even when not the PAN coordinator |
| TI154STACK-3646 | Device fails to transmit ACK after first coordinator realignment message |
| SCCM-64 | Corrected the security payload offset calculation in the image header for Off-Chip OAD |
| SCCM-63 | Enforced the program entry address to be within the OAD image range for On-Chip and Off-Chip OAD |
| SCCM-62 | Corrected the input parameter size for hash calculation to 32-bit for Off-Chip OAD |
| SCCM-61 | Add protections against zero image length and zero hash value for Off-Chip OAD |
| SCCM-60 | Enabled authentication of the persistent application image type for On-Chip OAD |
TI Z-Stack
| ID | Summary |
|---|---|
| ZIGBEE-1172 | NPI memory leak from buffer deallocation order |
| ZIGBEE-1167 | Routing devices force link down to neighbors on first failed attempt at forwarding packet without nwk retries |
| ZIGBEE-1159 | Network Update Request processing does not account for nwkUpdateID wraparound |
| ZIGBEE-1122 | Changing MAC Frame Retries in sysconfig does not change number of MAC retries |
| ZIGBEE-1066 | Unicast Network Status command does not append correct extended destination address |
| ZIGBEE-1043 | Incoming application payload larger than 255 bytes is truncated |
| ZIGBEE-1040 | ZNP acting as a ZED cannot set rx-on-idle configuration during run-time |
| ZIGBEE-1012 | Possible memory corruption from parsing malformed Touchlink / Zigbee Light Link commands |
| ZIGBEE-1011 | Possible memory corruption from parsing malformed ZCL Foundation commands |
| ZIGBEE-1010 | Touchlink Target does not use Network Update ID of new network |
| ZIGBEE-993 | Unable to turn off route expiry time |
| ZIGBEE-962 | MAC_MCPS_DATA_CNF messages incorrectly parsed from inter-pan data requests |
| ZIGBEE-851 | Touchlink commissioning does not automatically initiate finding and binding |
DMM
| ID | Summary |
|---|---|
| SCCM-64 | Corrected the security payload offset calculation in the image header for Off-Chip OAD |
| SCCM-63 | Enforced the program entry address to be within the OAD image range for On-Chip and Off-Chip OAD |
| SCCM-62 | Corrected the input parameter size for hash calculation to 32-bit for Off-Chip OAD |
| SCCM-61 | Add protections against zero image length and zero hash value for Off-Chip OAD |
| DMM-1042 | Make DMM headers C++ friendly by adding extern “C” in case C++ is defined |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIRTOS-2115 | TI POSIX Integer Overflow issue |
| TIDRIVERS-4799 | CC13X2_CC26X2 NoRTOS startup file uses incorrect vector table size |
| TIDRIVERS-4787 | PINCC26XX shall not update PORTID bits when updating IOCFG register |
| TIDRIVERS-4737 | SHA2 segmented hashing produces incorrect results for SHA224 or SHA384 |
| TIDRIVERS-4173 | I2S driver uses incorrect number of SCK cycles in DSP mode |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFDRIVER-472 | RF Driver RFCC26XX_schedulerPolicy weak definition fails to link in strong symbol counterpart for TICLANG DMM |
| RFCORE-682 | [Connectionless AoA]: Fix issues with receiving short(<16usec) CTE tones |
| SRFSTUDIO-2904 | SYSCFG: Missing custom 868 MHz band setting for CC1352P7 |
| SRFSTUDIO-2893 | SYSCFG: Change to CC2652P/CC2652RB device name |
| SRFSTUDIO-2883 | SYSCFG: 169 MHz PHY shows wrong symbol rate in UI |
Known Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-2961 | [MESH] Mesh solution is not qualified |
| BLE_AGAMA-2947 | [MESH] Simple Mesh Node + Peripheral examples don't support proxy service & Provisioning over GATT |
| BLE_AGAMA-2917 | [Build] Persistent Application failed to compile in debug configuration due to memory limitation with all platforms |
| BLE_AGAMA-2914 | [MESH] BLE Mesh Examples do not have TICLANG Support |
| BLE_AGAMA-2913 | [MESH] IAR Bluetooth LE Mesh examples have a few compilation warnings |
| BLE_AGAMA-2845 | [CLAOA] Scanner shows only one IQ report when advertiser sends multiple CTE in one periodic train with 2M PHY |
| BLE_AGAMA-2266 | Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms |
| BLE_AGAMA-2245 | [Simple Peripheral] Number of connections shows zero after a connection if the previous connections were unsuccessful |
| BLE_AGAMA-2094 | [GATT Builder] Missing characteristics attributes (Indication, Primary/Secondary, Authentication/Authorization) |
| BLE_AGAMA-2033 | [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release) |
| BLE_AGAMA-2010 | [Multi-Sensor] Updating Report Interval Have no effect |
| BLE_AGAMA-1970 | [Multi-Sensor] Some of the Multi Sensor services fail to initiate or open when loading up |
| BLE_AGAMA-1675 | IOP: Device fails to pair with Meizu Pro 7 |
| BLE_AGAMA-1652 | [RTLS] AoA multiple connection: When>4 slaves are connected, the passive node sometimes fails to track some of the connections. |
| BLE_AGAMA-1435 | [Multi-Sensor] Accelerometer Service Disappears After First Connection |
| BLE_AGAMA-1416 | OAD offchip examples needs additional reset to load Factory Image |
| BLE_AGAMA-546 | Central applications do not receive timeout when connection fails |
| BLE_AGAMA-139 | When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection |
| BLE_AGAMA-80 | The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases. |
EasyLink
| ID | Summary |
|---|---|
| None | None |
TI-OpenThread
| ID | Summary |
|---|---|
| TIOP-954 | Thermostat attempts to promote to leader and form separate partition during reliability test |
| TIOP-953 | IAR OAD image does not reboot upon a successful OAD transfer |
TI 15.4 Stack
| ID | Summary |
|---|---|
| TI154STACK-3736 | In OAD projects CCFG settings must be configured in BIM project as SysConfig Device Configuration settings are not used |
TI Z-Stack
| ID | Summary |
|---|---|
| None | None |
DMM
| ID | Summary |
|---|---|
| None | None |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-4844 | Implement restrictions in errata note IOC_01 in SysConfig |
| TIDRIVERS-4801 | SPI MOSI line may periodically tri-state between transmissions at higher temperatures |
| TIDRIVERS-4127 | ADCBuf causes jitter when switching clock sources |
| TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| None | None |