RTLS Toolbox

The RTLS (Real Time Localization System) Toolbox, is a collection of RTLS techniques that can be implemented on TI’s standard Bluetooth Low Energy radios in the CC26xx series. These techniques provide raw data that can be utilized for developing localization algorithms and secure range bounding other Bluetooth Low Energy nodes. The two main techniques included in the RTLS toolbox are RSSI and Bluetooth Core Specification Version 5.1 Angle of Arrival.

RSSI details the Received Signal Strength Indication of an incoming signal and is commonly leveraged for deriving the distance between a receiver and a transmitter through the process of trilateration in localization algorithms. The Bluetooth Low Energy stack enables developers to receive the RSSI of an incoming Bluetooth packet.

Bluetooth Core Specification Version 5.1 Angle of Arrival is a technique for finding the direction that an incoming Bluetooth packet is coming from, creating a basis for triangulation. The device samples an incoming constant tone and as I/Q data. This raw I/Q data represents the amplitude and phase data of a signal and this data can be used to derive the angle the device transmitting the constant tone.

For detailed information on the specific example, see the relevant README.html file in the simplelink_cc13x2_26x2_sdk_x_xx_xx_xx/examples/rtos/CC26X2R1_LAUNCHXL/ble5stack/PROJECT folder.

Using the raw data provided by the RTLS Toolbox, TI is enabling developers to improve localization algorithms based on Bluetooth technology by delivering more data that can be leveraged for trilateration and triangulation.

The inherent flexibility of the CC13x2 or CC26x2 RF Core is what enables this significant extension of functionality. The main advantages using the CC13x2 or CC26x2 are that customers can start adding RTLS features and security with little extra cost, very little extra energy consumption and no increase in peak power.

There are two fundamentally different approaches for localization:

Trilateration Triangulation
../_images/trilateration.png
../_images/triangulation.png

Trilateration is where you know the distance between a reference node and a target node. This means that the possible locations seen by one locator constitute a circle, so typically three locators are needed to find a single common intersect point. (Assuming a 2D scenario)

RSSI Based Localization gives you the distance from the receiver to the transmitter.

Triangulation is where you know the direction from a reference node to a target node. This means that the possible locations seen by one locator constitute a straight line, so two nodes will be enough to determine a single intersect point. (Assuming a 2D scenario)

Angle of Arrival gives you the angle from the receiver to the transmitter.

Note

Existing examples with no external control interface are discontinued. All RTLS examples now have an external control interface.

General RTLS Software Architecture

The diagram below shows the RTLS software architecture.

With multiple nodes that collect localization data, it is important to have an architecture that supports control of these nodes. It must be possible to configure and trigger localization and it must be possible to retrieve localization data. We achieve this by reuse of our Network Processor Interface (NPI). It is basically a means to support Remote Procedure Calls (RPC) over a serial interface. Note that the architecture is such that it is possible to replace NPI with your own preferred serial protocol.

In our example we use UART as the serial transport layer. This is because it is readily available on host PC as UART over USB, and our LaunchPads include a UART to USB bridge. Along with the embedded examples we provide PC software to act as host, to control, retrieve and present localization data. This also allows much quicker customer performance characterization, as well as configuration of important parameters, not to mention the ability to develop and test higher level post-processing algorithms.

../_images/ditaa-669b1d8ffa33a2ff01e7714b625adfeaf599c4b0.png

RTLS Toolbox

The RTLS toolbox is a collection of software that is purposed for the localization use case. A table below summarizes each software component in the toolbox as well as its applications for localization. The software components below will run on the embedded nodes.

Software Component Usage
BLE-Stack Advertising, scanning, connection, exchanging RTLS data
Connection Monitor Follows a BLE connection using Micro BLE-Stack
Angle of Arrival Radio patches and driver to read AoA data embedded in BLE packets
Unified Network Processor Interface (UNPI) A serial protocol including packet format and handshaking for power savings
RTLS Control Module Implements the command and event set used to communicate RTLS information between devices. This runs on the embedded devices and translates UNPI frames into the necessary AoA function calls

The software components in the following table run on a PC. TI has setup a PC based environment to facilitate in evaluating and prototyping various RTLS algorithms. Once the algorithms are complete, the various PC components above can be migrated to an embedded device.

Software Component Usage
RTLS Util Event handling and distrution across nodes. Implements results queues, and setting up worker threads for data handling.
RTLS Node Manager Framework for sending and receiving RTLS commands and events from the embedded devices to PC. Implements higher level logic such as forwarding necessary BLE connection information to the connection monitor node.
Websocket Server Implements the server side of a TCP socket. Intended to bridge serial connections over UNPI from the node manager to TI RTLS UI GUI
RTLS UI GUI A GUI for aggregating and logging RTLS communication and graphing AoA data. This is Javascript based and runs in the web browser

RTLS Utility

The RTLSUtil module is a convenience layer that is built on top of the node manager that implements event handling and blocking as required by the RTLS network (e.g. seed distribution). Additionally the RTLSUtil module is able to setup worker threads for data processing of results from the device as well as creating queues to store the incoming data.

RTLS Node Manager

The RTLS Node Manager provides the following functionality:

  • A bridge between RTLS US GUI and CC13x2 or CC26x2
  • Holds the state of each device and takes care of configuration
  • Enables the simplicity of RTLS Control Module and RTLS UI GUI
  • Minimizes amount of the transactions between RTLS UI GUI and the rest of the system

Due to the above functionality, the Node Manager can operate on user’s CPU and help with slow bus (LIN/CAN).

RTLS Control Module

The RTLS Control Module is an on-chip module which runs as a RTOS Task and it provides the following functionality:

  • Parsing commands coming from Node Manager
  • RTLS Driver configuration and operation
  • RF and NPI message queue

RTLS Roles and Topology

Each node in an RTLS network utilizes the software components listed above in a different way to perform a specific task related to localization. These capabilities map to a role within the RTLS network and ultimately are implemented by sample applications within the SDK. There are three examples: rtls_master, rtls_slave, and rtls_passive. The capabilities of these examples are explained below. All embedded nodes implement UNPI and act as slaves in the UNPI protocol. Additionally all embedded nodes have the RTLS Control module implemented for processing RTLS commands from the UNPI interface.

Note

The following subsections aim to describe what localization roles are implemented by the sample applications in the SDK. This is not a comprehensive list of what is possible on each node, but rather an explanation of what the examples will do out of the box. For a list of potential combinations, please see Role Combinations.

Master

The RTLS master runs a full BLE-Stack and acts as a central device. It will scan and connect to the RTLS slave over BLE. Once a connection is established the RTLS Master will do the following:

  • Share the connection parameters (access address, master sleep clock accuracy, and CRC init) with the PC.
  • Use the BLE link to share AoA parameters with the peripheral device.
  • Implements the AoA master role
  • Does not send out AoA packets, but configures the slave to do so.

Slave

The RTLS slave runs a full BLE-Stack and acts as a peripheral device. This is the device that is to be located. The slave device will advertise and enter a connection with the RTLS Master.

  • Sends data packets with AoA tone embedded using Constant Tone Extension (CTE)
  • Advertises special string to be detected by rtls_master
  • Implements AoA slave role
  • BLE-Stack peripheral role
  • Wireless/battery operated, not connected to PC

Passive

The RTLS passive does not actively participate in the BLE connection between the RTLS master and slave. Instead, it uses the Micro BLE Stack in connection monitoring mode to follow the connection. To do this, the passive device relies on the Master to distribute the connection parameters once a connection is formed. The passive node does the following:

  • Implement AoA passive role
  • Receives packets with CTE and performs in-phase and quadrature component (IQ) sampling
  • Implements the Micro BLE-Stack connection monitoring application layer. See Connection Monitor (CM) Application for more information on the connection monitor.

PC/Central Processing Node

The PC node is responsible for controlling the embedded RTLS nodes by sending commands and processing events. In the SDK, this is realized by a combination of a Python layer that implements the UNPI master role and a websocket server that translates UNPI commands to a socket interface that is used by the GUI Composer application running in the browser.

This software is intended to use as a framework for extracting data from the embedded nodes and using it to prototype high level RTLS algorithms on the PC.

Note

In a final product, these algorithms may be implemented on an embedded device or even perhaps the RTLS master node. TI has provided PC software to aid in data plotting and prototyping various algorithms.

The PC implements the following roles in Python:

  • UNPI master
  • COM port interface
  • Implementation of RTLS UNPI subsystem/command set
  • Websocket server

The PC implements the following roles in RTLS UI GUI/Javascript:

  • Websocket client on localhost
  • Graphing and logging data from websocket
  • Parsing JSON objects to extract RTLS data
  • Issue commands to RTLS nodes via websocket to UNPI conversion
  • Enumerate devices
  • Distribute connection parameters to passives

Role Combinations

Note

In all of the tables following (BLE, AoA) features listed as optional are not implemented by the sample applications included in the SDK, but are valid and possible configurations that can be implemented by the user.

For example: rtls_master could be a multi-role device or rtls_passive could operate as AoA master.

BLE-Stack

The Bluetooth Core Specification Version 5.1 allows for devices to operate in various roles as well as combinations of roles. The table below shows the required and optional features for each example.

Example Name Central Peripheral Broadcaster Observer
RTLS Master R O O R
RTLS Slave O R R O
RTLS Passive No No O R*

Legend:

  • R: Required
  • O: Optional
  • No: Not supported

Note

The R* above denotes that while the connection monitor is capable of scanning for beacons, it is also required that the connection monitor follow a connection. The monitoring role is not officially defined by the Bluetooth Spec, but it is a critical functionality in the rtls_passive.

AoA

The Bluetooth Core Specification Version 5.1 defines multiple roles for both connected and connection-less AoA. The following configurations are supported by the examples in the SimpleLink CC13x2 / 26x2 SDK.

Example Name Send CTE Perform IQ Sampling
RTLS Master No No
RTLS Slave R No
RTLS Passive N/A R

Legend:

  • R: Required
  • O: Optional
  • No: Not supported
  • N/A: Not applicable

An AoA Master / Passive is capable of connecting to / monitoring up to and including eight AoA slaves simultaneously.

RTLS Driver

The purpose of RTLS Driver is to handle the Direct Call implementation of the RTLS module.

For more detail please take a look at AoA Driver section.

Physical Considerations

Before evaluating the RTLS solution, it is important to consider the environment. All radio communication protocols can be susceptible to multi-path fading, and RTLS based systems are not exempt. It is important to control the environment when evaluating or at least be aware of the potential effects of multi-path on the results.

It is recommended to evaluate the RTLS solution in an area that optimizes RF conditions. This includes:

  • An open space with no large metal or concrete obstructions (pillars, poles, etc)
  • Relatively few interference sources (i.e. Wi-Fi access points, etc)
  • Raised platforms for the nodes made out of cardboard ~1 m off the ground.

A desk environment generally has sub-optimal RF conditions and should be avoided.

See the image below for a recommended layout of the nodes during evaluation, this is a 2D image where all devices are laying on a flat surface “pointing” as shown in the picture. In this case each node should be placed on a box so that it does not sit directly on the ground.

../_images/suggested_layout.png

For angle of arrival application, we have created Bluetooth Angle of Arrival Antenna Design to further explains what users should look for when making their own AoA board.

RSSI Based Localization

RSSI details the Received Signal Strength Indication of an incoming signal and is the most commonly used method of trilateration localization in Bluetooth. TI Bluetooth low energy stack enables developers to receive the RSSI of an incoming Bluetooth packet with can be used to enable RTLS algorithms.

RSSI localization is based on the the Frii’s Transmission Equation. The core concept is that received signal strength is proportional to the distance of the transmitting node. The graphic below describes how RSSI can be used to estimate distance.

../_images/friis_equation_illustrated.png

Figure 121. Frii’s Equation Relationship between received power and distance.

While RSSI based localization is the most commonly used method in today’s RTLS systems, it also faces challenges that need to be overcome:

  • Accuracy can be influenced by the presence of reflections and obstructions
  • No Relay Attack protection

Some of these challenges with RSSI can be overcome through smart system design. TI’s RTLS Toolbox enables developers to monitor the connection between a master and slave and get independent RSSI measurements from the same packet via the Connection Monitor. This approach gives more data and reference points that can be used to help improve the resolution of an RTLS application.

For future RTLS applications, it is recommended to combine RSSI with the other localization techniques such as AoA to help improve the accuracy and security.

Reading RSSI

The Micro BLE Stack. (foundation of the Connection Monitor (CM) Application) and the full BLE5-Stack provide APIs to read RSSI information of the received packet. The following sections will describe how to extract RSSI information from the received packet.

Connection Monitor

The connection monitor will keep an array of connection information for each connection it is tracking. This includes master and slave RSSI from the last scan. These fields can be found in the ubCM_ConnInfo_t structure. The fields are rssiMaster and rssiSlave respectively.

RSSI information is valid after the monitor complete callback is invoked (when the monitoring scan is complete for a connection event).

The rtls_passive sample application shows an example of extracting slave RSSI in RTLSPassive_monitorCompleteEvt.

BLE(5)-Stack

When using the BLE5-Stack, the Gap_RegisterConnEventCb (Generic Access Profile (GAP)) will provide RSSI from the last connection event. It can be used in the central or peripheral configuration. The connection event callback is already the synchronization method used by the RTLSCtrl module for reporting data to the PC/Node Manager. See Gap_ConnEventRpt_t for information on how to extract the RSSI from connection event callbacks.

In the case of communication that consists of multiple packets, only the RSSI of the last received packet is reported. There is no averaging over channels. In general, the received signal strength will vary across channels due to varying channel conditions and antenna gains. This has the following consequences in regards to BLE:

  • Advertising: The RSSI will only be reported on the last advertisement channel that data is received on.
  • Connection Events with multiple data packets: These occur on the same channel but the RSSI will still only be reported for the last data packet that was received.

Note

The algorithm that calculates RSSI is the same algorithm for all BLE channels.

Calculation Detail

The RSSI value is a measurement of the actual power level delivered to the input of the reference design RF matching and balun. A valid range for RSSI signals is approximately -90dbm to -30dBm. Note that it is not easy to directly correlate RSSI to distance as it is highly dependent on the antenna design and polarization of both the transmitter and the receiver antenna.

The RSSI can have negative tolerance which means that if you are receiving on the sensitivity limit, reported RSSI can potentially be lower than this. The sensitivity can be found in the device datasheet and is in accordance with Bluetooth requirements.

The RSSI performance will be the same between both single ended and differential configurations and the expected accuracy is +/-4 dbm as stated in the datasheet.

Angle of Arrival

Angle-of-Arrival (AoA) is a technique for finding the direction that an incoming Bluetooth packet is coming from, creating a basis for triangulation.

An array of antennas with well-defined properties is used, and the receiver will switch quickly between the individual antennas while measuring the phase shift resulting from the small differences in path length to the different antenna.

These path length differences will depend on the direction of the incoming RF waves relative to the antennas in the array. In order to facilitate the phase measurement, the packet must contain a section of constant tone (CT) where there are no phase shifts caused by modulation.

Packet Format

In order to get a good estimate of ϕ (phase), all other intentional phase shifts in the signal should be removed.

Bluetooth Core Specification Version 5.1 introduces AoA/AoD which are covered under Direction Finding Using Bluetooth Low Energy Device section and it also specifies the following states can support sending direction finding packets:

  1. Periodic advertising; also called Connectionless CTE
  2. Connection; also called Connection CTE

The theory behind AoA/AoD and Connectionless/Connection CTE(Constant Tone Extension) is the same, therefore, we will only focus on Connection CTE AoA, which is what is currently provided in BLE5-Stack.

First let’s take a look at the payload. By adding a section of consecutive 1’s at the end of connection packet, effectively transmitting a single tone at the carrier frequency + 250kHz.

../_images/connection_aoa_packet_format.png

In the header, the CP bit (CTE Present)determines whether header contains CTEInfo or not.

The CTEType field of CTEInfo further specifies which type of direction finding packet this is and the CTETime field specifies the duration of the CTE.

Table 20. CTEType value
Value Description
0 AoA CTE packet.
1 AoD CTE with 1 µs slots.
2 AoD CTE with 2 µs slots.

The value of CTETime should be within 2~20 and it’s interpreted as in 8us unit. That means when CTETime is set to 20, there will be CTE at the end of connection packet which lasts 8*20 = 160(us).

This gives the receiver time to synchronize the demodulator first, and then store I and Q samples from the single tone 250kHz section at the end into a buffer and the buffer can then be post-processed by an AoA application

Note

The I/Q Data Sample is the coordinates of your signal as seen down the time axis. In fact, I/Q data is merely a translation of amplitude and phase data from a polar coordinate system to a Cartesian (X,Y) coordinate system and using trigonometry, you can convert the polar coordinate sine wave information into Cartesian I/Q sine wave data.
../_images/iq_phasor_diagram.png

Integration

The I and Q samples from the transmitted carrier frequency + 250kHz tone can be captured, pre-processed, and buffered by the RF Core without any load on the main MCU.

Due to the pre-processing, the application can determine the phase shift without having to remove DC offset or IF first, significantly simplifying the estimation process and leaving the application MCU free to do more on top.

../_images/processing_phase.png

For rtls_passive, the I/Q sampling rate is currently not configurable and it is 4 MHz. Each I/Q pair occupies 32 bits space in radio RAM and the radio RAM can store up to 512 samples (i.e. 2048 bytes - 2 kB). This limitation is only due to the micro-stack which limits the amount of data read in the Radio RAM. The radio RAM length is 4 kB.

With sampling rate 4MHz, there will be 16 I/Q pairs every 4us, which equals to 16 * 4 (one I/Q pair takes up 4 bytes space) = 64 bytes per 4us.

That means even if the CTE is 160us long with 4MHz sampling rate, the radio RAM for rtls_passive can only store I/Q data for 128us duration. There is currently no workaround for it unless we shorten the CTE length. This is not an issue for rtls_master.

Note

For rtls_passive, I and Q samples only have 13 bits resolution even though they occupy 16 bits space in RF Core RAM. Since they only have 13 bits resolution, the maximum and minimum value you will observe as signed integers are [4095, -4096].

For rtls_master, the I/Q sampleRate Setting is configurable and it’s from 1MHz up to 4MHz. Each I/Q pair occupies 32 bits space in radio RAM and the radio RAM can store up to 624 samples (2496 bytes - around 2.5kB). When the sampling frequency is maximum (4 MHz), exactly 624 samples are stored during each CTE. (The CTE lasts 160 us, minus 4 us of guard period. When sampling frequency is 4 MHz, in 156 us, 156*4 = 624 samples are stored. More details are provided in Valid I/Q Samples For Angle Calculation.)

Note

For rtls_master, I and Q samples resolution is configurable, please see sampleSize Setting. You can either choose 16 bits which only have 13 bits resolution or 8 bit resolution which is Bluetooth Core Specification Version 5.1 standard. It does not matter which resolution is chosen, each I/Q pair will always take 32 bits space in radio RAM.

The application layer passes in the antenna toggling table into RF Core, RF Core then does the antenna switching while collecting I/Q samples.

In the slave device, the RF Core ensures that the CTE is inserted at the end of the connection event packet without being distorted by the whitening filter.

In the passive and master devices, the RF Core analyzes the packet and starts capturing samples at the right time while synchronizing antenna switching. The samples are left in the RF Core RAM for analysis by the main MCU

AoA Driver

For rtls_passive, an example that uses Micro BLE Stack, the AoA driver is responsible for pin initialization, aoa enabling, data extraction and angle estimation.

AoA functionality in rtls_master is implemented as Bluetooth Core Specification Version 5.1 compliant, therefore, the initialization, aoa enabling and data extraction are moved to host module. However, users can still use RTLS Control Module to setup the wanted parameters.

Configurations Supported

* Sampling slot of 1us is supported by the AoA driver but some limitations exist when using the BOOSTXL-AOA hardware. The antennas of the BOOSTXL-AOA require 1.6 us to switch and settle (leaving 0.4 us in the sampling period to collect data). Other designs with faster RF switches can support 1us switching.

Data Collection Flow

When RF Core detects AoA packets, it will start sampling the I/Q on the tone while toggling the antenna according to a user defined period.

For rtls_passive, IQ samples will be extracted after RTLSPassive_monitorCompleteEvt() has triggered the next sync event. During sync event processing RTLSCtrl_postProcessAoa will enable the radio RAM, and read out the IQ samples using AOA_postProcess()

For rtls_master, IQ samples will be sent to application from RTLS Service host module with event type RTLSSRV_CONNECTION_CTE_IQ_REPORT_EVT.

According to the AoA result mode set by python, different sets of functions will be called and will return the corresponding data set as illustrated below:

../_images/ditaa-58e58e13d58abc9a1a384cb9fca6a35444012a02.png

Note

For rtls_master, when using the AOA_MODE_RAW, the BLE5-Stack will filter out the I/Q data from switching period if bit[0] in sampleCtrl is set to 0. To obtain the full set of I/Q data, you will need to set bit[0] in sampleCtrl to 1. Please see sampleCtrl I/Q data Filter Setting for the overview.

Warning

For rtls_master, when bit[0] for sampleCtrl= 1, AOA_MODE_PAIR_ANGLE and AOA_MODE_ANGLE are not supported.

Antenna Switching

Antennas toggle pattern is set in the python as part of RTLS_CMD_AOA_SET_PARAMS.

Listing 99. AoaSetParamsReq
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
  class AoaSetParamsReq(NpiRequest, SyncReq, FromAp):
      command = Commands.RTLS_CMD_AOA_SET_PARAMS
      struct = Struct(
          "aoaRole" / Enum(Int8ul, AoaRole),  # AOA_MASTER, AOA_SLAVE, AOA_PASSIVE
          "aoaResultMode" / Enum(Int8ul, AoaResultMode),  # AOA_MODE_ANGLE, AOA_MODE_PAIR_ANGLES, AOA_MODE_RAW
          "connHandle" / Int16ul,
          "slotDurations" / Int8ul,  # 1us/2us sampling slots
          "sampleRate" / Int8ul,  # 1Mhz (BT5.1 spec), 2Mhz, 3Mhz or 4Mhz - this enables oversampling
          "sampleSize" / Int8ul,  # 8 bit sample (as defined by BT5.1 spec), 16 bit sample (higher accuracy)
          "sampleCtrl" / Int8ul,  # sample control flags bit[0] = 0-default filtering, bit[0]= 1-RAW_RF no filtering
                                  # bit 4,5 - 0x10 - ONLY_ANT_1, 0x20 - ONLY_ANT_2
                                  # 0x00 is not a valid option.
          "samplingEnable" / Int8ul,
          # 0 = mask CTE even if enabled, 1 = don't mask CTE, even if disabled (support Unrequested CTE)
          "numAnt" / Int8ul,  # Number of antennas in antenna array
          "antArray" / Int8ul[this.numAnt],  # GPIO's of antennas
      )
Table 21. Antenna Pattern
Variable Definition
numAnt Number of IOs RF Core should toggle during I/Q sampling
antArray The IOs should be toggled during I/Q sampling.

Note

For rtls_passive, the slotDuration, sampleRate, sampleSize, samplingEnable, numAnt and antArray are hardcoded in the embedded software. The only configurable parameter is the aoaResultMode.

Following is an example provided in our rtls_agent toolbox.

Listing 100. IO control pattern setup example
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
      if aoa:
          if rtlsUtil.is_aoa_supported(all_nodes):
              aoa_params = {
                  "aoa_run_mode": "AOA_MODE_ANGLE",  ## AOA_MODE_ANGLE, AOA_MODE_PAIR_ANGLES, AOA_MODE_RAW
                  "aoa_cc2640r2": {
                      "aoa_cte_scan_ovs": 4,
                      "aoa_cte_offset": 4,
                      "aoa_cte_length": 20,
                      "aoa_sampling_control": int('0x00', 16),
                      ## bit 0   - 0x00 - default filtering, 0x01 - RAW_RF no filtering - not supported,
                      ## bit 4,5 - 0x00 - default both antennas, 0x10 - ONLY_ANT_1, 0x20 - ONLY_ANT_2
                  },
                  "aoa_cc26x2": {
                      "aoa_slot_durations": 1,
                      "aoa_sample_rate": 1,
                      "aoa_sample_size": 1,
                      "aoa_sampling_control": int('0x10', 16),
                      ## bit 0   - 0x00 - default filtering, 0x01 - RAW_RF no filtering,
                      ## bit 4,5 - 0x10 - ONLY_ANT_1, 0x20 - ONLY_ANT_2
                      "aoa_sampling_enable": 1,
                      "aoa_pattern_len": 3,
                      "aoa_ant_pattern": [0, 1, 2]
                  }
              }

The example shows that 3 IOs(aoa_pattern_len) should be toggled during the I/Q sampling and the order for toggling is set to 0, 1 and 2 which is mapped to the antennaTbl[] array element 0, 1 and 2 in ble_user_config.c. Bit[4:5] for aoa_sampling_control is set to 1 which corresponds to use only antenna array 1. For more information regarding antenna array selection, Please see sampleCtrl Antenna Array Setting for the overview.

The RF Core will then repeat the pattern until the end of the CTE. Afterwards, the IOs will be restored to their original state.

Even though RF Core takes care of the toggling, it does not initialize the pin state. The application should initialize the pin state by calling either AOA_initAntArray for rtls_passive or calling RTLSSrv_initAntArray for rtls_master. This is taken care when host sends RTLS_CMD_AOA_SET_PARAMS.

For users that want to use different IOs and patterns, please visit SimpleLink Academy –> RTLS Toolbox –> Angle of Arrival –>Task 3.

The RTLS API does not provide a direct way to determine which antenna has been used to sample a given piece of data. However, knowing the antenna switch sequence and the number of samples recorded per slot, it is possible to deduce the antenna used. Please see details in Valid I/Q Samples For Angle Calculation.

Convert I/Q Data to Angle Difference

When the radio frequency wave incident on to an antenna array (assuming there are only 2 antennas on the board, 4MHz sampling rate and 2us slot) and arrives at different antennas at different time, there will be a phase difference between the antennas. So we extract the phase difference between ant1_sample[8 to 15] and ant2_sample[8 to 15]. The switch among antennas will cause measurement error, therefore I/Q samples from 0 to 7 are discarded when calculating angles.

When using a custom HW with different antenna switch than what TI has on BOOSTXL-AOA board, you might be able to use more I/Q samples if the antenna switch settling time is shorter than 1 us. The method for determining how many I/Q samples can be used is explained in Valid I/Q Samples For Angle Calculation

The I/Q data can be presented into a X-Y domain with real number I and imaginary number Q (90 degree difference). As mentioned before, for each period of 250 kHz signal, we sample 16 I and Q data. If there is no difference, that means that the I/Q data is the same, therefore the phase between ant_1 sample1 will be the same to ant_2 sample1.

../_images/ant1_ant2_samplen.png
../_images/anlge_of_interest.png

Here is the code putting I/Q data into 2 dimensions and then the I/Q pairs were passed into function AOA_AngleComplexProductComp() to get final angle.

Listing 101. Get the phase differences.
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
for (uint16_t r = 1; r < (numIqSamples - (AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate))/(numAnt*sampleRate) ; ++r) // Sample Slot
{
  for (uint16_t i = 0; i < sampleRate; ++i) // Sample inside Sample Slot
  {
    // Loop through antenna pairs and calculate phase difference
    for (uint8_t pair = 0; pair < numPairs; ++pair)
    {
      const AoA_AntennaPair *p = &gAoaReport.antConfig->pairs[pair];
      uint8_t a = p->a; // First antenna in pair
      uint8_t b = p->b; // Second antenna in pair

      // Calculate the phase drift across one antenna repetition (X * complex conjugate (Y))
      int16_t Paa_rel = AOA_AngleComplexProductComp(pI[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + r*numAnt*sampleRate + a*sampleRate + i],
                                                    pQ[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + r*numAnt*sampleRate + a*sampleRate + i],
                                                    pI[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + (r-1)*numAnt*sampleRate + a*sampleRate + i],
                                                    pQ[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + (r-1)*numAnt*sampleRate + a*sampleRate + i]);

      // Calculate phase difference between antenna a vs. antenna b
      int16_t Pab_rel = AOA_AngleComplexProductComp(pI[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + r*numAnt*sampleRate + a*sampleRate + i],
                                                    pQ[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + r*numAnt*sampleRate + a*sampleRate + i],
                                                    pI[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + r*numAnt*sampleRate + b*sampleRate + i],
                                                    pQ[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + r*numAnt*sampleRate + b*sampleRate + i]);

      // Add to averages
      // v-- Correct for angle drift / ADC sampling frequency error
      antenna_versus_avg[a][b] += Pab_rel + ((Paa_rel * abs(a-b)) / numAnt);
      antenna_versus_cnt[a][b] ++;
    }
  }
}

int32_t AOA_AngleComplexProductComp(int32_t Xre, int32_t Xim, int32_t Yre, int32_t Yim)
{
  int32_t Zre, Zim;
  int16_t angle;

  // X*conj(Y)
  Zre = Xre*Yre + Xim*Yim;
  Zim = Xim*Yre - Xre*Yim;

  // Angle. The angle is returned in 256/2*pi format [-128,127] values
  angle = AOA_iatan2sc((int32_t) Zim, (int32_t) Zre);

  return (angle * angleconst);
}

Something to highlight is that in reality the 250kHz might not be perfect (for example, could be 255kHz or 245kHZ), therefore, there is slightly phase difference between ant_1 sample_n and ant_1 sample_(n + 16*1). Therefore run time compensation is also applied:

Listing 102. Compensation method.
1
2
3
4
5
// Calculate the phase drift across one antenna repetition (X * complex conjugate (Y))
int16_t Paa_rel = AOA_AngleComplexProductComp(pI[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + r*numAnt*sampleRate + a*sampleRate + i],
                                              pQ[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + r*numAnt*sampleRate + a*sampleRate + i],
                                              pI[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + (r-1)*numAnt*sampleRate + a*sampleRate + i],
                                              pQ[AOA_OFFSET_FIRST_VALID_SAMPLE*sampleRate + (r-1)*numAnt*sampleRate + a*sampleRate + i]);

Because of the non-perfect 250kHz tone, the phase difference is aggregated. Let’s say that every period will have 45 degree of delay. Then when comparing ant_1 sample_n and ant_1 sample_(n+16*1), the aggregated phase difference is 90 degree. But the real phase difference between every period is only 45 degree. Therefore the calculated phase difference must be divided by the number of antennas used, in this case 2.

Listing 103. Final phase difference
1
antenna_versus_avg[a][b] += Pab_rel + ((Paa_rel * abs(a-b)) / numAnt);

Valid I/Q Samples For Angle Calculation

The BLE spec defines two terms “Switch slot” and “Sample slot”. The length of the switch slot and sample slot must be equal, and only two values (1us or 2us) are allowed.

At the beginning of a CTE, the number of elements to discard depends on the length of the switch and sample slots and of the sampling frequency.

The following figure presents the way the CTE is sampled. The image is copied from the BLUETOOTH CORE SPECIFICATION Version 5.1 | Vol 6, Part B | 2.5.1.

../_images/cte_sampling.png

Figure 122. Constant tone sampling structure

  • When using 1us slots:
    • the guard period is 4us (no sampling is done during the guard period / no sample has to be discarded)
    • the reference period is 8us. All the samples acquired during the reference period has to be discarded (e.g. if the sampling frequency is 4MHz, it means that 32 samples have to be discarded - 8 samples have to be discarded if sampling frequency is 1Mhz)
    • the first switch slot (and all the others) lasts 1us. The data sampled during a switch slot has to be discarded (e.g. if the sampling frequency is 4MHz, it means that 4 samples have to be discarded during each switch slot - 1 sample per switch slot has to be discarded if sampling frequency is 1MHz).

    As a result, when sampling frequency is 4MHz, the first sample to consider is the 37th. When sampling frequency is 1MHz, the first sample to consider is the 10th.


  • When using 2us slots:
    • the guard period is still 4us (no sampling is done during the guard period / no sample has to be discarded)
    • the reference period is still 8us. All the samples acquired during the reference period have to be discarded (e.g. if the sampling frequency is 4MHz, it means that 32 samples have to be discarded - 8 samples have to be discarded if sampling frequency is 1Mhz)
    • the first switch slot (and all the others) lasts 2us. The data sampled during a switch slot has to be discarded (e.g. if the sampling frequency is 4MHz, it means that 8 samples have to be discarded during each switch slot - 2 samples per switch slot have to be discarded if sampling frequency is 1MHz).
    • the sampling slots are divided in two
      • one idle slot of 1us (which allows the antenna to settle). The data sampled during the idle slot has to be discarded (e.g. if the sampling frequency is 4MHz, it means that 4 samples have to be discarded during each idle slot - 1 sample per idle slot has to be discarded if sampling frequency is 1MHz).
      • one sample slot of 1us (e.g. if the sampling frequency is 4MHz, 4 samples are recorded per sample slot - 1 sample is recorded per sample slot if the sampling frequency is 1MHz)

    As a result, when sampling frequency is 4MHz, the first sample to consider is the 45th. When sampling frequency is 1MHz, the first sample to consider is the 12th.

The following figure presents how each sample slot is divided. This image is copied from the BLUETOOTH CORE SPECIFICATION Version 5.1 | Vol 6, Part B | 2.5.4

../_images/sample_slot_detail.png

Figure 123. “Zoom” on a sampling slot

Note

It’s important to note that 1us switch slot can only be used if the antennas are able to switch and settle in less than 1us. If the antennas are not able to switch and settle in less than 1us a part of the data sampled during the sampling slot won’t be correct and will have to be discarded.

An other good way to determine what I/Q samples to use is to plot all the I/Q samples.

The picture below shows the I/Q samples which were collected using the rtls_passive example together with rtls_master and rtls_slave examples using 4MHz sampling rate and 2us slot.

Table 22. Axis description
Axis Description
X top Angle between a rtls_slave device and rtls_passive.
X bottom Index number of I/Q data.
Y I/Q values.

The first 32(index 0~31) samples are taken in reference period which there is no antenna switching. Therefore the I/Q plot looks like sinusoid wave.

After that at index 32, you can see when switching happened there comes discontinuity of I/Q samples.

../_images/IQ-sample-switching.png

Note

It’s easier to see the phase discontinuity when there is indeed phase difference. Therefore, before collecting I/Q data, make sure the angle between rtls_passive and rtls_slave is not 0 degree.

Angle Compensation

Under AoA_getPairAngles(), the phase differences based on I and Q data were acquired. After that, angle compensation is added. Please see the code below. This is because angle estimation is affected by antenna pairs and frequency. The values p->gain, p->offset, channelOffset_A1 and channelOffset_A2 are based on lab measurements. Different antenna board design and frequency will give you different p->gain, p->offset, channelOffset_A1 and channelOffset_A2.

The following code can be found in AOA.c AoA_getPairAngles(), this is antenna pairs compensation.

Listing 104. Antenna pair compensation
1
2
3
4
5
6
// Write back result for antenna pairs
for (int pair = 0; pair < numPairs; ++pair)
{
  const AoA_AntennaPair *p = &gAoaReport.antConfig->pairs[pair];
  gAoaReport.antResult->pairAngle[pair] = (int)((p->sign * antenna_versus_avg[p->a][p->b] + p->offset) * p->gain);
}
../_images/lab_tuning.png

As you can see from the image above, the offset is applied to make sure the data received at 0 degree will derive 0 degree after the calculation and then the slope is changed to make it fit better with all the rest of the angles.

The compensation values for antenna array 1 can be found in ant_array1_config_boostxl_rev1v1.c AoA_AntennaPair pair_A1[]

Listing 105. Values used for compensation
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
AoA_AntennaPair pair_A1[] =
{
   {// v12
    .a = 0,       // First antenna in pair
    .b = 1,       // Second antenna in pair
    .sign = 1,    // Sign for the result
    .offset = -5, // Measurement offset compensation
    .gain = 0.95, // Measurement gain compensation
   },
   {// v23
    .a = 1,
    .b = 2,
    .sign = 1,
    .offset = -20,
    .gain = 0.9,
   },
   {// v13
    .a = 0,
    .b = 2,
    .sign = 1,
    .offset = -20,
    .gain = 0.50,
   },
};

Followed by antenna pair compensation, we added frequency compensation. For antenna array 1, the values used for frequency compensation can be found in ant_array1_config_boostxl_rev1v1.c int8_t channelOffset_A1[40].

Listing 106. Values used for compensation
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
int8_t channelOffset_A1[40] = {2, // Channel 0
                               2, // Channel 1
                               1, // Channel 2
                               1, // Channel 3
                               1, // Channel 4
                               1, // Channel 5
                               1, // Channel 6
                               1, // Channel 7
                               0, // Channel 8
                               0, // Channel 9
                               0, // Channel 10
                               3, // Channel 11
                               3, // Channel 12
                               2, // Channel 13
                               3, // Channel 14
                               3, // Channel 15
                               3, // Channel 16
                               3, // Channel 17
                               3, // Channel 17
                               3, // Channel 18
                               3, // Channel 20
                               3, // Channel 21
                               2, // Channel 22
                               3, // Channel 23
                               3, // Channel 24
                               3, // Channel 25
                               3, // Channel 26
                               3, // Channel 27
                               3, // Channel 28
                               2, // Channel 29
                               2, // Channel 30
                               2, // Channel 31
                               2, // Channel 32
                               2, // Channel 33
                               2, // Channel 34
                               2, // Channel 35
                               1, // Channel 36
                               0, // Channel 37
                               0, // Channel 38
                               0, // Channel 39
                               };

AoA Functions Overview

Here is the list of the most important functions for AoA users.

Python
  1. aoa_set_params:
Listing 107. AoA Set Parameter
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
class AoaSetParamsReq(NpiRequest, SyncReq, FromAp):
    command = Commands.RTLS_CMD_AOA_SET_PARAMS
    struct = Struct(
        "aoaRole" / Enum(Int8ul, AoaRole),  # AOA_MASTER, AOA_SLAVE, AOA_PASSIVE
        "aoaResultMode" / Enum(Int8ul, AoaResultMode),  # AOA_MODE_ANGLE, AOA_MODE_PAIR_ANGLES, AOA_MODE_RAW
        "connHandle" / Int16ul,
        "slotDurations" / Int8ul,  # 1us/2us sampling slots
        "sampleRate" / Int8ul,  # 1Mhz (BT5.1 spec), 2Mhz, 3Mhz or 4Mhz - this enables oversampling
        "sampleSize" / Int8ul,  # 8 bit sample (as defined by BT5.1 spec), 16 bit sample (higher accuracy)
        "sampleCtrl" / Int8ul,  # sample control flags 0x0-default filtering, 0x1-RAW_RF no filtering
        "samplingEnable" / Int8ul,
        # 0 = mask CTE even if enabled, 1 = don't mask CTE, even if disabled (support Unrequested CTE)
        "numAnt" / Int8ul,  # Number of antennas in antenna array
        "antArray" / Int8ul[this.numAnt],  # GPIO's of antennas
    )
Table 23. slotDurations Setting
Value Description
2 2us for antenna switching and 2us for I/Q sampling.
1 1us for antenna switching and 1us for I/Q sampling.

Note

For users that choose to have slotDuration = 1 needs to make sure that the RF switches on the custom board can settle down within 1 us.
Table 24. sampleRate Setting
Value Description
4 Process packets with AoA present in the header and sample CTE at 4 MHz.
3 Process packets with AoA present in the header and sample CTE at 3 MHz.
2 Process packets with AoA present in the header and sample CTE at 2 MHz.
1 Process packets with AoA present in the header and sample CTE at 1 MHz.
Table 25. sampleSize Setting
Value Description
2 I/Q samples returned with 13 bits resolution.
1 I/Q samples returned with 8 bits resolution.
Table 26. sampleCtrl I/Q data Filter Setting
bit[0] Description
1 BLE5-Stack returns whole I/Q data to the application.
0 BLE5-Stack filters out the I/Q data from switching period and returns the rest to application.
Table 27. sampleCtrl Antenna Array Setting
bit[4:5] Description
0b01 Application use only antenna array 1.
0b10 Application use only antenna array 2.

Note

rtls_passive only supports the following configuration: slotDuration = 2, sampleRate = 4 and sampleSize = 2.

RTLS_Passive

The functions covered under this section are all in AOA.c.

  1. AOA_init: This function takes care of the IO initialization.
AoA Application Overview

In the out of box software, the rtls_master and rtls_slave will form a BLE connection. After establishing the connection, rtls_master will send connection information through UART to PC and then the node manager will pass this piece of information to rtls_passive which can then track the connection.

Next, the node manager sets up AoA parameters for master and passive and then master will send a packet over the air to slave to setup the CTETime.

After that, the rtls_master will send a start AoA request over the air to the rtls_slave and to rtls_passive over wire, then rtls_slave will append CTE at the end of every connection packet.

rtls_passive and rtls_master can then do I/Q sampling and calculate angles base on the ConnectionCTE packets.

The sequence diagram below illustrates the whole process of how out of box examples work.

@startuml
participant rtls_passive as passive
participant "Node_Manager \n(Host MCU)" as manager
participant rtls_master as master
participant rtls_slave as slave

manager -> master: RTLS_CMD_IDENTIFY_Req
master -> manager: RTLS_CMD_IDENTIFY_Rsp
manager -> passive: RTLS_CMD_IDENTIFY_Req
passive -> manager: RTLS_CMD_IDENTIFY_Rsp

manager -> master: RTLS_CMD_SCAN_Req

activate master
master -> master: Start scanning \nfor rtls_slave

group rtls_slave not found

    manager -> master: RTLS_CMD_SCAN_STOP
    deactivate master
    manager -> master: RTLS_CMD_SCAN_Req \nrestart scanning

    activate master
    master -> master: Start scanning \nfor rtls_slave
    manager -> master: RTLS_CMD_SCAN_STOP
    deactivate master
    ...
    ... Repeat until device found ...
    ...
end


group rtls_slave found
    master -> manager: RTLS_CMD_SCAN_AsyncReq
    manager -> master: RTLS_CMD_SCAN_STOP
    manager -> master: RTLS_CMD_CONNECT
    master --> slave: Connection request
    == After connection has established ==
    master -> manager: RTLS_CMD_CONN_PARAMS
    manager -> passive: RTLS_CMD_CONN_PARAMS \npass on the connection info \nfor passive to track connection

    group AoA
        manager -> master: RTLS_CMD_AOA_SET_PARAMS
        master --> slave: RTLS_REMOTE_CMD_AOA_SET_PARAMS
        manager -> passive: RTLS_CMD_AOA_SET_PARAMS
        manager -> master: RTLS_CMD_AOA_ENABLE
        master --> slave: Enable sending \npackets with CTE
        manager -> passive: RTLS_CMD_AOA_ENABLE

        activate passive
        passive -> passive: Start following connection \nand waiting for connectionCTE packets
        master--> slave: Empty packet
        slave --> master: ConnectionCTE packet
        master --> master: Received ConnectionCTE packet \nand then calculate angle \nbetween slave and master
        passive -> passive: Received ConnectionCTE packet \nand then calculate angle \nbetween slave and passive
        master -> manager: RTLS_CMD_AOA_RESULT_ANGLE
        passive -> manager: RTLS_CMD_AOA_RESULT_ANGLE

        ...
        ... master and slave stay in connection ...
        ... master captures I/Q samples and calculates angle ...
        ... passive tracks connection, captures I/Q samples and calculates angle ...
        ...
    end
end

@enduml

Figure 124. Setting up RTLS AoA network and enable AoA