405 #ifndef ti_drivers_crypto_CryptoCC26XX__include 406 #define ti_drivers_crypto_CryptoCC26XX__include 413 #include <ti/devices/DeviceFamily.h> 414 #include DeviceFamily_constructPath(driverlib/crypto.h) 416 #include <ti/drivers/dpl/HwiP.h> 417 #include <ti/drivers/dpl/SemaphoreP.h> 423 #if DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X2_CC26X2 424 #warning "This driver is deprecated for the CC26x2 and CC13x2 families.\ 425 It is superceded by AESECB and AESCCM." 456 #define CRYPTOCC26XX_TIMEOUT 20 458 #define CRYPTOCC26XX_STATUS_SUCCESS 0 459 #define CRYPTOCC26XX_STATUS_ERROR -1 460 #define CRYPTOCC26XX_STATUS_UNDEFINEDCMD -2 462 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT 0 463 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY 1 464 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT 2 465 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY 3 466 #define CRYPTOCC26XX_OP_AES_ECB_ENCRYPT 4 467 #define CRYPTOCC26XX_OP_AES_ECB_DECRYPT 5 468 #define CRYPTOCC26XX_OP_AES_CBC_ENCRYPT 6 469 #define CRYPTOCC26XX_OP_AES_CBC_DECRYPT 7 472 #define CRYPTOCC26XX_OP_AES_CCM CRYPTOCC26XX_OP_AES_CCM_ENCRYPT 473 #define CRYPTOCC26XX_OP_AES_CCM_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY 474 #define CRYPTOCC26XX_OP_AES_CCMINV CRYPTOCC26XX_OP_AES_CCM_DECRYPT 475 #define CRYPTOCC26XX_OP_AES_CCMINV_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY 476 #define CRYPTOCC26XX_OP_AES_ECB CRYPTOCC26XX_OP_AES_ECB_ENCRYPT 477 #define CRYPTOCC26XX_OP_AES_ECB_NOCRYPT CRYPTOCC26XX_OP_AES_ECB_DECRYPT int CryptoCC26XX_allocateKey(CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation, const uint32_t *keySrc)
Function that allocates key, writes key into key store RAM and returns a handle to CryptoCC26XX Key...
CryptoCC26XX Transaction.
Definition: CryptoCC26XX.h:572
CryptoCC26XX Global Configuration.
Definition: CryptoCC26XX.h:480
CryptoCC26XX_Transaction * currentTransact
Definition: CryptoCC26XX.h:771
void CryptoCC26XX_Params_init(CryptoCC26XX_Params *params)
Function to initialize the CryptoCC26XX_Params struct to its defaults.
CryptoCC26XX_Config * CryptoCC26XX_Handle
A handle that is returned from a CryptoCC26XX_open() call.
Definition: CryptoCC26XX.h:491
CryptoCC26XX AES-CCM Transaction.
Definition: CryptoCC26XX.h:628
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:703
int CryptoCC26XX_close(CryptoCC26XX_Handle handle)
Function to closes a given CryptoCC26XX peripheral specified by the CryptoCC26XX handle.
void * msgOut
Definition: CryptoCC26XX.h:658
CryptoCC26XX Parameters.
Definition: CryptoCC26XX.h:552
uint8_t keyIndex
Definition: CryptoCC26XX.h:705
void * msgIn
Definition: CryptoCC26XX.h:691
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:629
Definition: CryptoCC26XX.h:537
HwiP_Struct hwi
Definition: CryptoCC26XX.h:773
uint8_t CryptoCC26XX_Operation
CryptoCC26XX Operation Type.
Definition: CryptoCC26XX.h:527
uint8_t fieldLength
Definition: CryptoCC26XX.h:664
Definition: CryptoCC26XX.h:540
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:573
Definition: CryptoCC26XX.h:504
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:687
int CryptoCC26XX_loadKey(CryptoCC26XX_Handle handle, int keyIndex, const uint32_t *keySrc)
Function that writes a given key into a key store.
void * msgOut
Definition: CryptoCC26XX.h:707
uint8_t keyIndex
Definition: CryptoCC26XX.h:631
char * nonce
Definition: CryptoCC26XX.h:634
void * msgOut
Definition: CryptoCC26XX.h:692
void CryptoCC26XX_Transac_init(CryptoCC26XX_Transaction *trans, CryptoCC26XX_Operation opType)
Function to initialize the CryptoCC26XX_Transaction struct to its defaults.
int CryptoCC26XX_releaseKey(CryptoCC26XX_Handle handle, int *keyIndex)
Function that releases the specified CryptoCC26XX Key.
char * header
Definition: CryptoCC26XX.h:657
CryptoCC26XX Hardware Attributes.
Definition: CryptoCC26XX.h:739
int openCnt
Definition: CryptoCC26XX.h:768
void const * hwAttrs
Definition: CryptoCC26XX.h:485
uint16_t headerLength
Definition: CryptoCC26XX.h:677
Definition: CryptoCC26XX.h:510
uint16_t msgInLength
Definition: CryptoCC26XX.h:675
void * msgIn
Definition: CryptoCC26XX.h:706
uint32_t timeout
Definition: CryptoCC26XX.h:769
Definition: CryptoCC26XX.h:542
CryptoCC26XX_Mode
CryptoCC26XX Mode Settings.
Definition: CryptoCC26XX.h:499
CryptoCC26XX AES-ECB Transaction.
Definition: CryptoCC26XX.h:702
char * msgIn
Definition: CryptoCC26XX.h:651
void CryptoCC26XX_init(void)
Function to initialize CryptoCC26XX driver. Users of this module must call init(). Multiple users/libraries may call init(), though subsequent calls may be benign.
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: CryptoCC26XX.h:758
int CryptoCC26XX_transact(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto operation (encryption or decryption) in blocking mode.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:688
CryptoCC26XX_KeyStore keyStore
Definition: CryptoCC26XX.h:770
uint8_t keyIndex
Definition: CryptoCC26XX.h:689
uint16_t msgInLength
Definition: CryptoCC26XX.h:693
int powerMngrId
Definition: CryptoCC26XX.h:743
void * object
Definition: CryptoCC26XX.h:482
Definition: CryptoCC26XX.h:543
Definition: CryptoCC26XX.h:539
uint8_t CryptoCC26XX_KeyStore
CryptoCC26XX Key.
Definition: CryptoCC26XX.h:561
CryptoCC26XX_Handle CryptoCC26XX_open(unsigned int index, bool exclusiveAccess, CryptoCC26XX_Params *params)
Function to initialize a given CryptoCC26XX peripheral specified by the particular index value...
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:704
void * nonce
Definition: CryptoCC26XX.h:690
CryptoCC26XX_KeyLocation
CryptoCC26XX Key Store Location.
Definition: CryptoCC26XX.h:535
int intNum
Definition: CryptoCC26XX.h:745
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:574
Definition: CryptoCC26XX.h:541
uint32_t timeout
Definition: CryptoCC26XX.h:553
CryptoCC26XX Object.
Definition: CryptoCC26XX.h:766
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:630
uint32_t baseAddr
Definition: CryptoCC26XX.h:741
Definition: CryptoCC26XX.h:538
int CryptoCC26XX_transactPolling(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in polling mode...
int CryptoCC26XX_transactCallback(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in callback mode...
uint8_t authLength
Definition: CryptoCC26XX.h:632
CryptoCC26XX AES-CBC Transaction.
Definition: CryptoCC26XX.h:686
Definition: CryptoCC26XX.h:536