Changelog
Table of Contents
New Features
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-2080 | Allow GAPBondMGR to delete bonds while in a connection |
| BLE_AGAMA-2073 | Provide the ability to choose what channel to scan on |
| BLE_AGAMA-2071 | [Preview] SysConfig - Add GATT Builder to the BLE module |
EasyLink
| ID | Summary |
|---|---|
| None | None |
TI-OpenThread
| ID | Summary |
|---|---|
| TIOP-883 | Integrate CoreSDK GA for 2Q20 |
| TIOP-882 | Downstream public OpenThread 2Q20 |
| TIOP-618 | Enable support for CC1352P-4 LP + CC2652P device @ 10dBm |
TI 15.4-Stack
| ID | Summary |
|---|---|
| None | None |
TI Z-Stack
| ID | Summary |
|---|---|
| ZIGBEE-850 | Implement low voltage NV callback for Zigbee sample application |
| ZIGBEE-849 | Enable support for CC1352P-4 LP + CC2652P device @ 10dBm |
| ZIGBEE-662 | CUI keyboard key entry for Zigbee network configuration |
| ZIGBEE-488 | CUI status line for Zigbee OTA update progress |
DMM
| ID | Summary |
|---|---|
| DMM-933 | Enable 2.4G projects for CC1352P-4 |
| DMM-921 | Support Block Mode |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIRTOS-2046 | Update examples/docs to Q2 2020 templates |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFDRIVER-306 | Add support for DMM Block Mode by allowing scheduler executionHook to reject imminent command |
| RFDRIVER-349 | SYSCFG: Do not pull GRANT signal after CoEx feature initialized |
| RFDRIVER-359 | SYSCFG: Configurable priority indication time (T2) for CoEx |
| SRFSTUDIO-2688 | SYSCFG: Add CC13x2 WiSUN PHY settings (modes 1a, 2a, 2b) |
| SRFSTUDIO-2704 | SYSCFG: Add CC13x2 WBDSSS 480 ksps, 240 kbps |
| SRFSTUDIO-2705 | SYSCFG: Add CC13x2 WBDSSS 480 ksps, 120 kbps |
| SRFSTUDIO-2706 | SYSCFG: Add CC13x2 WBDSSS 480 ksps, 60 kbps |
| SRFSTUDIO-2707 | SYSCFG: Add CC13x2 WBDSSS 480 ksps, 30 kbps |
| SRFSTUDIO-2703 | SYSCFG: Add CC13x2 WiSUN PHY settings (mode 4b) |
| SRFSTUDIO-2718 | SYSCFG: Add CC2642 wBMS PHY setting |
| SRFSTUDIO-2712 | SYSCFG: Add CC13x2 OOK 4.8 kbps, 433 MHz PHY definition |
| SRFSTUDIO-2714 | SYSCFG: Add PHY settings designed for TCXO usage on CC1312LP |
| SRFSTUDIO-2717 | SYSCFG: Add CC13x2 OOK 4.8 kbps, 915 MHz PHY definition |
| SRFSTUDIO-2713 | SYSCFG: Add CC13x2 OOK 4.8 kbps, 868 MHz PHY definition |
Fixed Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-2170 | linkDB_NumActive() function return is increased even for unsuccessful connections |
| BLE_AGAMA-2152 | [Coex] BLE central connection is broken and scan fails when Wi-Fi is turned on |
| BLE_AGAMA-2149 | Simple Peripheral application stopped advertising after an unsuccessful connection |
| BLE_AGAMA-1891 | Variable for storing characteristic handle should be 16 bit |
| BLE_AGAMA-1772 | Description of multi_role_processParamUpdate is incorrect |
| BLE_AGAMA-1486 | gapBondMgr_ProcessAttErrRsp uses attribute handle for connection handle |
| BLE_AGAMA-1454 | HCI and Micro Stack doxygen has unworking links into User's Guide |
| BLE_AGAMA-707 | HCI_LE_ReadPhyCmd missing documentation |
EasyLink
| ID | Summary |
|---|---|
| None | None |
TI-OpenThread
| ID | Summary |
|---|---|
| None | None |
TI 15.4-Stack
| ID | Summary |
|---|---|
| TI154STACK-3347 | Fixed beacon losses observed in 15.4 BCN 2.4GHz mode (co-processor) with high data traffic in large network |
TI Z-Stack
| ID | Summary |
|---|---|
| ZIGBEE-867 | SysConfig indicates incorrect range of values for NWK_MAX_DATA_RETRIES |
| ZIGBEE-838 | Parent sends Leave to end device who requested an out-of-range end device timeout value |
| ZIGBEE-823 | Route Records not sent for children devices when route record required flag is set |
| ZIGBEE-813 | Minimal Poll Period setting is not hidden in SysConfig when Always On power mode selected |
| ZIGBEE-734 | Add APS ACKs to Verify Key and Confirm Key |
| ZIGBEE-728 | MT_SysNvRead attempts to read NV item even when error code is not ZSuccess |
| ZIGBEE-725 | Build errors inside GenericApp when enabling Touchlink |
| ZIGBEE-713 | Touchlink Stealing fails to rejoin |
| ZIGBEE-700 | Update default handling for NWKSTAT_SOURCE_ROUTE_FAILURE in the stack |
| ZIGBEE-698 | Inclusion of FEATURE_NVEXID causes compile errors |
| ZIGBEE-689 | GPD Data Frame Security Key should only be shown in SysConfig when Security Key Type is OOB GPD Key |
| ZIGBEE-687 | OTA Client does not send default response for a non-success status Upgrade End Request |
DMM
| ID | Summary |
|---|---|
| DMM-958 | CC13X2-CC26X2: Easylink_setFrequency() does not use scheduling commands when running DMM |
| DMM-943 | Discrepancy between DMM sensor lpstk project and actual hardware |
| DMM-886 | LPSTK Accelerometer not returning data |
| DMM-849 | Number of channels that can be used in 15.4 FH mode is limited in DMM use cases |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-4275 | SDFatFS_open() was disabling interrupts when calling SD_open() |
| TIDRIVERS-4195 | UARTCC26XX_close releases UART pins while still in use by the driver causing application to crash |
| TIDRIVERS-4125 | ECCParams_getUncompressedGeneratorPoint() returns incorrect result |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFDRIVER-389 | SYSCFG: Fix antenna pin selection for CC1352P-2 20dBm power after changing from Sub1G to 2.4G PHY |
| RFCORE-587 | CoEx: TX-entry status field not reset to ACTIVE(1) if abort during transmission |
| RFCORE-517 | Fix IEEE CSMA command hitting assertion in slotted mode in some cases after unslotted CSMA |
| SRFSTUDIO-2747 | SYSCFG: Updated CC13x2 PA table @ 433 MHz with values from characterization |
| SRFSTUDIO-2727 | SYSCFG: Missing standard TX Power override for IEEE 802.15.4 setting for 10 dBm |
| SRFSTUDIO-2626 | SYSCFG & Code Export: BLE command params not generated for some BLE5 commands |
Known Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-2266 | Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms |
| BLE_AGAMA-2245 | [Simple Peripheral] Number of connections shows zero after a connection if the previous connections were unsuccessful |
| BLE_AGAMA-2192 | High PA (6 to10dBm) is not supported for CC1352P-4 LP |
| BLE_AGAMA-2184 | CC2652RB(BAW) persistent app failed to compile in debug configuration |
| BLE_AGAMA-2094 | [GATT Builder] Missing characteristics attributes (Indication, Primary/Secondary, Authentication/Authorization) |
| BLE_AGAMA-2061 | [Stability] Simple Peripheral fails to maintain more than 2 connections for more than 3H |
| BLE_AGAMA-2033 | [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release) |
| BLE_AGAMA-2010 | [Multi-Sensor] Updating Report Interval Have no effect |
| BLE_AGAMA-1974 | [RTLS] Sometimes there are no Angle reports for all connections when configured to 4-1-1 [aoa_sample_rate-aoa_slot_durations-aoa_sample_size], when working with CCS |
| BLE_AGAMA-1970 | [Multi-Sensor] Some of the Multi Sensor services fail to initiate or open when loading up |
| BLE_AGAMA-1675 | IOP: Device fails to pair with Meizu Pro 7 |
| BLE_AGAMA-1652 | [RTLS] AoA multiple connection: When>4 slaves are connected, the passive node sometimes fails to track some of the connections. |
| BLE_AGAMA-1441 | [RTLS] AoA angle calculation is deviated for boundary angles |
| BLE_AGAMA-1435 | [Multi-Sensor] Accelerometer Service Disappears After First Connection |
| BLE_AGAMA-1416 | OAD offchip examples needs additional reset to load Factory Image |
| BLE_AGAMA-1370 | CC13x2-P2 persistent app failed to compile in debug configuration |
| BLE_AGAMA-546 | Central applications do not receive timeout when connection fails |
| BLE_AGAMA-273 | [Known Limitation] SC can't save Bond data for more than 10 devices to NV |
| BLE_AGAMA-139 | When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection |
| BLE_AGAMA-80 | The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases. |
EasyLink
| ID | Summary |
|---|---|
| None | None |
TI-OpenThread
| ID | Summary |
|---|---|
| TIOP-954 | Thermostat attempts to promote to leader and form separate partition during reliability test |
| TIOP-953 | IAR OAD image does not reboot upon a successful OAD transfer |
TI 15.4 Stack
| ID | Summary |
|---|---|
| TI154STACK-3560 | Sensor SM does not successfully re-commission in BCN mode after reset and disassociation |
TI Z-Stack
| ID | Summary |
|---|---|
| None | None |
DMM
| ID | Summary |
|---|---|
| DMM-993 | High PA (6 to10dBm) is not supported for CC1352P-4 LP |
| DMM-935 | 1 out of 9 DMM FH Sensor locks up in 10 node 24 hour stability test |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-4127 | ADCBuf causes jitter when switching clock sources |
| TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| None | None |