Changelog
Table of Contents
New Features
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-1850 | [RTLS] Remove ToF support from SDK |
| BLE_AGAMA-1793 | Added 1/3 wire Wi-Fi CoEx interface support |
| BLE_AGAMA-1781 | Added an indication to the application when a Connection Parameter Update has been rejected |
| BLE_AGAMA-667 | Added support for notification of Channel Map update in BLE application |
| BLE_AGAMA-116 | Enhance The AE Advertisment Set Scheduling Algorithm |
EasyLink
| ID | Summary |
|---|---|
| EZLINKPROP-871 | Change the default frequency to 433MHz, power level to 14dBm for CC1352P-4 |
TI-OpenThread
| ID | Summary |
|---|---|
| TIOP-851 | Downstream OpenThread code for 20q1 |
| TIOP-788 | Enable CUI for device example projects |
| TIOP-738 | Add ability to set default TX power in syscfg |
TI 15.4-Stack
| ID | Summary |
|---|---|
| None | None |
TI Z-Stack
| ID | Summary |
|---|---|
| None | None |
DMM
| ID | Summary |
|---|---|
| DMM-394 | Secure commissioning of TI 15.4 stack devices using BLE |
| DMM-390 | Enabled support of up to 4 BLE connections in DMM examples |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| None | None |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFDRIVER-304 | SYSCFG: Allow overriding generated rfDriverCallback when custom board is used |
| RFDRIVER-146 | SYSCFG: Add support for configuring BLE/WiFi coexistence interface |
| RFDRIVER-144 | Introduce a new global event RF_GlobalEventInit which can be used to initialize pins |
| SRFSTUDIO-2582 | SYSCFG: CC1352R/P, CC1312R: Add preview settings for 4.8 kbps OOK PHY |
| SRFSTUDIO-2581 | SYSCFG: CC1352P/CC2652P: Add 10 dBm settings |
| SRFSTUDIO-2670 | SYSCFG: CC1352R/P, CC1312R: Add 15.4g 50kbps 433 MHz PHY settings |
| SRFSTUDIO-2672 | SYSCFG: CC1352R/P, CC1312R: Add 4.8 kbps GFSK 433 MHz PHY settings |
| SRFSTUDIO-2673 | SYSCFG: CC1352P/R, CC1312: Add 200 kbps 433 MHz proprietary PHY settings |
| SRFSTUDIO-2600 | SYSCFG: CC1352R/P, CC1312R: Add SimpleLink Long Range (SLR) 433 MHz PHY settings |
| SRFSTUDIO-2577 | SYSCFG: Provide define to tell index of stack specific overrides |
| SRFSTUDIO-2613 | SYSCFG: CC1352R/P, CC1312R: Add 1 Mbps 2-GFSK 868/915 MHz PHY settings |
| SRFSTUDIO-2571 | SYSCFG: Add possibility to modify front-end settings from the UI |
Fixed Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-1887 | Fixed a specification incompliance where the DH Key check was skipped on the device in the peripheral role if a central device attempted to start encryption before it sends a DH Key check value to the peripheral |
| BLE_AGAMA-1708 | [RTLS] AoA multiple connection: When>4 slaves are connected, the master node might disconnect after aoa_start command is sent. WA requires delaying the aoa_start command for a few seconds after the connection is established. |
| BLE_AGAMA-1707 | Fixed a BLE Stack DoS (crash) vulnerability caused by invalid connection PDU parameters |
| BLE_AGAMA-1692 | Radio quits transmitting and receiving when enabling 3+ connections and advertising and scanning at the same time. |
| BLE_AGAMA-1613 | Sending connection update request fails when the device has previously been rejected |
| BLE_AGAMA-1597 | [RTLS] AoA Master sometimes get stuck in multiple connections scenario |
| BLE_AGAMA-1587 | Receiving a connection request packet with transmit window offset = 0 will fail. |
| BLE_AGAMA-1573 | [SYSCFG] Custom Board configuration in sysconfig is not supported |
| BLE_AGAMA-1448 | When using slave latency, the connection is often dropped with 1 phone, and sometimes dropped with multiple phones connected to central device |
| BLE_AGAMA-741 | Gracefully handle ATT_ERR_UNSUPPORTED_REQ |
EasyLink
| ID | Summary |
|---|---|
| EZLINKPROP-869 | Using Custom Board in SysConfig may cause unexpected build and runtime behavior |
TI-OpenThread
| ID | Summary |
|---|---|
| TIOP-840 | Thread Stack on CC2652RB can get stuck randomly after several hours when the temperature changes continuously. Issue not observed when temperature remains constant. |
TI 15.4-Stack
| ID | Summary |
|---|---|
| TI154STACK-3452 | Fixed issue of project debug entering Error_policySpin with BIOS asserts enabled |
| TI154STACK-3430 | Fixed issue of sensor orphan scan will take ~17 minutes before scanCnfCb is called |
| TI154STACK-3423 | Fixed usage of regional naming in PHY IDs |
| TI154STACK-3414 | Fixed issue of HEAPMGR_INIT should not assert out of box, when HEAPMGR_ASSERT is enabled |
| TI154STACK-3381 | Fixed issue of 15.4 sensor locking up when scanning after ~10-20 min |
| TI154STACK-3335 | Fixed issue of when using Custom Board in SysConfig causing unexpected build and runtime behavior |
TI Z-Stack
| ID | Summary |
|---|---|
| ZIGBEE-709 | NWK Route Requests sent with NWK DestAddr to all RxOnIdle devices instead of only Routing devices |
| ZIGBEE-704 | Touchlink Initiator not scanning secondary channels if network already formed |
| ZIGBEE-699 | Parent Annce / Parent Annce Rsp payload can exceed max packet size |
| ZIGBEE-688 | Zigbee Extended PAN ID in SysConfig is reversed |
| ZIGBEE-685 | In rare cases, sleepy ZEDs that send multiple Association Reqs during initial join can be sent a Leave Req |
| ZIGBEE-683 | ZCL Req/Rsp sequence numbers between OTA Server/Client do not match |
| ZIGBEE-681 | MTO Routing does not send Route Records for all relayed ZED unicast data frames |
| ZIGBEE-680 | Joining device broadcasts MgmtPermitJoining_req even if no TCLK was not received |
| ZIGBEE-676 | SysConfig does not allow configuration of TX power and PA |
| ZIGBEE-675 | Defining POLL RATE as 0 in SysConfig does not allow ZED to stay in network |
| ZIGBEE-673 | ZC crashes during TCLK exchange when more than 16 joiners connect with Install Codes |
| ZIGBEE-672 | Unnecessary route requests due to route replies not updating neighbor table entries |
| ZIGBEE-670 | Zigbee devices do not rejoin network if using install codes |
| ZIGBEE-668 | Zigbee Default Network Key in SysConfig is reversed |
| ZIGBEE-655 | ZCL OTA sends UNSUP_CLUSTER_COMMAND instead of MALFORMED_COMMAND status code |
| ZIGBEE-648 | Incorrect extAddr is used in bdb_TCAddJoiningDevice() |
| ZIGBEE-647 | Preconfigured PAN ID may not be selected correctly if multiple networks are open |
| ZIGBEE-607 | Using Custom Board in SysConfig may cause unexpected build and runtime behavior |
DMM
| ID | Summary |
|---|---|
| DMM-903 | Fixed issue in DMM projects where GAP_EVT_ADV_START_AFTER_ENABLE not received with TI 15.4-Stack in FH mode |
| DMM-853 | Fixed an issue where using ROV did not work when using the auto-heap feature. |
| DMM-845 | Fixed issue of DMM 15.4 collector unable to maintain connection with one DMM sensor when connected to 9 DMM sensors in 24 hour 15.4 beacon mode large network test |
| DMM-842 | Fixed issue of DMM RX-Always-On examples show BLE disconnection when changing from short to long connection interval at runtime |
| DMM-821 | Fixed issue of when using Custom Board in SysConfig causing unexpected build and runtime behavior |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-4130 | Logic error in UART driver blocking mode |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFDRIVER-319 | RF driver enters Error_policySpin with BIOS asserts enabled because PIN_open was called from SWI when using antenna switching |
| RFDRIVER-305 | SYSCFG: RF driver callback function name will sometimes be used undefined |
| RFDRIVER-335 | Add support for BLE/WiFi coexistence interface (Modes: 3-wire, 1-wire GRANT, and 1-wire REQUEST) |
| RFDRIVER-279 | RAT Timer should allow for RAT Channel owner to disable the channel |
| RFDRIVER-269 | Bus Error reading RAT registers when RAT module is powered down |
| RFCORE-469 | IEEE RX command ending while TX was starting left TX command in active state with no transmission |
| SRFSTUDIO-2671 | SYSCFG: CC1352R/P, CC2652R/P: Fixed issue in 100/250 kbps GFSK and 250 kbps MSK PHY settings causing higher current consumption. RF performance is unchanged. |
| SRFSTUDIO-2674 | CC1352P/R, CC1312R: Updated settings improving phase noise in Sub-1 GHz narrowband PHYs |
Known Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-2033 | [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release) |
| BLE_AGAMA-2010 | [Multi-Sensor] Updating Report Interval Have no effect |
| BLE_AGAMA-1974 | [RTLS] Sometimes there are no Angle reports for all connections when configured to 4-1-1 [aoa_sample_rate-aoa_slot_durations-aoa_sample_size], when working with CCS |
| BLE_AGAMA-1970 | [Multi-Sensor] Some of the Multi Sensor services fail to initiate or open when loading up |
| BLE_AGAMA-1675 | IOP: Device fails to pair with Meizu Pro 7 |
| BLE_AGAMA-1652 | [RTLS] AoA multiple connection: When>4 slaves are connected, the passive node sometimes fails to track some of the connections. |
| BLE_AGAMA-1441 | [RTLS] AoA angle calculation is deviated for boundary angles |
| BLE_AGAMA-1435 | [Multi-Sensor] Accelerometer Service Disappears After First Connection |
| BLE_AGAMA-1416 | OAD offchip examples needs additional reset to load Factory Image |
| BLE_AGAMA-1370 | CC13x2-P2 persistent app failed to compile in debug configuration |
| BLE_AGAMA-546 | Central applications do not receive timeout when connection fails |
| BLE_AGAMA-273 | [Known Limitation] SC can't save Bond data for more than 10 devices to NV |
| BLE_AGAMA-139 | When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection |
| BLE_AGAMA-80 | The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases. |
EasyLink
| ID | Summary |
|---|---|
| None | None |
TI-OpenThread
| ID | Summary |
|---|---|
| None | None |
TI 15.4 Stack
| ID | Summary |
|---|---|
| TI154STACK-3347 | Beacon losses observed in 15.4 BCN 250kbps mode(co-processor) at 2.4GHz with high data traffic in large network |
TI Z-Stack
| ID | Summary |
|---|---|
| ZIGBEE-698 | Inclusion of FEATURE_NVEXID causes compile errors, MT_SysNv* APIs need to be updated |
| ZIGBEE-687 | OTA Client does not send default response for a non-success status Upgrade End Request |
DMM
| ID | Summary |
|---|---|
| DMM-937 | IAR OAD Projects lock up when performing OAD the third time |
| DMM-935 | 1 out of 9 DMM FH Sensor locks up in 10 node 24 hour stability test |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-3635 | UART_read returns 0 in portable after a power-cycle on CC13x0 and CC26x0 devices |
| TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| None | None |