Over-the-Air Download (OAD)¶
The following sections aim to describe the lower layers of OAD software that are common across all protocol stack implementations. This includes the OAD image header, the flash layout, Boot Image Manager, and the oad_image_tool.
Warning
The Z-Stack OAD does not implement or perform any security or authentication mechanisms as part of the firmware update process. System developers should take measures to adequately authenticate peer devices and only accept and/or apply firmware images transferred from trusted sources via OAD.
When using the Secure OAD feature along with recommended parameters, firmware images are authenticated on the device using ECDSA signature validation algorithms to ensure image authenticity prior to updating the running firmware image.
- Introduction
- Boot Image Manager (BIM)
- BIM for Off-Chip OAD
- OAD Image Header
- OAD External Flash Image Header
- Flash Layout for Off-Chip OAD
- OAD Image Tool